<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Uboot booting M7 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Uboot-booting-M7/m-p/1730426#M4896</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am currently working on an attempt to boot a M7 application on S32G399A board using Uboot. So for this to be successful, which Uboot version should i be using.&lt;/P&gt;&lt;P&gt;Tried flashing the application using Uboot v2020.04 , Which was already used for booting QNX on A53. But for M7 the application is not running.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, is there any other version of Uboot that can be used for my usecase. Or should i add anymore configurations within this current version?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thankyou.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Sep 2023 10:33:23 GMT</pubDate>
    <dc:creator>aswinknp</dc:creator>
    <dc:date>2023-09-27T10:33:23Z</dc:date>
    <item>
      <title>Uboot booting M7</title>
      <link>https://community.nxp.com/t5/S32G/Uboot-booting-M7/m-p/1730426#M4896</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am currently working on an attempt to boot a M7 application on S32G399A board using Uboot. So for this to be successful, which Uboot version should i be using.&lt;/P&gt;&lt;P&gt;Tried flashing the application using Uboot v2020.04 , Which was already used for booting QNX on A53. But for M7 the application is not running.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, is there any other version of Uboot that can be used for my usecase. Or should i add anymore configurations within this current version?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thankyou.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 10:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Uboot-booting-M7/m-p/1730426#M4896</guid>
      <dc:creator>aswinknp</dc:creator>
      <dc:date>2023-09-27T10:33:23Z</dc:date>
    </item>
  </channel>
</rss>