<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Questions about S32G2 CAN gateway</title>
    <link>https://community.nxp.com/t5/S32G/Questions-about-S32G2-CAN-gateway/m-p/1725238#M4838</link>
    <description>&lt;P&gt;We are using S32G2 as the CAN gateway and the LLCE engine is used. What should I do if only specific packets are forwarded?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For example, the 1-channel CAN bus has 10 ID packets, and I only need the packets with two ids. How can I configure the forwarding for only these two ids?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Sep 2023 06:21:48 GMT</pubDate>
    <dc:creator>pole</dc:creator>
    <dc:date>2023-09-19T06:21:48Z</dc:date>
    <item>
      <title>Questions about S32G2 CAN gateway</title>
      <link>https://community.nxp.com/t5/S32G/Questions-about-S32G2-CAN-gateway/m-p/1725238#M4838</link>
      <description>&lt;P&gt;We are using S32G2 as the CAN gateway and the LLCE engine is used. What should I do if only specific packets are forwarded?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For example, the 1-channel CAN bus has 10 ID packets, and I only need the packets with two ids. How can I configure the forwarding for only these two ids?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Sep 2023 06:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Questions-about-S32G2-CAN-gateway/m-p/1725238#M4838</guid>
      <dc:creator>pole</dc:creator>
      <dc:date>2023-09-19T06:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about S32G2 CAN gateway</title>
      <link>https://community.nxp.com/t5/S32G/Questions-about-S32G2-CAN-gateway/m-p/1727954#M4861</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Hope you are doing well&lt;/P&gt;
&lt;P&gt;Refer the Document Number: AN13423 (Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G ).&amp;nbsp; There are also example in s32ds as Can_Llce_Ds_Can2Can_S32G274a_M7 which show the internal routing functionality of CAN_LLCE Driver&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards ,&lt;/P&gt;
&lt;P&gt;Tushar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 09:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Questions-about-S32G2-CAN-gateway/m-p/1727954#M4861</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-09-22T09:57:25Z</dc:date>
    </item>
  </channel>
</rss>