<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Uboot for S32G3 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1724424#M4826</link>
    <description>&lt;P&gt;Hi Aswini,&lt;/P&gt;&lt;P&gt;fip image is combination of multiple images like ATF (BL2+BL31+BL33). once u boot binary is generated.&lt;/P&gt;&lt;P&gt;feed it to ATF during compilation which will generate final fip image.&lt;/P&gt;</description>
    <pubDate>Mon, 18 Sep 2023 05:47:10 GMT</pubDate>
    <dc:creator>yellapu_anishkh</dc:creator>
    <dc:date>2023-09-18T05:47:10Z</dc:date>
    <item>
      <title>'initsram' command in Uboot</title>
      <link>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1709948#M4539</link>
      <description>&lt;P&gt;The command initsram in uboot is not working for initializing the memory region for the SRAM for M7 in NXPS32G3rdb3 board.Could you pls provide the alternative command for this, or explain how to enable this command in Uboot&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 13:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1709948#M4539</guid>
      <dc:creator>aswinknp</dc:creator>
      <dc:date>2023-08-23T13:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: 'initsram' command in Uboot</title>
      <link>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1710319#M4546</link>
      <description>&lt;P&gt;Hi Aswin,&lt;/P&gt;&lt;P&gt;With latest BSP, this is not required in uboot, as it is already initialized previous build stages.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 05:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1710319#M4546</guid>
      <dc:creator>yellapu_anishkh</dc:creator>
      <dc:date>2023-08-24T05:42:26Z</dc:date>
    </item>
    <item>
      <title>Uboot for S32G3</title>
      <link>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1722731#M4783</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've taken the U-Boot source code from NXP and I've updated the code for my use case.&lt;BR /&gt;Compiled the source code using readme file and able to generate .bin file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At the time of testing found that fip.s32-qspi is required. But we're not sure&amp;nbsp;&lt;BR /&gt;how to generate/build this file. could you pls support here for building file fip.s32-qspi?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 05:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1722731#M4783</guid>
      <dc:creator>aswinknp</dc:creator>
      <dc:date>2023-09-14T05:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot for S32G3</title>
      <link>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1724424#M4826</link>
      <description>&lt;P&gt;Hi Aswini,&lt;/P&gt;&lt;P&gt;fip image is combination of multiple images like ATF (BL2+BL31+BL33). once u boot binary is generated.&lt;/P&gt;&lt;P&gt;feed it to ATF during compilation which will generate final fip image.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 05:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/initsram-command-in-Uboot/m-p/1724424#M4826</guid>
      <dc:creator>yellapu_anishkh</dc:creator>
      <dc:date>2023-09-18T05:47:10Z</dc:date>
    </item>
  </channel>
</rss>