<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Some questions about LLCE</title>
    <link>https://community.nxp.com/t5/S32G/Some-questions-about-LLCE/m-p/1720601#M4747</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222587"&gt;@pole&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;1.LLCE can it only be deployed on AutoSar platforms?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Could you elaborate more the question, the examples provided are created for EBT and design studio.&lt;/P&gt;
&lt;P&gt;Also, the S32G LLCE getting started guide chapter 1.2 states that a set of Autosar compatible drivers are provided in the same package as the firmware. These drivers are designed to integrate with the NXP RTD suite and resemble to a degree the corresponding RTD drivers&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;2.Why CAN only 4 channels be configured on the S32G2 Drivers configuration page?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Are you refering to the FlexCAN module or the LLCE BCAN interfaces? The FlexCan module has 4 configurable instances and the LLCE module has 16 BCAN interfaces.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;3.If I do not use the Autosar platform and use LLCE to complete CAN2CAN functionality, what do I need to do?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Can you tell me more of your approach? I think that the examples provided on the S32G's software package can help you, you can refer to them too.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;4.Is the source code for LLCE in the installation directory? I only read in the guide article how to deploy LLCE using EB Tresos.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The LLCE runs its own software. This is provided in two variants – Standard (binary) and FDK (Firmware Development Kit). The FDK provides more functionality, and comes with the source code, allowing for customization and extension of the code run by LLCE. I must say that if you want the FDK, help us contacting your local NXP FAE/DFAE, since this is a premium software.&lt;/P&gt;
&lt;P&gt;I hope this information helps you.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Sep 2023 20:51:51 GMT</pubDate>
    <dc:creator>Miguel04</dc:creator>
    <dc:date>2023-09-11T20:51:51Z</dc:date>
    <item>
      <title>Some questions about LLCE</title>
      <link>https://community.nxp.com/t5/S32G/Some-questions-about-LLCE/m-p/1720001#M4736</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We use S32G2 for gateway development but we have some questions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1.LLCE can it only be deployed on AutoSar platforms?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.Why CAN only 4 channels be configured on the S32G2 Drivers configuration page?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.If I do not use the Autosar platform and use LLCE to complete CAN2CAN functionality, what do I need to do?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4.Is the source code for LLCE in the installation directory? I only read in the guide article how to deploy LLCE using EB Tresos.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope you can take the time to answer my questions!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Thank you!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 05:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Some-questions-about-LLCE/m-p/1720001#M4736</guid>
      <dc:creator>pole</dc:creator>
      <dc:date>2023-09-11T05:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: Some questions about LLCE</title>
      <link>https://community.nxp.com/t5/S32G/Some-questions-about-LLCE/m-p/1720601#M4747</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222587"&gt;@pole&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;1.LLCE can it only be deployed on AutoSar platforms?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Could you elaborate more the question, the examples provided are created for EBT and design studio.&lt;/P&gt;
&lt;P&gt;Also, the S32G LLCE getting started guide chapter 1.2 states that a set of Autosar compatible drivers are provided in the same package as the firmware. These drivers are designed to integrate with the NXP RTD suite and resemble to a degree the corresponding RTD drivers&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;2.Why CAN only 4 channels be configured on the S32G2 Drivers configuration page?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Are you refering to the FlexCAN module or the LLCE BCAN interfaces? The FlexCan module has 4 configurable instances and the LLCE module has 16 BCAN interfaces.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;3.If I do not use the Autosar platform and use LLCE to complete CAN2CAN functionality, what do I need to do?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Can you tell me more of your approach? I think that the examples provided on the S32G's software package can help you, you can refer to them too.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;4.Is the source code for LLCE in the installation directory? I only read in the guide article how to deploy LLCE using EB Tresos.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The LLCE runs its own software. This is provided in two variants – Standard (binary) and FDK (Firmware Development Kit). The FDK provides more functionality, and comes with the source code, allowing for customization and extension of the code run by LLCE. I must say that if you want the FDK, help us contacting your local NXP FAE/DFAE, since this is a premium software.&lt;/P&gt;
&lt;P&gt;I hope this information helps you.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 20:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Some-questions-about-LLCE/m-p/1720601#M4747</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-09-11T20:51:51Z</dc:date>
    </item>
  </channel>
</rss>