<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [S32G274 RDB2] [IPCF 4.6] M7 start success，linux kernel panic in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G274-RDB2-IPCF-4-6-M7-start-success-linux-kernel-panic/m-p/1716321#M4670</link>
    <description>Hello, has this been resolved? I also encountered the same problem</description>
    <pubDate>Mon, 04 Sep 2023 08:04:35 GMT</pubDate>
    <dc:creator>tianwei</dc:creator>
    <dc:date>2023-09-04T08:04:35Z</dc:date>
    <item>
      <title>[S32G274 RDB2] [IPCF 4.6] M7 start success，linux kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-RDB2-IPCF-4-6-M7-start-success-linux-kernel-panic/m-p/1645095#M3098</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I download BSP35.0，and reference&amp;nbsp;SW32G_IPCF_4.6.0_D2205_UserManual.pdf，add the IPCF feature in&amp;nbsp; Image，&amp;nbsp; and the image has been built successful.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; This image has been burned to SD card，and image can be start normally.(Not hit anykey after power on the RDB2 board)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; But when I boot M7(bin file is IPCF_Example_S32G274A_M7_0.bin),and then boot linux,the kernel panic,how can i slove this problom.&lt;/P&gt;&lt;P&gt;IPCF UserManual:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NicholasZheng_0-1683249300484.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/221872i8E08DA5D2AA8ED9D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="NicholasZheng_0-1683249300484.png" alt="NicholasZheng_0-1683249300484.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;NicholasZheng_0-1683249300484.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Error Serial log:&lt;/P&gt;&lt;P&gt;=&amp;gt; startm7 0x34501000&lt;BR /&gt;Starting CM7_0 core at SRAM address 0x34501000 ... done.&lt;BR /&gt;=&amp;gt; boot&lt;BR /&gt;PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2&lt;BR /&gt;PFE: emac0: sgmii emac1: none emac2: rgmii&lt;BR /&gt;pfeng_cfg_mode_enable: Invalid PFE device&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;13758472 bytes read in 624 ms (21 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;44501 bytes read in 21 ms (2 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 0000000083000000, end 000000008300ddd4&lt;BR /&gt;fixup: pfe0 set to 00:01:be:be:ef:11&lt;BR /&gt;fixup: pfe1 set to 00:01:be:be:ef:22&lt;BR /&gt;fixup: pfe2 set to 00:01:be:be:ef:33&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 5.10.145-rt74+g1594b25154a2 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 SMP PREEMPT Tue Nov 29 10:33:39 UTC 2022&lt;BR /&gt;[ 0.000000] Machine model: NXP S32G274A-RDB2&lt;BR /&gt;[ 0.000000] earlycon: linflex0 at MMIO 0x00000000401c8000 (options '115200n8')&lt;BR /&gt;[ 0.000000] printk: bootconsole [linflex0] enabled&lt;BR /&gt;[ 0.000000] SError Interrupt on CPU0, code 0xbf000000 -- SError&lt;BR /&gt;[ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 5.10.145-rt74+g1594b25154a2 #1&lt;BR /&gt;[ 0.000000] Hardware name: NXP S32G274A-RDB2 (DT)&lt;BR /&gt;[ 0.000000] pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 0.000000] pc : setup_arch+0x164/0x58c&lt;BR /&gt;[ 0.000000] lr : setup_arch+0x15c/0x58c&lt;BR /&gt;[ 0.000000] sp : ffffffc010c83ef0&lt;BR /&gt;[ 0.000000] x29: ffffffc010c83ef0 x28: 0000000080b40018&lt;BR /&gt;[ 0.000000] x27: 00000000ffaa27f8 x26: 0000000000000000&lt;BR /&gt;[ 0.000000] x25: 00000000ffb39a20 x24: 00000000ffe03f18&lt;BR /&gt;[ 0.000000] x23: ffffffc010d23000 x22: ffffffc010c8e380&lt;BR /&gt;[ 0.000000] x21: fffffffefe600094 x20: ffffffc010cd7158&lt;BR /&gt;[ 0.000000] x19: ffffffc010000000 x18: 0000000000000030&lt;BR /&gt;[ 0.000000] x17: 0000000000001800 x16: 0000000000000000&lt;BR /&gt;[ 0.000000] x15: ffffffc010c8e7e8 x14: ffffffffffffffff&lt;BR /&gt;[ 0.000000] x13: 0000000000000000 x12: 0000000000000028&lt;BR /&gt;[ 0.000000] x11: 0000000000000015 x10: 0101010101010101&lt;BR /&gt;[ 0.000000] x9 : 3334ff6b6e6e6f5e x8 : 7f7f7f7f7f7f7f7f&lt;BR /&gt;[ 0.000000] x7 : 736d647164676e62 x6 : 000006161d090b74&lt;BR /&gt;[ 0.000000] x5 : 740b091d16060000 x4 : 0000000000000000&lt;BR /&gt;[ 0.000000] x3 : ce6ded8ca0000000 x2 : 000000000000000c&lt;BR /&gt;[ 0.000000] x1 : 0000000000000000 x0 : 0000000000000080&lt;BR /&gt;[ 0.000000] Kernel panic - not syncing:&lt;BR /&gt;[ 0.000000] Asynchronous SError Interrupt&lt;BR /&gt;[ 0.000000] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 01:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-RDB2-IPCF-4-6-M7-start-success-linux-kernel-panic/m-p/1645095#M3098</guid>
      <dc:creator>NicholasZheng</dc:creator>
      <dc:date>2023-05-05T01:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: [S32G274 RDB2] [IPCF 4.6] M7 start success，linux kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-RDB2-IPCF-4-6-M7-start-success-linux-kernel-panic/m-p/1716321#M4670</link>
      <description>Hello, has this been resolved? I also encountered the same problem</description>
      <pubDate>Mon, 04 Sep 2023 08:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-RDB2-IPCF-4-6-M7-start-success-linux-kernel-panic/m-p/1716321#M4670</guid>
      <dc:creator>tianwei</dc:creator>
      <dc:date>2023-09-04T08:04:35Z</dc:date>
    </item>
  </channel>
</rss>