<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LLCE-CAN AND LLCE-LOGGER in S32G</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1716052#M4662</link>
    <description>&lt;P&gt;My BSP Version is bsp37&lt;/P&gt;</description>
    <pubDate>Sun, 03 Sep 2023 07:24:21 GMT</pubDate>
    <dc:creator>leehaonan</dc:creator>
    <dc:date>2023-09-03T07:24:21Z</dc:date>
    <item>
      <title>LLCE-CAN AND LLCE-LOGGER</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1715665#M4649</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Can llce-can and llce-logger coexist, or is it possible to switch between them in U-Boot? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have appended both features to DISTRO_FEATURES using 'DISTRO_FEATURES_append = " llce-can llce-logger "', but when I run 'ifconfig -a', I find that llce-can is still the default&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Sep 2023 08:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1715665#M4649</guid>
      <dc:creator>leehaonan</dc:creator>
      <dc:date>2023-09-01T08:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE-CAN AND LLCE-LOGGER</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1715920#M4659</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;With which BSP version are you working with? Under BSP33.0, the following is told:&lt;/P&gt;
&lt;P&gt;"The driver is able to operate in two modes: along with Linux LLCE CAN driver or in scenarios where the LLCE CAN host management is part of an another software stack."&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Sep 2023 17:23:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1715920#M4659</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-09-01T17:23:00Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE-CAN AND LLCE-LOGGER</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1716052#M4662</link>
      <description>&lt;P&gt;My BSP Version is bsp37&lt;/P&gt;</description>
      <pubDate>Sun, 03 Sep 2023 07:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1716052#M4662</guid>
      <dc:creator>leehaonan</dc:creator>
      <dc:date>2023-09-03T07:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE-CAN AND LLCE-LOGGER</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1716643#M4678</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We understand that the LLCE logger should be enabled under the "advanced/premium" LLCE-FW. Can you share the output of the following command?:&lt;/P&gt;
&lt;P&gt;dmesg | grep llce&lt;/P&gt;
&lt;P&gt;Under our setup, we see the following output:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1693862920823.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/239441iBAA89C2278D0CE43/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1693862920823.png" alt="DanielAguirre_0-1693862920823.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Which is because we are using the standard LLCE-FW.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 21:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-CAN-AND-LLCE-LOGGER/m-p/1716643#M4678</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-09-04T21:29:28Z</dc:date>
    </item>
  </channel>
</rss>