<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: LLCE on M7 stop unexpectly while A53 start u-boot</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1714447#M4619</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;When you say "&lt;SPAN&gt;I didn't enable LLCE CAN or specify the location where firmware binaries on A53&lt;/SPAN&gt;", we understand that you are not using the pre-built BSP by NXP, is this correct?&lt;/P&gt;
&lt;P&gt;As for additional guidance, we can recommend also looking into AN13750 which details an application with M7_0 + M7_1 + M7_2 + A53. The linker being used under the M7 application is different than the one being explained under the "&lt;SPAN&gt;S32G_Bootloader_V2-2022.1024_eng.pdf&lt;/SPAN&gt;" file.&lt;/P&gt;
&lt;P&gt;You could verify if the steps you are following are similar to the ones explained under AN13750 and verify if using the M7 app linker could provide any difference.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 22:37:11 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-08-30T22:37:11Z</dc:date>
    <item>
      <title>LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1711876#M4572</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use can_mcal_can2can example and run on M7, it can run normally only on M7_0.&lt;/P&gt;&lt;P&gt;But when I tried to boot M7 and A53 at the same time, I met a problem that M7 would stop work while A53 started u-boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Info:&lt;/P&gt;&lt;P&gt;1. The board is S32G274ARDB2. LLCE version: 1.0.4. RTD version: 3.0.2 HF01. Platform Software Integration: 2022_06. BSP version: 34.&lt;/P&gt;&lt;P&gt;2. I refer to S32G_Bootloader_V2-2022.1024_eng.pdf to configure bootloader.&lt;/P&gt;&lt;P&gt;3. As UART demo, I disable “Mcu Init Clock API”&amp;nbsp;and “Port”&amp;nbsp;in “Sample_App_LLCE_CAN2CAN”&amp;nbsp;project, also modified app’s code:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="图片1.png" style="width: 849px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238199iDDD3E735A2C10302/image-size/large?v=v2&amp;amp;px=999" role="button" title="图片1.png" alt="图片1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="图片2.png" style="width: 948px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238200iFC8C443642330034/image-size/large?v=v2&amp;amp;px=999" role="button" title="图片2.png" alt="图片2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;4. Configure clock for MCU configuration of M7 app and bootloader.&lt;/P&gt;&lt;P&gt;Bootloader_S32G2XX_ASR_4.4_M7:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="图片3.png" style="width: 586px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238206iD8C63225D7EE1FEB/image-size/large?v=v2&amp;amp;px=999" role="button" title="图片3.png" alt="图片3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Sample_App_LLCE_CAN2CAN:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="图片4.png" style="width: 592px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238202i21D7F94DF60E0D3D/image-size/large?v=v2&amp;amp;px=999" role="button" title="图片4.png" alt="图片4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;5. Modify&amp;nbsp;sample_app_llce\llce_sample_app_af\platform_common\build_files\src\gcc\sample_app_linker_file.ld. Change the region of int_sram to&amp;nbsp;0x34400000.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="图片5.png" style="width: 894px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238207i708B2FF135440C43/image-size/large?v=v2&amp;amp;px=999" role="button" title="图片5.png" alt="图片5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The problem: M7 stopped work while A53 start u-boot.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="图片6.png" style="width: 611px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238204iB757235F816F3BD6/image-size/large?v=v2&amp;amp;px=999" role="button" title="图片6.png" alt="图片6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Question: Any other conflict between M7 and bootloader except port/clock/interrupt?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 04:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1711876#M4572</guid>
      <dc:creator>ShenYi</dc:creator>
      <dc:date>2023-08-28T04:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1712589#M4583</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Have you modified anything under the dts files? We understand that all LLCE pins are also enabled under Linux, which may cause a resource conflict.&lt;/P&gt;
&lt;P&gt;Also, how do you know that the M7 stopped working? Does the A53 can continue no problem?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 19:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1712589#M4583</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-08-28T19:39:46Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1712672#M4588</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I didn't modify anything under the dts files before. And I modified Can_Driver_Sample_Test to make CONTROLLER1 keep sending messages all the time. But when UART0 printing messages below, CONTROLLER1 stopped sending messages while A53 can continue no problem.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;NOTICE: BL2: v2.5(release):bsp33.0-2.5-dirty&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;NOTICE: BL2: Built : 21:48:25, Mar 24 2023&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;NOTICE: BL2: Booting BL31&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;U-Boot 2020.04 (Mar 23 2023 - 18:15:43 -0700)&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; This time I tried to modify dts file to resolve this problem, but I failed.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; First, I modified status of "&amp;amp;llce_can0" to "&amp;amp;llce_can15" from "okay" to "disabled" in ~/linux/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi. Then remake to generate new dtb file into SD-Card.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Secondly, I modified status of "&amp;amp;llce_dte_sram" to "&amp;amp;llce_boot_status" from "okay" to "disabled" too.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Finally, I modified "s32g.dtsi" which has config "llce_canX_pins".&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; However, the problem still exists.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, are my these changes correct? And I have met the problem before A53 "Load and exeDTB &amp;amp; Kernel" accordint to AN13750.pdf, is it possible that m7 app and fip.bin conflict?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 09:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1712672#M4588</guid>
      <dc:creator>ShenYi</dc:creator>
      <dc:date>2023-08-29T09:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1713515#M4602</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;Could be a problem of LLCE FW being loaded 2 times, have you eliminated the LLCE loading from Linux? The following thread may provide insight on this:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/How-to-make-LLCE-CAN-work-on-M7-for-multiboot-M7-A53/m-p/1711562/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExMUVI3TVk0T0ZRMjcxfDE3MTE1NjJ8U1VCU0NSSVBUSU9OU3xoSw#M4567" target="_blank"&gt;Re: How to make LLCE_CAN work on M7 for multiboot ... - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, can you confirm if loading a simple blink provides the same outcome? To discard the modifications to the linker.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 22:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1713515#M4602</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-08-29T22:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1713573#M4604</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I didn't enable LLCE CAN or specify the location where firmware binaries on A53. So it's unlikely to be the problem of LLCE FW being loaded 2 times.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; And I have already completed the UART example (M7 + A53) successfully refer to S32G_Bootloader_V2-2022.1024_eng.pdf before. Same to LLCE example, I modifyied the link file in which the region of int_sram changed from 0x34000000 to 0x34400000.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; However, I still think maybe there is conflict between M7 app and fip.bin. Because S32G is at Booting BL31 or U-Boot when M7 stopped sending CAN messages, which time Linux hasn't boot yet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; But I have no idea what conflict it is, could you give me a little &lt;SPAN&gt;guidance&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 01:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1713573#M4604</guid>
      <dc:creator>ShenYi</dc:creator>
      <dc:date>2023-08-30T01:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1714447#M4619</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;When you say "&lt;SPAN&gt;I didn't enable LLCE CAN or specify the location where firmware binaries on A53&lt;/SPAN&gt;", we understand that you are not using the pre-built BSP by NXP, is this correct?&lt;/P&gt;
&lt;P&gt;As for additional guidance, we can recommend also looking into AN13750 which details an application with M7_0 + M7_1 + M7_2 + A53. The linker being used under the M7 application is different than the one being explained under the "&lt;SPAN&gt;S32G_Bootloader_V2-2022.1024_eng.pdf&lt;/SPAN&gt;" file.&lt;/P&gt;
&lt;P&gt;You could verify if the steps you are following are similar to the ones explained under AN13750 and verify if using the M7 app linker could provide any difference.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 22:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1714447#M4619</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-08-30T22:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE on M7 stop unexpectly while A53 start u-boot</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1714827#M4626</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your reply. I have found the reason that CAN_PE_CLK conflict between ATF and M7 which caused baudrate of LLCE_CAN been changed not as expected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 08:29:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-on-M7-stop-unexpectly-while-A53-start-u-boot/m-p/1714827#M4626</guid>
      <dc:creator>ShenYi</dc:creator>
      <dc:date>2023-08-31T08:29:20Z</dc:date>
    </item>
  </channel>
</rss>