<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックHow can I boot to the SDCard using the M7 binary?</title>
    <link>https://community.nxp.com/t5/S32G/How-can-I-boot-to-the-SDCard-using-the-M7-binary/m-p/1403228#M449</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I am using the S32G274ARDB board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Referring to "03. Light Up RGB LED Based On Real Time Drivers" in the "S32G-VNP-GLDBOX Software Enablement Guide" document, the UART operation test program was created and the operation was confirmed using the S32 Debug Probe.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And like the guide document, the SDCard image was created, and the operation was checked after writing the image to the SDCard, but it did not work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you help us with what we're missing and the checkpoints?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 21 Jan 2022 12:08:13 GMT</pubDate>
    <dc:creator>ljy</dc:creator>
    <dc:date>2022-01-21T12:08:13Z</dc:date>
    <item>
      <title>How can I boot to the SDCard using the M7 binary?</title>
      <link>https://community.nxp.com/t5/S32G/How-can-I-boot-to-the-SDCard-using-the-M7-binary/m-p/1403228#M449</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am using the S32G274ARDB board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Referring to "03. Light Up RGB LED Based On Real Time Drivers" in the "S32G-VNP-GLDBOX Software Enablement Guide" document, the UART operation test program was created and the operation was confirmed using the S32 Debug Probe.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And like the guide document, the SDCard image was created, and the operation was checked after writing the image to the SDCard, but it did not work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you help us with what we're missing and the checkpoints?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 12:08:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-can-I-boot-to-the-SDCard-using-the-M7-binary/m-p/1403228#M449</guid>
      <dc:creator>ljy</dc:creator>
      <dc:date>2022-01-21T12:08:13Z</dc:date>
    </item>
    <item>
      <title>Re: How can I boot to the SDCard using the M7 binary?</title>
      <link>https://community.nxp.com/t5/S32G/How-can-I-boot-to-the-SDCard-using-the-M7-binary/m-p/1405060#M469</link>
      <description>&lt;P&gt;I'm assuming the board in question in S32G-VNP-RDB2, not S32G274ARDB, which is&lt;BR /&gt;an invalid part number. There is a document specific to your board which &lt;BR /&gt;describes exactly what you want - boot S32G2 M7 core from an SD card&amp;nbsp;directly &lt;BR /&gt;into an application created in S32DS:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32G-VNP-RDB2-SW-UG" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32G-VNP-RDB2-SW-UG&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you want to create a workable demo for an M7 SD card boot, all that you need &lt;BR /&gt;is to follow it strictly. The same slides discussing IVT, DCD and the linker file&lt;BR /&gt;give you the checkpoints for a modified code. If you changed the demo code and it&lt;BR /&gt;fails with with your modifications, you have to&amp;nbsp; debug it. See S32DS User Guide, &lt;BR /&gt;section titled "Debugging with S32 Debug Probe from flash for all other targets" &lt;BR /&gt;on page 100.&lt;/P&gt;
&lt;P&gt;Additional information on the bootable SD card image layout and SD card boot &lt;BR /&gt;flow can be found in S32G2RM, Sections 30.4 and 30.13.2&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 09:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-can-I-boot-to-the-SDCard-using-the-M7-binary/m-p/1405060#M469</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2022-01-26T09:31:55Z</dc:date>
    </item>
  </channel>
</rss>