<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to Configure a Static IP in S32G2 BSP37 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/How-to-Configure-a-Static-IP-in-S32G2-BSP37/m-p/1701648#M4401</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In doc "&lt;STRONG&gt;S32G-VNP-RDB2 Ethernet Enablement.pdf&lt;/STRONG&gt;"：6. Ethernet Port Enablement&lt;/P&gt;&lt;P&gt;GMAC&lt;/P&gt;&lt;P&gt;&amp;nbsp;ifconfig eth0 192.168.1.20&lt;/P&gt;&lt;P&gt;It do works,i can ping my pc.&lt;SPAN&gt;But how do I automatically configure eth0 with a specific static IP after the system starts up。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In doc "&lt;STRONG&gt;S32G2_LinuxBSP_35.0_User_Manual_updated_D230119.pdf&lt;/STRONG&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Set the CAN interfaces:&lt;BR /&gt;– Set the bitrate of can0 and can1 interfaces to 500kbps:&lt;BR /&gt;ip link set can0 type can bitrate 500000&lt;BR /&gt;ip link set can1 type can bitrate 500000&lt;BR /&gt;– Start the can interfaces like a standard net interface:&lt;BR /&gt;ip link set can0 up&lt;BR /&gt;ip link set can1 up&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I got the same question.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And can you tell me hao to find the bsp doc of bsp37?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Aug 2023 06:58:56 GMT</pubDate>
    <dc:creator>leehaonan</dc:creator>
    <dc:date>2023-08-09T06:58:56Z</dc:date>
    <item>
      <title>How to Configure a Static IP in S32G2 BSP37</title>
      <link>https://community.nxp.com/t5/S32G/How-to-Configure-a-Static-IP-in-S32G2-BSP37/m-p/1701648#M4401</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In doc "&lt;STRONG&gt;S32G-VNP-RDB2 Ethernet Enablement.pdf&lt;/STRONG&gt;"：6. Ethernet Port Enablement&lt;/P&gt;&lt;P&gt;GMAC&lt;/P&gt;&lt;P&gt;&amp;nbsp;ifconfig eth0 192.168.1.20&lt;/P&gt;&lt;P&gt;It do works,i can ping my pc.&lt;SPAN&gt;But how do I automatically configure eth0 with a specific static IP after the system starts up。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In doc "&lt;STRONG&gt;S32G2_LinuxBSP_35.0_User_Manual_updated_D230119.pdf&lt;/STRONG&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Set the CAN interfaces:&lt;BR /&gt;– Set the bitrate of can0 and can1 interfaces to 500kbps:&lt;BR /&gt;ip link set can0 type can bitrate 500000&lt;BR /&gt;ip link set can1 type can bitrate 500000&lt;BR /&gt;– Start the can interfaces like a standard net interface:&lt;BR /&gt;ip link set can0 up&lt;BR /&gt;ip link set can1 up&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I got the same question.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And can you tell me hao to find the bsp doc of bsp37?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 06:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-Configure-a-Static-IP-in-S32G2-BSP37/m-p/1701648#M4401</guid>
      <dc:creator>leehaonan</dc:creator>
      <dc:date>2023-08-09T06:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to Configure a Static IP in S32G2 BSP37</title>
      <link>https://community.nxp.com/t5/S32G/How-to-Configure-a-Static-IP-in-S32G2-BSP37/m-p/1702156#M4411</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The following community thread talks about setting an static IP under the S32G platform, for both legacy and systemd init:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/How-to-Debug-Serdes-SGMII/m-p/1670689" target="_blank"&gt;Solved: How to Debug Serdes SGMII - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 17:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-Configure-a-Static-IP-in-S32G2-BSP37/m-p/1702156#M4411</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-08-09T17:35:44Z</dc:date>
    </item>
  </channel>
</rss>