<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックWhether the IPCF user space code supports multiple instances?</title>
    <link>https://community.nxp.com/t5/S32G/Whether-the-IPCF-user-space-code-supports-multiple-instances/m-p/1691960#M4193</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Does the IPCF user state code support multiple instances?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I see finit_module in the os_init function, and as far as I know, each ipc-shm-uio.ko only allows finit_module once.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Looking forward to reply!&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jul 2023 07:00:57 GMT</pubDate>
    <dc:creator>jiahaisheng</dc:creator>
    <dc:date>2023-07-25T07:00:57Z</dc:date>
    <item>
      <title>Whether the IPCF user space code supports multiple instances?</title>
      <link>https://community.nxp.com/t5/S32G/Whether-the-IPCF-user-space-code-supports-multiple-instances/m-p/1691960#M4193</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Does the IPCF user state code support multiple instances?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I see finit_module in the os_init function, and as far as I know, each ipc-shm-uio.ko only allows finit_module once.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Looking forward to reply!&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 07:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Whether-the-IPCF-user-space-code-supports-multiple-instances/m-p/1691960#M4193</guid>
      <dc:creator>jiahaisheng</dc:creator>
      <dc:date>2023-07-25T07:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: Whether the IPCF user space code supports multiple instances?</title>
      <link>https://community.nxp.com/t5/S32G/Whether-the-IPCF-user-space-code-supports-multiple-instances/m-p/1692414#M4207</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We may not be understanding the overall request, if so we apologize.&lt;/P&gt;
&lt;P&gt;Under the AN13750 available under the S32G2 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g2-processors-for-vehicle-networking:S32G2" target="_blank"&gt;S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;) a multi-instance IPCF application is implemented, where 3 M7 cores and the A53 cluster are used. Since the A53 is running linux, we suppose that it supports the multi-instance application.&lt;/P&gt;
&lt;P&gt;For BSP33.0 (which is the ones being used under the AN) there is a required patch for IPCF multi-instance, which is also provided under the AN13750SW package under the S32G2 product page.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 17:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Whether-the-IPCF-user-space-code-supports-multiple-instances/m-p/1692414#M4207</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-07-25T17:39:49Z</dc:date>
    </item>
  </channel>
</rss>