<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32g274ardb2-GOLDVIP. Necessary feature in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1690774#M4177</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204248"&gt;@MayanksPatel&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When we removed optional feature, the size is still more than 3GB and there are lots of unused packages inside our images.&lt;/P&gt;&lt;P&gt;Also we removed both all optional feature and all required feature, the size of image is 2.5GB-3GB&amp;nbsp;and there are lots of unused packages inside our images.&lt;/P&gt;&lt;P&gt;Below are my options What is your suggestion when we want to add some feature?&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)Modify goldvip source code depends on our board(Remove unused optional packages)Disadvantage the size of image is around 2.5GB, there are lots of unused packages&lt;/P&gt;&lt;P&gt;2) Extract the feature which we want to use and add it to our source code. Disadvantage it is compicated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Sun, 23 Jul 2023 12:06:12 GMT</pubDate>
    <dc:creator>irfank</dc:creator>
    <dc:date>2023-07-23T12:06:12Z</dc:date>
    <item>
      <title>S32g274ardb2-GOLDVIP. Necessary feature</title>
      <link>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1686602#M4103</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;There are some required features and optional features under fsl-goldvip.conf.&amp;nbsp; &amp;nbsp;Can i deleted required features. Can you explain one-by-one why do i need required features?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Required features are :&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;DISTRO_FEATURES_append&lt;/SPAN&gt;&lt;SPAN&gt; = &lt;/SPAN&gt;&lt;SPAN&gt;" pfe"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;DISTRO_FEATURES_append&lt;/SPAN&gt;&lt;SPAN&gt; = &lt;/SPAN&gt;&lt;SPAN&gt;" xen"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;DISTRO_FEATURES_append&lt;/SPAN&gt;&lt;SPAN&gt; = &lt;/SPAN&gt;&lt;SPAN&gt;" bridge_utils"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;XEN_EXAMPLE&lt;/SPAN&gt;&lt;SPAN&gt; = &lt;/SPAN&gt;&lt;SPAN&gt;"xen-examples-goldvip"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Also, There are 2 extra layers, meta-java and meta-aws. What is the purpose of these layers?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Also, can you explain what is the purpose of optional feature, required feature and meta-java and meta-aws. What is the relationship between them?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;SPAN&gt;if i want to use ONLY fota feature. Can i delete meta-java, meta-aws, and required feature, then can i add only&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;" goldvip-ota". Is it enough?&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 12 Jul 2023 11:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1686602#M4103</guid>
      <dc:creator>irfank</dc:creator>
      <dc:date>2023-07-12T11:45:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32g274ardb2-GOLDVIP. Necessary feature</title>
      <link>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1687544#M4131</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212774"&gt;@irfank&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;PFE is the hardware accelerator for incoming and outgoing frames through ethernet and can.&lt;/P&gt;
&lt;P&gt;It is fine you can skip this for the OTA feature.&lt;/P&gt;
&lt;P&gt;Xen is a hypervisor that helps to create virtualization of board resources and by default added support in the GOLD VIP release. Need to check whether g&lt;SPAN&gt;oldvip-ota is using virtualization or not.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There was an Xen hypervisor sample example provided with the release.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;meta-java and meta-aws layers you need to keep because, for the OTA feature, you will be required those.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Mayank s Patel&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jul 2023 11:56:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1687544#M4131</guid>
      <dc:creator>MayanksPatel</dc:creator>
      <dc:date>2023-07-13T11:56:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32g274ardb2-GOLDVIP. Necessary feature</title>
      <link>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1690774#M4177</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204248"&gt;@MayanksPatel&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When we removed optional feature, the size is still more than 3GB and there are lots of unused packages inside our images.&lt;/P&gt;&lt;P&gt;Also we removed both all optional feature and all required feature, the size of image is 2.5GB-3GB&amp;nbsp;and there are lots of unused packages inside our images.&lt;/P&gt;&lt;P&gt;Below are my options What is your suggestion when we want to add some feature?&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)Modify goldvip source code depends on our board(Remove unused optional packages)Disadvantage the size of image is around 2.5GB, there are lots of unused packages&lt;/P&gt;&lt;P&gt;2) Extract the feature which we want to use and add it to our source code. Disadvantage it is compicated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Sun, 23 Jul 2023 12:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1690774#M4177</guid>
      <dc:creator>irfank</dc:creator>
      <dc:date>2023-07-23T12:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: S32g274ardb2-GOLDVIP. Necessary feature</title>
      <link>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1691911#M4190</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212774"&gt;@irfank&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;We understand that there are lots of packages inside the GOLDVIP BSP release and we provided support for that packages in demand from customers.&lt;/P&gt;
&lt;P&gt;We suggest you that, list down packages that you think are unnecessary by analyzing your project requirement and proceed to remove those from the yocto project.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Mayank s Patel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 06:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32g274ardb2-GOLDVIP-Necessary-feature/m-p/1691911#M4190</guid>
      <dc:creator>MayanksPatel</dc:creator>
      <dc:date>2023-07-25T06:02:56Z</dc:date>
    </item>
  </channel>
</rss>