<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to access UART1 (dev/ttyLF1) in Linux (A-Core) in S32G</title>
    <link>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1685243#M4070</link>
    <description>&lt;P&gt;Hi nxf92355,&lt;/P&gt;&lt;P&gt;I use BSP_33.0.&lt;/P&gt;&lt;P&gt;I tyied to modify the console environment variable as ttyLF1 in u-boot, than booted to kernel.&lt;/P&gt;&lt;P&gt;But the console still used UART0, although the /sys/class/tty/ttyLF1/console was "Y".&lt;/P&gt;&lt;P&gt;We just want to verify the function of UART1, no matter using A53 or M7.&lt;/P&gt;&lt;P&gt;We have tried to print string through UART1 using M7, but that just verified TX of UART1.&lt;/P&gt;&lt;P&gt;Are there any documents about simple examples to verify RX of UART1 using M7?&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jul 2023 01:22:19 GMT</pubDate>
    <dc:creator>ZeusChen</dc:creator>
    <dc:date>2023-07-11T01:22:19Z</dc:date>
    <item>
      <title>How to access UART1 (dev/ttyLF1) in Linux (A-Core)</title>
      <link>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1683659#M4044</link>
      <description>&lt;P&gt;Hi NXP Community,&lt;/P&gt;&lt;P&gt;I want to verify the UART1 on our board (referenced&amp;nbsp;S32G-VNP-RDB2) in Linux System.&lt;/P&gt;&lt;P&gt;As I execute "echo "XXX" &amp;gt; /dev/ttyLF1", I could not probe the signal on UATR1 TXD.&lt;/P&gt;&lt;P&gt;I could not&amp;nbsp;&lt;SPAN&gt;communicate with other PC using minicom through UART1 either.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How could I verify the UART1 in&amp;nbsp;Linux System?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Or UART1 is used by M-Core only?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 05:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1683659#M4044</guid>
      <dc:creator>ZeusChen</dc:creator>
      <dc:date>2023-07-07T05:55:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to access UART1 (dev/ttyLF1) in Linux (A-Core)</title>
      <link>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1684936#M4064</link>
      <description>&lt;P&gt;Hi Liang-Chou Chen&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well&lt;/P&gt;
&lt;P&gt;Can you tell us which bsp version you are using ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards ,&lt;/P&gt;
&lt;P&gt;Tushar&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 13:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1684936#M4064</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-07-10T13:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to access UART1 (dev/ttyLF1) in Linux (A-Core)</title>
      <link>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1685243#M4070</link>
      <description>&lt;P&gt;Hi nxf92355,&lt;/P&gt;&lt;P&gt;I use BSP_33.0.&lt;/P&gt;&lt;P&gt;I tyied to modify the console environment variable as ttyLF1 in u-boot, than booted to kernel.&lt;/P&gt;&lt;P&gt;But the console still used UART0, although the /sys/class/tty/ttyLF1/console was "Y".&lt;/P&gt;&lt;P&gt;We just want to verify the function of UART1, no matter using A53 or M7.&lt;/P&gt;&lt;P&gt;We have tried to print string through UART1 using M7, but that just verified TX of UART1.&lt;/P&gt;&lt;P&gt;Are there any documents about simple examples to verify RX of UART1 using M7?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 01:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1685243#M4070</guid>
      <dc:creator>ZeusChen</dc:creator>
      <dc:date>2023-07-11T01:22:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to access UART1 (dev/ttyLF1) in Linux (A-Core)</title>
      <link>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1685530#M4077</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi Liang-Chou Chen&lt;/P&gt;&lt;P&gt;Yes,&amp;nbsp; There are a uart example for M7 in S32ds. &lt;FONT color="#000000"&gt;&lt;SPAN class=""&gt;Uart_Example_S32G274A_M7&lt;/SPAN&gt;&lt;/FONT&gt; this example&lt;/P&gt;&lt;P&gt;uses uart1 and tx rx. read d&lt;SPAN class=""&gt;escription.txt file of this example. let us know for more quarry&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards ,&lt;/P&gt;&lt;P&gt;Tushar&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 11 Jul 2023 07:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-access-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1685530#M4077</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-07-11T07:31:00Z</dc:date>
    </item>
  </channel>
</rss>