<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G-VNP-RDB2 Ethernet Enablement Guide test Ethernet question</title>
    <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Ethernet-Enablement-Guide-test-Ethernet-question/m-p/1399594#M405</link>
    <description>&lt;P&gt;For all cases where ping works in one direction but not in the opposite, you&lt;BR /&gt;are either pinging the board running u-Boot which does not respond to ICMP, or using an&lt;BR /&gt;invalid IP configuration or diagnostic tool. The standard ping&lt;BR /&gt;utility requires bidirectional communication to report a success. If you &lt;BR /&gt;ping successfully in one direction, the both directions are working. Everything&lt;BR /&gt;else is a result of either filtering, invalid configuration or improper &lt;BR /&gt;diagnostic tool.&lt;/P&gt;
&lt;P&gt;Regarding what you called "router tests" it is especially unclear what was&lt;BR /&gt;the purpose of testing against a port marked as "down". Do you expect &lt;BR /&gt;Linux to forward a packet to a port that is disconnected from it's IP stack?&lt;BR /&gt;Anyway, I would suggest starting with checking that packet forwarding &lt;BR /&gt;is enabled:&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;cat /proc/sys/net/ipv4/ip_forward&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;and checking the ICMP errors returned by the board to the source of the test&lt;BR /&gt;traffic.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jan 2022 17:52:52 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2022-01-14T17:52:52Z</dc:date>
    <item>
      <title>S32G-VNP-RDB2 Ethernet Enablement Guide test Ethernet question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Ethernet-Enablement-Guide-test-Ethernet-question/m-p/1399270#M403</link>
      <description>&lt;P&gt;Hi NXP TechSupport&lt;BR /&gt;My Board : S32g274ardb2&lt;BR /&gt;According this file "VNPRDBEEUG.pdf(S32G-VNP-RDB2 Ethernet Enablement Guide)" and I follow page 12 to test each port.&lt;BR /&gt;(1)The information of linux version is "Auto Linux BSP 30.0 s32g274ardb2 ttyLF0"&lt;BR /&gt;(2)PC PING Board and Board PING PC . The attach file is the test result.&lt;BR /&gt;(3)Port to Port test(router test). The attach file is the test result.&lt;/P&gt;&lt;P&gt;Can you help me to giver the answer the fail state ?&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 05:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Ethernet-Enablement-Guide-test-Ethernet-question/m-p/1399270#M403</guid>
      <dc:creator>tzeng015</dc:creator>
      <dc:date>2022-01-14T05:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 Ethernet Enablement Guide test Ethernet question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Ethernet-Enablement-Guide-test-Ethernet-question/m-p/1399594#M405</link>
      <description>&lt;P&gt;For all cases where ping works in one direction but not in the opposite, you&lt;BR /&gt;are either pinging the board running u-Boot which does not respond to ICMP, or using an&lt;BR /&gt;invalid IP configuration or diagnostic tool. The standard ping&lt;BR /&gt;utility requires bidirectional communication to report a success. If you &lt;BR /&gt;ping successfully in one direction, the both directions are working. Everything&lt;BR /&gt;else is a result of either filtering, invalid configuration or improper &lt;BR /&gt;diagnostic tool.&lt;/P&gt;
&lt;P&gt;Regarding what you called "router tests" it is especially unclear what was&lt;BR /&gt;the purpose of testing against a port marked as "down". Do you expect &lt;BR /&gt;Linux to forward a packet to a port that is disconnected from it's IP stack?&lt;BR /&gt;Anyway, I would suggest starting with checking that packet forwarding &lt;BR /&gt;is enabled:&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;cat /proc/sys/net/ipv4/ip_forward&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;and checking the ICMP errors returned by the board to the source of the test&lt;BR /&gt;traffic.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 17:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Ethernet-Enablement-Guide-test-Ethernet-question/m-p/1399594#M405</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2022-01-14T17:52:52Z</dc:date>
    </item>
  </channel>
</rss>