<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IPCF sample application in S32G</title>
    <link>https://community.nxp.com/t5/S32G/IPCF-sample-application/m-p/1679834#M3935</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We might be misunderstanding the request. Below will be some comments.&lt;/P&gt;
&lt;P&gt;IPCF is available on both the bare-metal application inside the M7 core (with the examples provided under the IPCF package) and linux. Under the IPCF example (the one for M7 core) a "description.txt" is provided, in which detailed steps are provided on how to run the example application.&lt;/P&gt;
&lt;P&gt;Also, which RTD/BSP versions are you using?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jun 2023 20:58:20 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-06-30T20:58:20Z</dc:date>
    <item>
      <title>IPCF sample application</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-sample-application/m-p/1679478#M3923</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I tried compiling the IPCF application framework given for NXP S32 RTD running on Cortex-M7 core of NXP S32 platform. The application was builded for bare-metal. To access the shared memory whether any other framework is required other than the&amp;nbsp;IPCF_4.6.0_D2205.&lt;/P&gt;&lt;P&gt;Also, is there any flashing procedure available for Cortex-M7 core?&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 09:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-sample-application/m-p/1679478#M3923</guid>
      <dc:creator>SriramVenkat</dc:creator>
      <dc:date>2023-06-30T09:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF sample application</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-sample-application/m-p/1679834#M3935</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We might be misunderstanding the request. Below will be some comments.&lt;/P&gt;
&lt;P&gt;IPCF is available on both the bare-metal application inside the M7 core (with the examples provided under the IPCF package) and linux. Under the IPCF example (the one for M7 core) a "description.txt" is provided, in which detailed steps are provided on how to run the example application.&lt;/P&gt;
&lt;P&gt;Also, which RTD/BSP versions are you using?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 20:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-sample-application/m-p/1679834#M3935</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-30T20:58:20Z</dc:date>
    </item>
  </channel>
</rss>