<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G PCIe Question</title>
    <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1668528#M3638</link>
    <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;Thanks for you feedback. Then, the EB Tresos example is the only documentation available on this regards. The following is told under the "readme.txt" attached to the example:&lt;/P&gt;&lt;P&gt;"Memory transaction are already enabled by the s32gep.ko module so you can start to read and write in the endpoint shared memory. For example:&lt;BR /&gt;Read:&lt;BR /&gt;devmem2 0x4800100000&lt;BR /&gt;Write:&lt;BR /&gt;devmem2 0x4800100000 w 0x12345678&lt;BR /&gt;Note that the addresses from the examples above are in the range displayed by the lspci command."&lt;/P&gt;&lt;P&gt;The above-mentioned module is provided under the EB Tresos example.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 15:38:42 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-06-13T15:38:42Z</dc:date>
    <item>
      <title>S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1665802#M3560</link>
      <description>&lt;P&gt;I am a novice PCIe user and I would like to know the following questions:&lt;/P&gt;&lt;P&gt;1. How to test PCIe?&lt;/P&gt;&lt;P&gt;2. How to read and write PCIe (when two development boards are interconnected through PCIe cables and configured as RC and EP respectively)?&lt;/P&gt;&lt;P&gt;3. How to support NTB?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 04:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1665802#M3560</guid>
      <dc:creator>Coco111</dc:creator>
      <dc:date>2023-06-08T04:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1666468#M3580</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;There is an example available for PCIe, still, the requirements are having an EVB and an RDB board for making it work.&lt;/P&gt;
&lt;P&gt;The example is available under the following path:&lt;/P&gt;
&lt;P&gt;"C:\nxp\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03\SW32_RTD_4_4_3_0_2_D2203\Pcie_TS_T40D11M30I2R0\examples\EBT\Pcie_Example_EBT_S32G274A_M7_001"&lt;/P&gt;
&lt;P&gt;The path could vary depending on the specific installation of the RTD plugins. In there, the EB Tresos project is provided, as well as the steps to follow in order to enable PCIe communication between an EVB and an RDB ("readme.txt" file).&lt;/P&gt;
&lt;P&gt;As for supporting NTB, we are not seeing anything on regards of the specific function under the provided driver. We do apologize.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 21:39:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1666468#M3580</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-08T21:39:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1666575#M3587</link>
      <description>&lt;P&gt;Thank you for your reply. I'm sorry I didn't explain it clearly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I want to know is &lt;FONT color="#FF0000"&gt;the usage in the Linux development environment&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 03:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1666575#M3587</guid>
      <dc:creator>Coco111</dc:creator>
      <dc:date>2023-06-09T03:14:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1667044#M3600</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;The only information it seems to be available for PCIe under Linux is the one provided under Chapter 9 of the BSP36.0 User Manual for S32G2 platforms. Also, Linux usage is provided under the M7 example, since one of the boards will use Linux for communication.&lt;/P&gt;
&lt;P&gt;Aside from the previously mentioned information, we did not find anything else. We do apologize.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 15:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1667044#M3600</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-09T15:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1667233#M3605</link>
      <description>&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;but&amp;nbsp; I can only obtain the bsp35 user manual. please tell me&amp;nbsp; how get the bsp36 user manual?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-06-10 18-47-06.png" style="width: 808px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227083i7513FA5E96944AEF/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2023-06-10 18-47-06.png" alt="Screenshot from 2023-06-10 18-47-06.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2023-06-10 18-47-06.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 10 Jun 2023 10:51:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1667233#M3605</guid>
      <dc:creator>Coco111</dc:creator>
      <dc:date>2023-06-10T10:51:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1667632#M3616</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;BSP35.0 also has the previously mentioned chapter 9 for PCIe support [Page 65, BSP35.0 User Manual Updated] under the provided User Manual.&lt;/P&gt;
&lt;P&gt;As for BSP36.0, it seems that you are not provided with access to that specific release. If you would like to access it, help us contacting your local NXP representative/FAE, for them to start the process of providing you with the required access.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jun 2023 17:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1667632#M3616</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-12T17:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1668060#M3627</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-06-13 15-10-47.png" style="width: 459px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227328i18217CDC4419612C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2023-06-13 15-10-47.png" alt="Screenshot from 2023-06-13 15-10-47.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2023-06-13 15-10-47.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As we can see, the content of the document is&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "enable", "scan", and "msi interrupt",&lt;BR /&gt;But &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;my question is how users can use PCIe to send/receive data&lt;/STRONG&gt; &lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;(&lt;FONT color="#FF0000"&gt;such as communication between two SoCs&lt;/FONT&gt;).&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 07:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1668060#M3627</guid>
      <dc:creator>Coco111</dc:creator>
      <dc:date>2023-06-13T07:17:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1668528#M3638</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;Thanks for you feedback. Then, the EB Tresos example is the only documentation available on this regards. The following is told under the "readme.txt" attached to the example:&lt;/P&gt;&lt;P&gt;"Memory transaction are already enabled by the s32gep.ko module so you can start to read and write in the endpoint shared memory. For example:&lt;BR /&gt;Read:&lt;BR /&gt;devmem2 0x4800100000&lt;BR /&gt;Write:&lt;BR /&gt;devmem2 0x4800100000 w 0x12345678&lt;BR /&gt;Note that the addresses from the examples above are in the range displayed by the lspci command."&lt;/P&gt;&lt;P&gt;The above-mentioned module is provided under the EB Tresos example.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 15:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1668528#M3638</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-13T15:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32G PCIe Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1670680#M3681</link>
      <description>I am busy testing the network, and I will handle it later</description>
      <pubDate>Fri, 16 Jun 2023 01:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-PCIe-Question/m-p/1670680#M3681</guid>
      <dc:creator>Coco111</dc:creator>
      <dc:date>2023-06-16T01:22:55Z</dc:date>
    </item>
  </channel>
</rss>