<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: IPCF Error: uboot stop in FCCU status</title>
    <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667810#M3620</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I think it's different .&amp;nbsp;&lt;/P&gt;&lt;P&gt;This one is to start up from QSPI flash in m7 .&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/IPCF-Example-multi-instance-S32G274-do-not-work/td-p/1666643" target="_blank"&gt;IPCF_Example_multi_instance_S32G274 do not work - NXP Community&lt;/A&gt;&amp;nbsp; start up from SD card,&amp;nbsp; we tryed two ways to test IPCF code ,but it both does not work.&lt;/P&gt;&lt;P&gt;We search the community and read the document , but we can nof find out the problem.&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 01:29:33 GMT</pubDate>
    <dc:creator>Ada_Lovelace</dc:creator>
    <dc:date>2023-06-13T01:29:33Z</dc:date>
    <item>
      <title>IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1665979#M3565</link>
      <description>&lt;P&gt;Hi,All&lt;/P&gt;&lt;P&gt;I reference the Document Number: AN13750 :&amp;nbsp;Enabling Multicore Application on S32G2&lt;BR /&gt;using S32G2 Platform Software Integration&lt;/P&gt;&lt;P&gt;Then I use BSP36.0 in &lt;SPAN&gt;S32g274ardb2,then I use the steps :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ada_Lovelace_0-1686210031773.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226795i76A53C69F3C82204/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ada_Lovelace_0-1686210031773.png" alt="Ada_Lovelace_0-1686210031773.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ada_Lovelace_0-1686210031773.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;but the uboot stop it in FCCU&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ada_Lovelace_1-1686210153849.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226796i461A5C6A5D0136A5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ada_Lovelace_1-1686210153849.png" alt="Ada_Lovelace_1-1686210153849.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ada_Lovelace_1-1686210153849.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I will show you the content in SD card&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ada_Lovelace_2-1686210407164.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226797iF199CAA8805C75AF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ada_Lovelace_2-1686210407164.png" alt="Ada_Lovelace_2-1686210407164.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ada_Lovelace_2-1686210407164.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I aslo try&amp;nbsp;binaries_auto_linux_bsp33.0_s32g2_pfe in NXP, and I write the command in uboot , uboot and kernel start up succesfully , but when I put the command:&amp;nbsp;insmod ipc-shm-sample_multi-instance.ko , it shows invaild parameter.&lt;/P&gt;&lt;P&gt;Could someone tells me how to fix it?&lt;/P&gt;&lt;P&gt;I use the the&amp;nbsp;SW32G_IPCF_4.6.0_D2205 in S32DS platform.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 07:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1665979#M3565</guid>
      <dc:creator>Ada_Lovelace</dc:creator>
      <dc:date>2023-06-08T07:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1666385#M3576</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We understand that you used the NXP provided Bootloader to boot the A53 core into Linux. If so, the IPCF instructions that are provided under the example take into account that you are booting Linux without a Bootloader. Have you verified the same steps without the NXP bootloader step? We have run the examples and did not encounter this situation.&lt;/P&gt;
&lt;P&gt;As for the BSP33.0, IPCF was not correctly compiled under the provided image. AN13750 provides the required patches for BSP33.0.&lt;/P&gt;
&lt;P&gt;We can either recommend booting directly into Linux, without the use of a bootloader, or following AN13750 steps one by one, which do not require any uboot commands.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 19:20:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1666385#M3576</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-08T19:20:33Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1666513#M3583</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am&amp;nbsp;&lt;SPAN&gt;following AN13750 steps again, try to boot from NOR flash, but when I&amp;nbsp; program the Nor-flash and insert the SD card , I found nothing in&amp;nbsp;Tera Term, it seems that it is not in linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ada_Lovelace_0-1686272227083.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226921iBDCDB84DAF7548B7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ada_Lovelace_0-1686272227083.png" alt="Ada_Lovelace_0-1686272227083.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ada_Lovelace_0-1686272227083.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ada_Lovelace_1-1686272310742.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226922i362DA7A4D38C150F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ada_Lovelace_1-1686272310742.png" alt="Ada_Lovelace_1-1686272310742.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ada_Lovelace_1-1686272310742.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; will upload the IPCF project and files , please help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 01:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1666513#M3583</guid>
      <dc:creator>Ada_Lovelace</dc:creator>
      <dc:date>2023-06-09T01:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667145#M3603</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;We have confirmed that AN13750 steps works, and we can see a Linux output under our terminal. We have confirmed this with both BSP33.0 and BSP36.0 and with M7 running an application.&lt;/P&gt;
&lt;P&gt;Are you using the BSP image as it is? Or are you setting up the patch for the FIP_ALIGN value?, which is needed. You need to build the ATF with FIP_ALIGN=64, since this is a restriction over the NXP provided bootloader.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 20:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667145#M3603</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-09T20:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667327#M3610</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;I use the&amp;nbsp;&lt;SPAN&gt;BSP image&amp;nbsp;by my own and change&amp;nbsp;FIP_ALIGN=64,but&amp;nbsp; it does not work, can you provide the BSP image for me ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jun 2023 01:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667327#M3610</guid>
      <dc:creator>Ada_Lovelace</dc:creator>
      <dc:date>2023-06-12T01:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667630#M3615</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It does seem that this has merged with the following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/IPCF-Example-multi-instance-S32G274-do-not-work/td-p/1666643" target="_blank"&gt;IPCF_Example_multi_instance_S32G274 do not work - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Is that correct?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jun 2023 17:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667630#M3615</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-12T17:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667810#M3620</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I think it's different .&amp;nbsp;&lt;/P&gt;&lt;P&gt;This one is to start up from QSPI flash in m7 .&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/IPCF-Example-multi-instance-S32G274-do-not-work/td-p/1666643" target="_blank"&gt;IPCF_Example_multi_instance_S32G274 do not work - NXP Community&lt;/A&gt;&amp;nbsp; start up from SD card,&amp;nbsp; we tryed two ways to test IPCF code ,but it both does not work.&lt;/P&gt;&lt;P&gt;We search the community and read the document , but we can nof find out the problem.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 01:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1667810#M3620</guid>
      <dc:creator>Ada_Lovelace</dc:creator>
      <dc:date>2023-06-13T01:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF Error: uboot stop in FCCU status</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1668533#M3640</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;Since the last comment was talking about asking for the BSP36.0 image, we assume that both threads were merging, we do apologize.&lt;/P&gt;
&lt;P&gt;Even though they did not merge, the comment on the above-mentioned thread provides the insight over the BSP36.0 image.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 15:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-Error-uboot-stop-in-FCCU-status/m-p/1668533#M3640</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-13T15:49:59Z</dc:date>
    </item>
  </channel>
</rss>