<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Communication between Dom0 and device connected to SJA1110 on s32g</title>
    <link>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1663447#M3509</link>
    <description>&lt;P&gt;I have connected a device to sja1110 switch on nxp s32g and got the ip for the device . Now I need to communicate over ethernet from DOM0 / DomU to device using SJA1110 Switch. I am able to ping the switch ip from device , but not able to ping from Dom0 / DomU .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also I need to share the internet from GMAC0 port to SJA1110 Switch Ports , so that other devices connected to SJA1110 switch can access internet&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let me know , as I am stuck here . I have tried all the examples given in ethernet enablement guide related to SJA1110 switch&lt;/P&gt;</description>
    <pubDate>Mon, 05 Jun 2023 11:30:56 GMT</pubDate>
    <dc:creator>girkulkarni</dc:creator>
    <dc:date>2023-06-05T11:30:56Z</dc:date>
    <item>
      <title>Communication between Dom0 and device connected to SJA1110 on s32g</title>
      <link>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1663447#M3509</link>
      <description>&lt;P&gt;I have connected a device to sja1110 switch on nxp s32g and got the ip for the device . Now I need to communicate over ethernet from DOM0 / DomU to device using SJA1110 Switch. I am able to ping the switch ip from device , but not able to ping from Dom0 / DomU .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also I need to share the internet from GMAC0 port to SJA1110 Switch Ports , so that other devices connected to SJA1110 switch can access internet&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let me know , as I am stuck here . I have tried all the examples given in ethernet enablement guide related to SJA1110 switch&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 11:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1663447#M3509</guid>
      <dc:creator>girkulkarni</dc:creator>
      <dc:date>2023-06-05T11:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between Dom0 and device connected to SJA1110 on s32g</title>
      <link>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1666203#M3573</link>
      <description>&lt;P&gt;Hello, Girish,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you please provide more details regarding:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;what BSP version you're using&lt;/LI&gt;
&lt;LI&gt;a full log including the commands you ran to configure the networking over Xen&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Andrei Cherechesu&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 13:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1666203#M3573</guid>
      <dc:creator>andrei_cherechesu</dc:creator>
      <dc:date>2023-06-08T13:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between Dom0 and device connected to SJA1110 on s32g</title>
      <link>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1666698#M3589</link>
      <description>&lt;P&gt;Hi Andrei,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The linux BSP which I am using is 33.0 and using Goldvip 1.5 Image provided by NXP.&lt;/P&gt;&lt;P&gt;I ran the below commands in U-boot&amp;nbsp; from ethernet enablement guide to enable the SJA1110 Ports ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=both"&lt;BR /&gt;setenv pfeng_mode enable,sgmii,sgmii,rgmii&lt;BR /&gt;saveenv&lt;BR /&gt;reset&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are the logs of SJA1110 switch during boot, SJA1110 Firmware has been flashed ,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[ 4.766549] sja1110 spi5.1: Successfully configured!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 4.766600] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 4.782953] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 4.782972] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 320312&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 4.783115] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 4.783190] sja1110 spi5.0: [sja1110_pre_uc_upload] µC not ready for download (Status=0x31)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 4.783471] sja1110 spi5.0: Uploading firmware...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.912053] sja1110 spi5.0: Upload successfully verified!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.938436] pfeng 46000000.pfe pfe0: configuring for fixed/sgmii link mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.938791] pfeng 46000000.pfe pfe0: Link is Up - 1Gbps/Full - flow control off&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.012975] pfeng 46000000.pfe: HIF1 started&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.015651] pfeng 46000000.pfe pfe1: PHY [stmmac-0:08] driver [Aquantia AQR113c] (irq=POLL)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.015673] pfeng 46000000.pfe pfe1: configuring for phy/sgmii link mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.015705] phy-s32gen1-serdes 44180000.serdes: Speed not supported&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.099616] pfeng 46000000.pfe: HIF2 started&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.164600] pfeng 46000000.pfe pfe2: PHY [PFEng Ethernet MDIO.2:04] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 6.164622] pfeng 46000000.pfe pfe2: configuring for phy/rgmii-id link mode&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 06:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1666698#M3589</guid>
      <dc:creator>girkulkarni</dc:creator>
      <dc:date>2023-06-09T06:54:52Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between Dom0 and device connected to SJA1110 on s32g</title>
      <link>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1666728#M3592</link>
      <description>&lt;P&gt;Hello, Girish,&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;One option would be to use the PFE0 interface that is connected to the SJA1110 switch to expose the traffic to/from the switch in the Dom0 VM. For example, if you are using the &lt;EM&gt;192.168.0.x/24&lt;/EM&gt; subnet for the devices connected to the SJA1110 switch, assign an IP from this range to the &lt;EM&gt;pfe0&lt;/EM&gt; interface and try to ping the other devices.&lt;BR /&gt;&lt;BR /&gt;If you intend to share the traffic in any unprivileged domain (i.e., v2xdomu), you will have to create a bridge in the same manner as &lt;EM&gt;xenbr0&lt;/EM&gt; is currently used, but you'll have to add the &lt;EM&gt;pfe0&lt;/EM&gt; physical interface to it. More details on how to create such a bridge / network setup can be found in the Linux BSP User Manual, under &lt;EM&gt;Networking in DomUs&lt;/EM&gt; chapter.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;George&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 07:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Communication-between-Dom0-and-device-connected-to-SJA1110-on/m-p/1666728#M3592</guid>
      <dc:creator>gmocanu</dc:creator>
      <dc:date>2023-06-09T07:33:33Z</dc:date>
    </item>
  </channel>
</rss>