<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
    <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1659268#M3414</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I already create a case, case number is "00540772".&lt;/P&gt;&lt;P&gt;It also including the source code of whole project.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 29 May 2023 17:37:07 GMT</pubDate>
    <dc:creator>RubyHsu</dc:creator>
    <dc:date>2023-05-29T17:37:07Z</dc:date>
    <item>
      <title>Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1656207#M3346</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am developing the PFE interface on the develop board(S32G-VNP-RDB2).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I followed the steps of document "GUIDE TO ENABLE PFE WITH LWIP BASED ON RTD" and&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Use MCAL PFE Driver(PFE-DRV_S32G_M7_MCAL_1.0.0_QLP2) + RTD(RTD_4.4_4.0.0_D2210) and EB tresos 29.0.0, then generate project.&lt;/P&gt;&lt;P&gt;2. Copy paste generated Eth_43_PFE related files and&amp;nbsp;Eth_43_PFE_TS_T40D11M10I0R0 to PFE folder&lt;/P&gt;&lt;P&gt;3. Create S32 DS Project based on LWIP example(TCPIP_RTM_1_0_3_HF1_D2301)&lt;/P&gt;&lt;P&gt;4.&amp;nbsp;Route pins for PFE EMAC2&lt;/P&gt;&lt;P&gt;5. Configure Clock for PFE MAC2&lt;/P&gt;&lt;P&gt;6. Add POWER module and setup MCU partition component.&lt;/P&gt;&lt;P&gt;7.Add tcpip module and configure the pbuf pool and&amp;nbsp;Receive window&amp;nbsp;&lt;/P&gt;&lt;P&gt;8.&amp;nbsp;Add PFE folder to project&amp;nbsp;and add related include folders to project's include paths setting&lt;/P&gt;&lt;P&gt;9.Change the defined value of HIF_CFG_DETACH_RX_JOB to TRUE&lt;/P&gt;&lt;P&gt;10.Replace gmacif.h with pfe-if.h&lt;/P&gt;&lt;P&gt;Now I can successfully compiler, but after running this project in&amp;nbsp;&lt;SPAN&gt;RDB2, it will stuck in DevAssert()&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="s32g.JPG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224598iEBEABB22EAA70F34/image-size/large?v=v2&amp;amp;px=999" role="button" title="s32g.JPG" alt="s32g.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;s32g.JPG&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is anything I'm missing to modify?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 03:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1656207#M3346</guid>
      <dc:creator>RubyHsu</dc:creator>
      <dc:date>2023-05-24T03:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1657043#M3362</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Since the guide you are following is using old RTD versions, the steps might vary to the newer ones. There is a document that explains how to create a "PFE Master Demo for M7" (link:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-PFE-Master-Demo-building-on-M7/ta-p/1603420" target="_blank"&gt;S32G PFE Master Demo building on M7 - NXP Community&lt;/A&gt;) all within EB Tresos. It uses a more recent version of the RTD. In there, the following integration requirement is mentioned:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1684960410624.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224741i4A91ED4BBAB122CE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1684960410624.png" alt="DanielAguirre_0-1684960410624.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;DanielAguirre_0-1684960410624.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Could be one possibility.&lt;/P&gt;
&lt;P&gt;Also, the out-of-the-box LWiP example needs the HSE FW to be already installed, do you have it installed?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 20:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1657043#M3362</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-05-24T20:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1657144#M3365</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I tried to add Eth_43_PFE_PreInit(NULL_PTR) in the beginning of&amp;nbsp;device_init(), but it still stuck in DevAssert.&lt;/P&gt;&lt;P&gt;About the LWIP example, I use&amp;nbsp;&lt;SPAN&gt;TCPIP_RTM_1_0_3_HF1_D2301 to generate the LWIP code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this still need HSE FW install?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 01:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1657144#M3365</guid>
      <dc:creator>RubyHsu</dc:creator>
      <dc:date>2023-05-25T01:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1657864#M3385</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;You are correct, we were mistaking the TCPIP version, the 1.0.3 does not require HSE FW to be installed.&lt;/P&gt;
&lt;P&gt;We verified and the example runs with no modification. Prior to any modification, do you have any trouble with the LWiP example?&lt;/P&gt;
&lt;P&gt;As for the specific DevAssert behavior, can you tell when it is happening? In which function access.&lt;/P&gt;
&lt;P&gt;Since we might need to ask for your project, we might recommend opening a ticker under the NXP online services, for us to provide you with a private channel.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 17:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1657864#M3385</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-05-25T17:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1658223#M3392</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using LWIP example to add PFE feature. This DevAssert happend in Eth_43_PFE_Init().&lt;/P&gt;&lt;P&gt;Please&amp;nbsp;&lt;SPAN&gt;opening a ticker under the NXP online services for me, thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 08:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1658223#M3392</guid>
      <dc:creator>RubyHsu</dc:creator>
      <dc:date>2023-05-26T08:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1658562#M3399</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback. We understand that you will open a ticket under the NXP online services, for which we will be waiting for it.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 18:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1658562#M3399</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-05-26T18:00:41Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1659268#M3414</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I already create a case, case number is "00540772".&lt;/P&gt;&lt;P&gt;It also including the source code of whole project.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 May 2023 17:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1659268#M3414</guid>
      <dc:creator>RubyHsu</dc:creator>
      <dc:date>2023-05-29T17:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck in DevAssert  when running PFE_MAC2 ethernet interface with LWIP and FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1660112#M3424</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the follow-up.&lt;/P&gt;&lt;P&gt;We will continue supporting this request through the case you have provided.&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 17:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Stuck-in-DevAssert-when-running-PFE-MAC2-ethernet-interface-with/m-p/1660112#M3424</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-05-30T17:14:37Z</dc:date>
    </item>
  </channel>
</rss>