<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: s32g274aevb booting</title>
    <link>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1642007#M3024</link>
    <description>&lt;P&gt;Any update for the above issue, i am facing the same issue.Any missing part please let me know.&lt;/P&gt;</description>
    <pubDate>Fri, 28 Apr 2023 06:06:41 GMT</pubDate>
    <dc:creator>kamal_n</dc:creator>
    <dc:date>2023-04-28T06:06:41Z</dc:date>
    <item>
      <title>s32g274aevb booting</title>
      <link>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1516688#M1388</link>
      <description>&lt;P&gt;actually there is sometimes issue like under log&lt;/P&gt;&lt;P&gt;BUT now the issue appear all times when i try to boot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;what is the reason ??&lt;/P&gt;&lt;P&gt;bsp : binaries_auto_linux_bsp28.0_s32g274&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04+geef88755a7 (Mar 03 2021 - 07:18:34 +0000)&lt;/P&gt;&lt;P&gt;CPU: NXP S32G274A rev. 2.1.0&lt;BR /&gt;Reset cause: Power-On Reset&lt;BR /&gt;Model: NXP S32G2XX&lt;BR /&gt;Board: NXP S32G274A-EVB&lt;BR /&gt;DRAM: 3.5 GiB&lt;BR /&gt;CA53 core 1 running.&lt;BR /&gt;CA53 core 2 running.&lt;BR /&gt;CA53 core 3 running.&lt;BR /&gt;All (4) cores are up.&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from MMC... OK&lt;BR /&gt;Using external clock for PCIe0&lt;BR /&gt;Configuring PCIe0 as RootComplex(x2)&lt;BR /&gt;Using external clock for PCIe1&lt;BR /&gt;Frequency 125Mhz configured for PCIe1&lt;BR /&gt;Configuring PCIe1 as SGMII [XPCS0 1G, XPCS1 OFF(PCIex1)]&lt;BR /&gt;PCIe0: Failed to get link up&lt;BR /&gt;Pcie0: LINK_DBG_1: 0x00000000, LINK_DBG_2: 0x00000800 (expected 0x000000d1)&lt;BR /&gt;DEBUG_R0: 0x000f0600, DEBUG_R1: 0x08200000&lt;BR /&gt;PCI: Failed autoconfig bar 20&lt;BR /&gt;PCI: Failed autoconfig bar 24&lt;BR /&gt;PCIe1: Not configuring PCIe, PHY not configured&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;usb dr_mode not found&lt;BR /&gt;EHCI fail to reset&lt;BR /&gt;enable_saf1508bet: Cannot find USB device&lt;BR /&gt;initcall sequence 00000000fcfc8ca8 failed at call 00000000340a2f98 (err=-1)&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 03:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1516688#M1388</guid>
      <dc:creator>bbbjj</dc:creator>
      <dc:date>2022-09-05T03:36:09Z</dc:date>
    </item>
    <item>
      <title>Re: s32g274aevb booting</title>
      <link>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1525049#M1432</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;did any changes in u-boot ?&amp;nbsp; or on board ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;regrade&lt;/P&gt;</description>
      <pubDate>Tue, 20 Sep 2022 12:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1525049#M1432</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2022-09-20T12:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: s32g274aevb booting</title>
      <link>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1642007#M3024</link>
      <description>&lt;P&gt;Any update for the above issue, i am facing the same issue.Any missing part please let me know.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 06:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g274aevb-booting/m-p/1642007#M3024</guid>
      <dc:creator>kamal_n</dc:creator>
      <dc:date>2023-04-28T06:06:41Z</dc:date>
    </item>
  </channel>
</rss>