<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: S32G STM Question</title>
    <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1636746#M2945</link>
    <description>&lt;P&gt;Hi, Daniel,&lt;/P&gt;&lt;P&gt;Does that mean if STM_7 is selected as the Timestamp source, it must be configured through the STM_TS register and configuration through the STM_7 register has no effect. And if STM_7 is not selected as the Timestamp source, STM_7 and STM_TS can be used as two separate timers.&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 00:59:25 GMT</pubDate>
    <dc:creator>Siyan</dc:creator>
    <dc:date>2023-04-20T00:59:25Z</dc:date>
    <item>
      <title>S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1633733#M2870</link>
      <description>&lt;P&gt;Hi, NXP Experts,&lt;/P&gt;&lt;P&gt;Q1: What's the meaning of " &lt;SPAN class=""&gt;One STM instance (STM_7) is tied to Timestamp&lt;/SPAN&gt;", how does it works?&lt;/P&gt;&lt;P&gt;Q2: Is "STM_TS" have any differences with other STM instances?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Siyan_0-1681458966299.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219266i5CFAA673291B92D2/image-size/medium?v=v2&amp;amp;px=400" alt="Siyan_0-1681458966299.png" title="Siyan_0-1681458966299.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Apr 2023 07:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1633733#M2870</guid>
      <dc:creator>Siyan</dc:creator>
      <dc:date>2023-04-14T07:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1634077#M2890</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Below will be some comments on regards of your questions:&lt;/P&gt;
&lt;P&gt;Q1 &amp;gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;What's the meaning of "&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;One STM instance (STM_7) is tied to Timestamp&lt;/SPAN&gt;&lt;SPAN&gt;", how does it works?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;A1 &amp;gt;&amp;gt; This is related to the "CAN_TS_CNT_SEL" bit available under the&amp;nbsp;TIMESTAMP_CONTROL_REGISTER, which Table 394 from the reference manual [Page 2443, S32G2 Reference Manual, Rev. 6, 11/2022] describes:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1681501281285.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219331i6A5122E3EE377278/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1681501281285.png" alt="DanielAguirre_0-1681501281285.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;DanielAguirre_0-1681501281285.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;It means STM_7 can be used to enable timestamp on CAN.&lt;/P&gt;
&lt;P&gt;Q2 &amp;gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;Is "STM_TS" have any differences with other STM instances?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;A2 &amp;gt;&amp;gt; Should be related to the timestamp selection of STM_7. If it is selected as the timestamp source, the memory map to configure the timer should be the one under STM_TS register description.&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Apr 2023 19:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1634077#M2890</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-04-14T19:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1635709#M2921</link>
      <description>Hi, Daniel,&lt;BR /&gt;I can't fully understand the A2 content. Could you explain it by other aspects. Thank you.</description>
      <pubDate>Wed, 19 Apr 2023 00:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1635709#M2921</guid>
      <dc:creator>Siyan</dc:creator>
      <dc:date>2023-04-19T00:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1636381#M2935</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your feedback. Below will be a different approach for A2.&lt;/P&gt;&lt;P&gt;STM_TS should be the configuration registers [Chapter 40.3, Page 1896, S32G2 Reference Manual, Rev. 6, 11/2022] to be used for STM_7 if STM_7 is selected as a Timestamp source as mentioned on the Table 394 of the S32G2 Reference Manual.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 15:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1636381#M2935</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-04-19T15:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1636746#M2945</link>
      <description>&lt;P&gt;Hi, Daniel,&lt;/P&gt;&lt;P&gt;Does that mean if STM_7 is selected as the Timestamp source, it must be configured through the STM_TS register and configuration through the STM_7 register has no effect. And if STM_7 is not selected as the Timestamp source, STM_7 and STM_TS can be used as two separate timers.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 00:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1636746#M2945</guid>
      <dc:creator>Siyan</dc:creator>
      <dc:date>2023-04-20T00:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1638152#M2956</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We apologize for our delay, we sent this inquiry to the internal to team to be sure of the provided information. The comment from the internal team is provided below:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;STM_7 and STM_TS are separate timer modules and have no relationship. STM_7 is tied to timestamp and can be configured as a timestamp resource via the TIMESTAMP_CONTROL_REGISTER in the SRC.&amp;nbsp;&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;For which we apologize for the comments provided before, it seems STM_7 and STM_TS are not related whatsoever. STM_7 is to be configured under the STM_7 registers with or without Timestamp, for what the internal team has provided.&lt;/P&gt;
&lt;P&gt;Again, we apologize, please let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 15:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1638152#M2956</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-04-21T15:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1649212#M3176</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205137"&gt;@Daniel-Aguirre&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you depict what STM_TS is intended for? In the S32GRM i don't see any special difference among this and the other STM_x. What i saw is STM_TS is in another memory map region.&lt;/P&gt;&lt;P&gt;In addition, S32DS clock source diagram does not provide info about what clock sources drives this STM_TS. However S32GRM claims STM timers are driven by same clock source so we can assume STM_TS timer is driven by the same clock source than other STM_x timers.&lt;/P&gt;&lt;P&gt;Why the TS suffix for this STM? Is tied to a peripheral to make some kind of timestamp like STM_7 has the feature to make timestamp for FlexCAN?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 07:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1649212#M3176</guid>
      <dc:creator>jmsc</dc:creator>
      <dc:date>2023-05-12T07:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32G STM Question</title>
      <link>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1649555#M3179</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The following is told from our internal team:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;STM_TS and STM_0~7 just have different interrupt design. for STM_TS, the interrupt is off-chassis. I didn't see any other differences between STM_TS and STM_0~7.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 15:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-STM-Question/m-p/1649555#M3179</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-05-12T15:28:14Z</dc:date>
    </item>
  </channel>
</rss>