<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G LLCE CAN Rx Frames are not Received in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1633836#M2871</link>
    <description>&lt;P&gt;Hi Tushar,&lt;/P&gt;&lt;P&gt;Hope you are doing well and Thank You for the reply.&lt;/P&gt;&lt;P&gt;My Apologies for the late reply.&lt;/P&gt;&lt;P&gt;We did run the NXP given example without Modification but None of the frames were Transmitted or Recived.&lt;/P&gt;&lt;P&gt;With Modification of we made now we are able to Recieve Frames on Configured Channels and Transmit as per our requirements with Slow Path ( with routing done by M7).&lt;/P&gt;&lt;P&gt;we are trying to configure Fast path with Advance Features But it is not working .&lt;/P&gt;&lt;P&gt;Here are the modification we have done in LLCE_AF&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_0-1681467804736.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219280i74BCC1D8B2D5F0EA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_0-1681467804736.png" alt="Santhosh_Addula_0-1681467804736.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_1-1681467884794.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219281iECB30DA7DEFE0C10/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_1-1681467884794.png" alt="Santhosh_Addula_1-1681467884794.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We have configured 6 Adance Features such&amp;nbsp; that each channel should recieve Rx CAN Frames and Transmit to Destination Channels .&lt;/P&gt;&lt;P&gt;Configgured the HOH as below&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_2-1681468263559.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219282iD0DC267DD8A9EB0D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_2-1681468263559.png" alt="Santhosh_Addula_2-1681468263559.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_3-1681468302110.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219283i1C4A01D7613D5125/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_3-1681468302110.png" alt="Santhosh_Addula_3-1681468302110.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;confgured the above HOH Advanced Features with&amp;nbsp;Can_43_LLCE_CreateAfDestination and&amp;nbsp;Can_43_LLCE_SetAfFilter API's&lt;/P&gt;&lt;P&gt;after the CAN Controller initialization , added below code such that it would configure the destination filters and re-route the recieved frames to Destination Channels as per the defination ( this is our understanding , Please let us know if we are wrong and please correct us what are need to be configured and corresponding Advance Feature setting).&lt;/P&gt;&lt;P&gt;Can_Af_DestRulesType Can2CanRule = {&lt;BR /&gt;{.Can2Can = {&lt;BR /&gt;/* ======= Routing Rule ======= */&lt;BR /&gt;(uint32)(&lt;BR /&gt;LLCE_CAN_ROUTING_CANFD |&lt;BR /&gt;LLCE_CAN_ROUTING_OPTION_DEFAULT_CONFIG&lt;BR /&gt;),&lt;BR /&gt;(uint32)0U,&lt;BR /&gt;{&lt;BR /&gt;(uint8)1,&lt;BR /&gt;(uint8)2,&lt;BR /&gt;(uint8)3,&lt;BR /&gt;(uint8)4,&lt;BR /&gt;(uint8)5,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0&lt;BR /&gt;},&lt;BR /&gt;(uint8)5U&lt;BR /&gt;}},&lt;BR /&gt;/* ======= Destination rule type ======= */&lt;BR /&gt;CAN_AF_CAN2CAN&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can_SetAfFilterType Can2CanFilter = {&lt;BR /&gt;{ /* RxFilter */&lt;BR /&gt;(Can_IdType)800U, /* uIdMask = RangeEnd */&lt;BR /&gt;(Can_IdType)700U, /* MessageId = RangeStart*/&lt;BR /&gt;(uint16)0x14, /* MBCount */&lt;BR /&gt;(Can_HwHandleType)0x6U, /* FilterId */&lt;BR /&gt;(uint8)0U, /* Rx is reported through this interface . */&lt;BR /&gt;LLCE_CAN_STANDARD,&lt;BR /&gt;LLCE_CAN_ENTRY_CFG_RANGED,&lt;BR /&gt;},&lt;BR /&gt;{ /* AdvancedFeature */&lt;BR /&gt;LLCE_AF_AUTHENTICATION_DISABLED, /* Option for frame authentication feature */&lt;BR /&gt;LLCE_AF_HOSTRECEIVE_DISABLED, /* Option for host receive feature */&lt;BR /&gt;LLCE_AF_LOGGING_DISABLED, /* Option for logging feature */&lt;BR /&gt;LLCE_AF_CUSTOMPROCESSING_DISABLED, /* Option for custom processing in FDK */&lt;BR /&gt;(uint8)0U, /* Reference to Can2Can routing entry */&lt;BR /&gt;(uint8)LLCE_CAN_ADVANCED_FILTER_NOT_USED, /* Can2Eth not used */&lt;BR /&gt;}&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Can_43_LLCE_CreateAfDestination(Can2CanRule,&amp;amp;RuleIndex);&lt;/P&gt;&lt;P&gt;Can2CanFilter.AdvancedFeature.u8Can2CanRoutingTableIdx = RuleIndex;&lt;/P&gt;&lt;P&gt;Can_43_LLCE_SetAfFilter(&amp;amp;Can2CanFilter);&lt;/P&gt;&lt;P&gt;with the above changes , when a Frame given within Range of HOH filter , LLCE should Recive frame and FastRoute to Destination Channels , but it is not happening.&lt;/P&gt;&lt;P&gt;1. Could you pls let us know what is the procedure for Fast path Implementation?&lt;/P&gt;&lt;P&gt;2. whether do we need to buy the separate packages for LLCE Fast path routing from NXP?&lt;/P&gt;&lt;P&gt;Thanks for your time in guiding us .&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 17 Apr 2023 13:58:54 GMT</pubDate>
    <dc:creator>Santhosh_Addula</dc:creator>
    <dc:date>2023-04-17T13:58:54Z</dc:date>
    <item>
      <title>S32G LLCE CAN Rx Frames are not Received</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1627706#M2728</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;we are trying to do &lt;SPAN&gt;Can_Llce_DS_Can2Can_S32G274A Example given by NXP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;we have modified linker file as per&amp;nbsp;Light Up RGB LED Based On Real Time Drivers example provided by NXP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;we have made the connections are per the NXP instructions.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;when we board is booted,&amp;nbsp;No frames are transmitted from M7 (verified in CANoe with Configured BaudRate as per the example).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. Not sure what is going wrong here , can you pls guide us .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;we have modified the Configuration for LLCE CAN Channel 0 to Receive&amp;nbsp;and Transmit the message on LLCE Channel 1. As of now we are not able to receive&amp;nbsp;the CAN Messages but able transmit dummy message&amp;nbsp; on LLCE CAN 1 Channel.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;we observe that&amp;nbsp;Can_RxIndication counter which Indicates that Rx Frame is recived is not updating (for the debugging purpose updated the local PDU data with&amp;nbsp;Can_RxIndication &amp;amp;&amp;nbsp;Can_TxConfirmation in CAN PDU and transmitted on LLCE_CAN1 Channel , in the CANoe Trace we found that Can_RxIndication is always 0 &amp;amp; Can_TxConfirmation is updating sequentially).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;we traced back the code w.r.t. Rx channel interrupts used and calling functions seems to be defined okay but in the Board these seems to be not called or not processed.&lt;/P&gt;&lt;P&gt;2. Please look into the attached S32DS project and guide us any configuration changes need to be done .&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Santhosh .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 05:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1627706#M2728</guid>
      <dc:creator>Santhosh_Addula</dc:creator>
      <dc:date>2023-04-07T05:14:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE CAN Rx Frames are not Received</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1630476#M2792</link>
      <description>&lt;P&gt;Hi Santhosh&lt;/P&gt;
&lt;P&gt;hope you are doing well.&lt;/P&gt;
&lt;P&gt;Did you run example without modified ? are you getting issue after modification&amp;nbsp; ?&lt;/P&gt;
&lt;P&gt;Regards ,&lt;/P&gt;
&lt;P&gt;Tushar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 09:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1630476#M2792</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-04-10T09:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE CAN Rx Frames are not Received</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1633836#M2871</link>
      <description>&lt;P&gt;Hi Tushar,&lt;/P&gt;&lt;P&gt;Hope you are doing well and Thank You for the reply.&lt;/P&gt;&lt;P&gt;My Apologies for the late reply.&lt;/P&gt;&lt;P&gt;We did run the NXP given example without Modification but None of the frames were Transmitted or Recived.&lt;/P&gt;&lt;P&gt;With Modification of we made now we are able to Recieve Frames on Configured Channels and Transmit as per our requirements with Slow Path ( with routing done by M7).&lt;/P&gt;&lt;P&gt;we are trying to configure Fast path with Advance Features But it is not working .&lt;/P&gt;&lt;P&gt;Here are the modification we have done in LLCE_AF&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_0-1681467804736.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219280i74BCC1D8B2D5F0EA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_0-1681467804736.png" alt="Santhosh_Addula_0-1681467804736.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_1-1681467884794.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219281iECB30DA7DEFE0C10/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_1-1681467884794.png" alt="Santhosh_Addula_1-1681467884794.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We have configured 6 Adance Features such&amp;nbsp; that each channel should recieve Rx CAN Frames and Transmit to Destination Channels .&lt;/P&gt;&lt;P&gt;Configgured the HOH as below&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_2-1681468263559.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219282iD0DC267DD8A9EB0D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_2-1681468263559.png" alt="Santhosh_Addula_2-1681468263559.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Santhosh_Addula_3-1681468302110.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219283i1C4A01D7613D5125/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Santhosh_Addula_3-1681468302110.png" alt="Santhosh_Addula_3-1681468302110.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;confgured the above HOH Advanced Features with&amp;nbsp;Can_43_LLCE_CreateAfDestination and&amp;nbsp;Can_43_LLCE_SetAfFilter API's&lt;/P&gt;&lt;P&gt;after the CAN Controller initialization , added below code such that it would configure the destination filters and re-route the recieved frames to Destination Channels as per the defination ( this is our understanding , Please let us know if we are wrong and please correct us what are need to be configured and corresponding Advance Feature setting).&lt;/P&gt;&lt;P&gt;Can_Af_DestRulesType Can2CanRule = {&lt;BR /&gt;{.Can2Can = {&lt;BR /&gt;/* ======= Routing Rule ======= */&lt;BR /&gt;(uint32)(&lt;BR /&gt;LLCE_CAN_ROUTING_CANFD |&lt;BR /&gt;LLCE_CAN_ROUTING_OPTION_DEFAULT_CONFIG&lt;BR /&gt;),&lt;BR /&gt;(uint32)0U,&lt;BR /&gt;{&lt;BR /&gt;(uint8)1,&lt;BR /&gt;(uint8)2,&lt;BR /&gt;(uint8)3,&lt;BR /&gt;(uint8)4,&lt;BR /&gt;(uint8)5,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0,&lt;BR /&gt;(uint8)0&lt;BR /&gt;},&lt;BR /&gt;(uint8)5U&lt;BR /&gt;}},&lt;BR /&gt;/* ======= Destination rule type ======= */&lt;BR /&gt;CAN_AF_CAN2CAN&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can_SetAfFilterType Can2CanFilter = {&lt;BR /&gt;{ /* RxFilter */&lt;BR /&gt;(Can_IdType)800U, /* uIdMask = RangeEnd */&lt;BR /&gt;(Can_IdType)700U, /* MessageId = RangeStart*/&lt;BR /&gt;(uint16)0x14, /* MBCount */&lt;BR /&gt;(Can_HwHandleType)0x6U, /* FilterId */&lt;BR /&gt;(uint8)0U, /* Rx is reported through this interface . */&lt;BR /&gt;LLCE_CAN_STANDARD,&lt;BR /&gt;LLCE_CAN_ENTRY_CFG_RANGED,&lt;BR /&gt;},&lt;BR /&gt;{ /* AdvancedFeature */&lt;BR /&gt;LLCE_AF_AUTHENTICATION_DISABLED, /* Option for frame authentication feature */&lt;BR /&gt;LLCE_AF_HOSTRECEIVE_DISABLED, /* Option for host receive feature */&lt;BR /&gt;LLCE_AF_LOGGING_DISABLED, /* Option for logging feature */&lt;BR /&gt;LLCE_AF_CUSTOMPROCESSING_DISABLED, /* Option for custom processing in FDK */&lt;BR /&gt;(uint8)0U, /* Reference to Can2Can routing entry */&lt;BR /&gt;(uint8)LLCE_CAN_ADVANCED_FILTER_NOT_USED, /* Can2Eth not used */&lt;BR /&gt;}&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Can_43_LLCE_CreateAfDestination(Can2CanRule,&amp;amp;RuleIndex);&lt;/P&gt;&lt;P&gt;Can2CanFilter.AdvancedFeature.u8Can2CanRoutingTableIdx = RuleIndex;&lt;/P&gt;&lt;P&gt;Can_43_LLCE_SetAfFilter(&amp;amp;Can2CanFilter);&lt;/P&gt;&lt;P&gt;with the above changes , when a Frame given within Range of HOH filter , LLCE should Recive frame and FastRoute to Destination Channels , but it is not happening.&lt;/P&gt;&lt;P&gt;1. Could you pls let us know what is the procedure for Fast path Implementation?&lt;/P&gt;&lt;P&gt;2. whether do we need to buy the separate packages for LLCE Fast path routing from NXP?&lt;/P&gt;&lt;P&gt;Thanks for your time in guiding us .&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 13:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1633836#M2871</guid>
      <dc:creator>Santhosh_Addula</dc:creator>
      <dc:date>2023-04-17T13:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE CAN Rx Frames are not Received</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1635135#M2905</link>
      <description>&lt;P&gt;Hi Santhosh&lt;/P&gt;
&lt;P&gt;Thanks for sharing information , we will look into and update.&lt;/P&gt;
&lt;P&gt;Regards ,&lt;/P&gt;
&lt;P&gt;Tushar&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 06:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1635135#M2905</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-04-18T06:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE CAN Rx Frames are not Received</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1635973#M2930</link>
      <description>&lt;P&gt;Hi Santosh&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;1. Could you pls let us know what is the procedure for Fast path Implementation?&lt;/P&gt;
&lt;P&gt;A. Read the &lt;SPAN class="markedContent"&gt;&lt;SPAN&gt;Document Number: AN13423&lt;/SPAN&gt;&lt;/SPAN&gt; for this. i have also attached here.&lt;/P&gt;
&lt;P&gt;2. whether do we need to buy the separate packages for LLCE Fast path routing from NXP?&lt;/P&gt;
&lt;P&gt;A. No, you have not to buy separate for same.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hope this helps you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards ,&lt;/P&gt;
&lt;P&gt;Tushar&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 07:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-Rx-Frames-are-not-Received/m-p/1635973#M2930</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-04-19T07:20:06Z</dc:date>
    </item>
  </channel>
</rss>