<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G2 Eth_43_PFE Problem in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1630659#M2801</link>
    <description>&lt;P&gt;Hi Jack,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can i share same thread with you, for the same topic. In My case EBtresos but for you its davinci tool. 1. i am unable to load EB tresos generated code s32 design studio.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Unable to find the good NXP example code for PFE. could you please share info like which sample project taken as example for PFE ??&lt;/P&gt;&lt;P&gt;3. PFE MCAL driver 0.9.7 is asking EBtresos project generated code and unable to compile the source code.&lt;/P&gt;&lt;P&gt;4. PFE-Demo code is there - which we too wanted PFE as Master bit it not compiling too. Unable to progress in PFE with sample project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN13423 we following but for PFE few steps they missed and directly came to CAN2CAN project leave CAN2ETH project code in hanging in AIR.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Viswa&lt;/P&gt;</description>
    <pubDate>Mon, 10 Apr 2023 17:56:28 GMT</pubDate>
    <dc:creator>viswa_kondapall</dc:creator>
    <dc:date>2023-04-10T17:56:28Z</dc:date>
    <item>
      <title>S32G2 Eth_43_PFE Problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1630407#M2788</link>
      <description>&lt;P&gt;Dear，&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN&gt;When the eth_43_PFE module was imported into the Davinci tool, the generated code failed to be compiled.&amp;nbsp;See Figure 1 for details.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;The error content is as follows: &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;/include/oal_mutex_autosar.h:660:22: error: &lt;/SPAN&gt;&lt;SPAN class=""&gt;'SchM_Exit_Eth_43_PFE_ETH_EXCLUSIVE_AREA_173' undeclared here (not in a function); &lt;/SPAN&gt;&lt;SPAN class=""&gt;did you mean 'SchM_Exit_Eth_43_PFE_ETH_EXCLUSIVE_AREA_ID'? &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;But there's actually a definition for SchM_Exit_Eth_43_PFE_ETH_EXCLUSIVE_AREA_173.&amp;nbsp;&lt;SPAN&gt;See Figure 2 for details&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I wonder if there is something wrong with the writing.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Macro functions cannot directly assign values to a variable. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;RTD uses SW32G_RTD_4.4_S32CC_4.0.1 &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;PFE uses pfe-drv_s32g_m7_mcal_1.0.0_qlp3 &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please help to see how to solve it. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Best Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 08:20:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1630407#M2788</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2023-04-10T08:20:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Eth_43_PFE Problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1630659#M2801</link>
      <description>&lt;P&gt;Hi Jack,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can i share same thread with you, for the same topic. In My case EBtresos but for you its davinci tool. 1. i am unable to load EB tresos generated code s32 design studio.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Unable to find the good NXP example code for PFE. could you please share info like which sample project taken as example for PFE ??&lt;/P&gt;&lt;P&gt;3. PFE MCAL driver 0.9.7 is asking EBtresos project generated code and unable to compile the source code.&lt;/P&gt;&lt;P&gt;4. PFE-Demo code is there - which we too wanted PFE as Master bit it not compiling too. Unable to progress in PFE with sample project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN13423 we following but for PFE few steps they missed and directly came to CAN2CAN project leave CAN2ETH project code in hanging in AIR.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Viswa&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 17:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1630659#M2801</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2023-04-10T17:56:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Eth_43_PFE Problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1631513#M2821</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Could be a problem with the tool itself, but due to you using a non-public RTD (v4.0.1 for what we understood), we recommend either opening a ticket under the NXP online service or sending this same topic to your local NXP FAE/representative, for them to channel it adequately, since could be related to a bug since it is still under development.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 18:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1631513#M2821</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-04-11T18:44:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Eth_43_PFE Problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1871721#M7007</link>
      <description>&lt;P&gt;Is there any solution to this problem?&lt;/P&gt;&lt;P&gt;I have the same problem using PFE.&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 07:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1871721#M7007</guid>
      <dc:creator>Youngsoo_do</dc:creator>
      <dc:date>2024-05-23T07:29:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Eth_43_PFE Problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1872095#M7012</link>
      <description>&lt;P&gt;We left it. me too eagerly waiting to find the solution. PFE--&amp;gt;ETH_43 interface.&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 14:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Eth-43-PFE-Problem/m-p/1872095#M7012</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2024-05-23T14:31:08Z</dc:date>
    </item>
  </channel>
</rss>