<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IPCF course kernel panic when memcpy from sram to kfifo in S32G</title>
    <link>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627017#M2711</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you provide which BSP/IPCF/RTD version are you using? Are you using an NXP platform? Or is it a custom board?&lt;/P&gt;&lt;P&gt;Also, have you disabled dcache on u-boot? This is explained on the "description.txt" file available on the M7 core project.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Mon, 03 Apr 2023 17:15:55 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-04-03T17:15:55Z</dc:date>
    <item>
      <title>IPCF course kernel panic when memcpy from sram to kfifo</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1626629#M2707</link>
      <description>&lt;P&gt;Hi， Based on the module(ipc-shm-dev) provided in ipcf, I implemented another module to receive mcore messages and distribute them. when i use the kfifo_in() api , copying data from sram to kernel space buffer, kernel panic occurred. According to the dmesg log, the problem is in the memcpy() function. When i use ipc_memcpy(), which copy byte to byte, no error occurred. So i use ipc_memcpy() to copy data from sram to kernel space, then use the kfifo_in() api. this will increase the data process time, which is important to my use case. Do you know how to fix the memcpy problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[ 97.621545] ipc-shm-com: ch 1 &amp;lt;&amp;lt; 49 bytes: &amp;#1;1&lt;BR /&gt;[ 97.621551] ipc-shm-com: get message 12545&lt;BR /&gt;[ 97.621554] ipc-shm-com: data_chan_rx_cb(): message id 12545, ipc channel mask: 4&lt;BR /&gt;[ 97.621559] ipc-shm-com: data_chan_rx_cb(): ipc channel : 2 want message id 12545&lt;BR /&gt;[ 97.621576] Unable to handle kernel paging request at virtual address ffffffc014400746&lt;BR /&gt;[ 103.432905] Mem abort info:&lt;BR /&gt;[ 103.441557] ESR = 0x96000021&lt;BR /&gt;[ 103.456041] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;[ 103.468617] SET = 0, FnV = 0&lt;BR /&gt;[ 103.477557] EA = 0, S1PTW = 0&lt;BR /&gt;[ 103.492139] Data abort info:&lt;BR /&gt;[ 103.502294] ISV = 0, ISS = 0x00000021&lt;BR /&gt;[ 103.512016] CM = 0, WnR = 0&lt;BR /&gt;[ 103.526425] swapper pgtable: 4k pages, 39-bit VAs, pgdp=0000000080ca6000&lt;BR /&gt;[ 103.540399] [ffffffc014400746] pgd=00000008dffff003, p4d=00000008dffff003, pud=00000008dffff003, pmd=000000088361e003, pte=0068000034200717&lt;BR /&gt;[ 103.558804] Internal error: Oops: 96000021 [#1] PREEMPT SMP&lt;BR /&gt;[ 103.570271] ipc-shm-dev: ipc_hw_irq_notify(): *********ipc irq notify**********&lt;BR /&gt;[ 103.570272] printk: console [ttyLF0]: printing thread stopped&lt;BR /&gt;[ 103.575805] Modules linked in: ipc_shm_com(O) ipc_shm_dev(O) pfeng(O) [last unloaded: ipc_shm_dev]&lt;BR /&gt;[ 103.597765] CPU: 0 PID: 403 Comm: mcu_forwarding_ Tainted: G O 5.10.109-rt65 #1&lt;BR /&gt;[ 103.612258] Hardware name: NXP S32G399A-RDB3 (DT)&lt;BR /&gt;[ 103.628403] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 103.641683] pc : __memcpy+0x84/0x180&lt;BR /&gt;[ 103.651144] lr : kfifo_copy_in+0x78/0x98&lt;BR /&gt;[ 103.666507] sp : ffffffc01115bcb0&lt;BR /&gt;[ 103.677096] x29: ffffffc01115bcb0 x28: ffffffc0089e8958&lt;BR /&gt;[ 103.682391] x27: 0000000000000004 x26: ffffff8801361530&lt;BR /&gt;[ 103.687686] x25: ffffffc0089f2180 x24: ffffffc0089f0000&lt;BR /&gt;[ 103.692981] x23: 0000000000000026 x22: ffffffc014400720&lt;BR /&gt;[ 103.698275] x21: ffffff8801361530 x20: 0000000000000031&lt;BR /&gt;[ 103.709473] x19: 0000000000000026 x18: 0000000000000001&lt;BR /&gt;[ 103.726225] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 103.738811] x15: ffffff88015927e8 x14: ffffffffffffffff&lt;BR /&gt;[ 103.750008] x13: ffffffc01110d309 x12: ffffffc01110d302&lt;BR /&gt;[ 103.766761] x11: ffffffc011014840 x10: ffffffc010feeff0&lt;BR /&gt;[ 103.779347] x9 : ffffffc0100981ac x8 : 000000c040000010&lt;BR /&gt;[ 103.790544] x7 : fa00080000007b01 x6 : ffffff8804a07000&lt;BR /&gt;[ 103.807296] x5 : ffffff885f856890 x4 : 0000000000000000&lt;BR /&gt;[ 103.819882] x3 : 0000000000000000 x2 : 000000000000000b&lt;BR /&gt;[ 103.831079] x1 : ffffffc014400746 x0 : ffffff8804a07000&lt;BR /&gt;[ 103.847835] Call trace:&lt;BR /&gt;[ 103.857556] __memcpy+0x84/0x180&lt;BR /&gt;[ 103.866668] __kfifo_in+0x38/0x58&lt;BR /&gt;[ 103.881423] data_chan_rx_cb+0x1b8/0x284 [ipc_shm_com]&lt;BR /&gt;[ 103.893836] ipc_shm_rx+0x12c/0x220 [ipc_shm_dev]&lt;BR /&gt;[ 103.904426] ipc_shm_softirq+0x64/0xe0 [ipc_shm_dev]&lt;BR /&gt;[ 103.920831] tasklet_action_common.isra.0+0x138/0x150&lt;BR /&gt;[ 103.933156] tasklet_action+0x30/0x40&lt;BR /&gt;[ 103.936802] __do_softirq+0x130/0x3e0&lt;BR /&gt;[ 103.940447] irq_exit+0xc0/0xe8&lt;BR /&gt;[ 103.943573] __handle_domain_irq+0x70/0xc8&lt;BR /&gt;[ 103.947652] gic_handle_irq+0x60/0x12c&lt;BR /&gt;[ 103.951386] el1_irq+0xcc/0x180&lt;BR /&gt;[ 103.960413] vprintk_store+0x27c/0x4a8&lt;BR /&gt;[ 103.975603] vprintk_emit+0x4c/0x88&lt;BR /&gt;[ 103.986366] printk+0x88/0xb0&lt;BR /&gt;[ 103.995219] __dynamic_pr_debug+0x78/0xa8&lt;BR /&gt;[ 104.010670] ipc_shm_com_read+0xd8/0x270 [ipc_shm_com]&lt;BR /&gt;[ 104.023082] vfs_read+0xb4/0x1a8&lt;BR /&gt;[ 104.032196] ksys_read+0x74/0x108&lt;BR /&gt;[ 104.046951] __arm64_sys_read+0x24/0x30&lt;BR /&gt;[ 104.058062] el0_svc_common.constprop.0+0x80/0x1d0&lt;BR /&gt;[ 104.068738] do_el0_svc+0x2c/0x98&lt;BR /&gt;[ 104.083494] el0_svc+0x20/0x30&lt;BR /&gt;[ 104.093825] el0_sync_handler+0xb0/0xb8&lt;BR /&gt;[ 104.103545] el0_sync+0x180/0x1c0&lt;BR /&gt;[ 104.118307] Code: a88120c7 a8c12027 a88120c7 36180062 (f8408423)&lt;BR /&gt;[ 104.131674] ---[ end trace d813e9c44a4d873a ]---&lt;BR /&gt;[ 104.242446] Kernel panic - not syncing:&lt;BR /&gt;[ 104.251252] Oops: Fatal exception in interrupt&lt;BR /&gt;[ 104.351558] SMP: stopping secondary CPUs&lt;BR /&gt;[ 104.355045] Kernel Offset: disabled&lt;BR /&gt;[ 104.358511] CPU features: 0x00040022,2000200c&lt;BR /&gt;[ 104.362851] Memory Limit: none&lt;BR /&gt;[ 104.365895] ---[ end Kernel panic - not syncing: Oops: Fatal exception in interrupt ]---&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 06:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1626629#M2707</guid>
      <dc:creator>superyyf</dc:creator>
      <dc:date>2023-04-03T06:53:50Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF course kernel panic when memcpy from sram to kfifo</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627017#M2711</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you provide which BSP/IPCF/RTD version are you using? Are you using an NXP platform? Or is it a custom board?&lt;/P&gt;&lt;P&gt;Also, have you disabled dcache on u-boot? This is explained on the "description.txt" file available on the M7 core project.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 17:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627017#M2711</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-04-03T17:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF course kernel panic when memcpy from sram to kfifo</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627303#M2718</link>
      <description>&lt;P&gt;BSP version:&amp;nbsp; 33.0&lt;/P&gt;&lt;P&gt;IPCF:&amp;nbsp;SW32G_IPCF_4.7.0_D2208&lt;/P&gt;&lt;P&gt;RTD: 3.0.2&lt;/P&gt;&lt;P&gt;we did not disabled dcache on u-boot&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 05:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627303#M2718</guid>
      <dc:creator>superyyf</dc:creator>
      <dc:date>2023-04-04T05:14:17Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF course kernel panic when memcpy from sram to kfifo</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627860#M2734</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;Have you tried running with dcahe off?&lt;/P&gt;
&lt;P&gt;Also, have you zeroed the region where you are having the shared memory space?&lt;/P&gt;
&lt;P&gt;There is an example provided on IPCF for M7 which describes some pre-requisites that need to be done on u-boot, have you had this same problem under the example itself?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 18:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-course-kernel-panic-when-memcpy-from-sram-to-kfifo/m-p/1627860#M2734</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-04-04T18:40:56Z</dc:date>
    </item>
  </channel>
</rss>