<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: If any examples for S32G2 Multicore use the same project with FreeRTOS</title>
    <link>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1623681#M2674</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Thank you for your response. I appreciate your prompt attention and assistance. If I have any further questions, I'll be sure to reach out.&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;</description>
    <pubDate>Wed, 29 Mar 2023 01:20:37 GMT</pubDate>
    <dc:creator>bakerliu</dc:creator>
    <dc:date>2023-03-29T01:20:37Z</dc:date>
    <item>
      <title>If any examples for S32G2 Multicore use the same project with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1621973#M2630</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was wondering if there are any examples of using FreeRTOS with S32G2 multicore M7 processors. Please let me know if the same project can be used for this purpose.&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;BR /&gt;Baker&lt;/P&gt;</description>
      <pubDate>Sat, 25 Mar 2023 06:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1621973#M2630</guid>
      <dc:creator>bakerliu</dc:creator>
      <dc:date>2023-03-25T06:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: If any examples for S32G2 Multicore use the same project with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1622775#M2646</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The main example that is provided for multicore application under the S32G platform is the one explained on the AN13750 available under the S32G2 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g2-processors-for-vehicle-networking:S32G2" target="_blank"&gt;S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;It can be done integrating FreeRTOS, but there is not an out-of-the-box example that uses FreeRTOS. We do apologize.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 18:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1622775#M2646</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-03-27T18:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: If any examples for S32G2 Multicore use the same project with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1622907#M2654</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have created a multicore application using S32DS, but it is separated into three projects. I am wondering if it is possible to create a single project application that runs on the multicore M7 using a single image file?&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Mar 2023 01:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1622907#M2654</guid>
      <dc:creator>bakerliu</dc:creator>
      <dc:date>2023-03-28T01:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: If any examples for S32G2 Multicore use the same project with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1623519#M2661</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;Under the S32G platform, the multicore application requires independent files. This means that each core has its own application. Hence, no single file (at this moment) multicore application is possible. That is why AN13750 uses different files for each core.&lt;/P&gt;&lt;P&gt;We apologize for this.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Mar 2023 15:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1623519#M2661</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-03-28T15:42:55Z</dc:date>
    </item>
    <item>
      <title>Re: If any examples for S32G2 Multicore use the same project with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1623681#M2674</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Thank you for your response. I appreciate your prompt attention and assistance. If I have any further questions, I'll be sure to reach out.&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 01:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/If-any-examples-for-S32G2-Multicore-use-the-same-project-with/m-p/1623681#M2674</guid>
      <dc:creator>bakerliu</dc:creator>
      <dc:date>2023-03-29T01:20:37Z</dc:date>
    </item>
  </channel>
</rss>