<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet Bring up in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620848#M2602</link>
    <description>&lt;P&gt;we are using baremetal configuration in that we don't have&amp;nbsp;&lt;SPAN&gt;sdk_port.c file . So for that do we need HSE firmware or will it work without that&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Mar 2023 12:07:23 GMT</pubDate>
    <dc:creator>NP1</dc:creator>
    <dc:date>2023-03-23T12:07:23Z</dc:date>
    <item>
      <title>Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587085#M2070</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am working on the bring up of the Ethernet interface in the S32G2, In datasheet it mentioned that the GMAC will support different versions of ethernet, but the corresponding register details were not present in the reference manual,&lt;/P&gt;&lt;P&gt;and also tried the Eth_lnternal llopback_s32g274a example for ethernet, in this example the IO's are not configured for the ethernet by default, so it is confusing that which instance of the ethernet is used.&lt;/P&gt;&lt;P&gt;Kindly provide information regarding the IO's that are needed for the example and also steps needed to bring up the ETHERNET&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#S32G2 #ETHERNET&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 11:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587085#M2070</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2023-01-24T11:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587289#M2076</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;There is an "Ethernet Enablement Guide" [S32G-VNP-RDB2 Ethernet Enablement Guide, User Guide, Rev. 1, 05/2021] for RDB2 that gives an overview on how to use the available ethernet ports on the board. This can be downloaded from the RDB2 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/design/designs/s32g2-vehicle-networking-reference-design:S32G-VNP-RDB2" target="_blank"&gt;S32G2 Vehicle Networking Reference Design | NXP Semiconductors&lt;/A&gt;) under the "Documentation" section.&lt;/P&gt;
&lt;P&gt;There is also an available stack under the "Automotive SW – S32G Reference Software &amp;gt; Automotive SW - S32G - TCP/IP Stack (Cortex-M7)" section from Flexera which has an out-of-the-box example that uses the GMAC interface (lwip_s32g274a) that could help you with your question. Just, verify that you have the pre-requisites for the stack (mainly the versions) for you to be able to use it.&lt;/P&gt;
&lt;P&gt;Last but not least, there is a "GMAC Subsystem RM" [GMAC Subsystem RM, Rev. 2, 03/2021] in the S32G2 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g2-processors-for-vehicle-networking:S32G2" target="_blank"&gt;S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;) in the "Documentation" section that could help to understand the insides of the GMAC module.&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 18:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587289#M2076</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-24T18:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587588#M2077</link>
      <description>&lt;P&gt;Hi Daniel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply&lt;/P&gt;&lt;P&gt;i found the TCP/IP stack and it is installed in the S32 Design studio, i am trying to compile the lwip_s32g274a example, but i am getting error in freertos,&lt;/P&gt;&lt;P&gt;I have added the Packages of FREERTOS, RTD, TCP/IP Stacks are all installed in the IDE,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ethernet.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208321iD5EC6AC058D553AD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ethernet.jpg" alt="Ethernet.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ethernet.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="naveenkumar_muthusamy_0-1674645526984.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208323i226458E722809C0D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="naveenkumar_muthusamy_0-1674645526984.jpeg" alt="naveenkumar_muthusamy_0-1674645526984.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;naveenkumar_muthusamy_0-1674645526984.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="packages_1.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208324i3F107CAC8ABFB3C6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="packages_1.jpg" alt="packages_1.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;packages_1.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly help me in fixing this error,&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 11:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587588#M2077</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2023-01-25T11:20:02Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587636#M2079</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to compile the project, i had a issue with the packages installed in the PC, so now build is fine&lt;/P&gt;&lt;P&gt;i am facing issue that, whenever i run the project it is going into the dev_Assert handler,&lt;/P&gt;&lt;P&gt;for physical connections i have connected the ethernet port of RGMII with the PC and both are in same network 192.168.0.1 gateway,&lt;/P&gt;&lt;P&gt;Even when i try to ping the IP of 192.168.0.200 , i am not getting any reply&lt;/P&gt;&lt;P&gt;in discription i found that HSE need to flashed, is it mandatory to flash the CPU,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if it is mandatory kindly provide the Links and documents regarding how to do it&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 12:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587636#M2079</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2023-01-25T12:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587884#M2081</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding HSE information, we recommend sending the inquiry to your local NXP representative/FAE due to this information being confidential.&lt;/P&gt;
&lt;P&gt;As if you could run the application without it, we have done the following modification and can ping the board:&lt;/P&gt;
&lt;P&gt;- Under sdk_port.c comment the line 282&lt;/P&gt;
&lt;P&gt;#if defined(NXP_RTD_HSE) // Line 281&lt;BR /&gt;// HSE_DAL_Init();&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; // Line 282&lt;BR /&gt;#endif /* NXP_RTD_HSE */&amp;nbsp; // Line 283&lt;/P&gt;
&lt;P&gt;This should let you run the application.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 18:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1587884#M2081</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-25T18:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1588776#M2087</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your continued support.&lt;/P&gt;&lt;P&gt;Now we are able to ping the Board from PC and workaround you have suggested is working&lt;/P&gt;&lt;P&gt;Thanks once again&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 09:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1588776#M2087</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2023-01-27T09:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620436#M2587</link>
      <description>&lt;P&gt;Can you share the HSE FW which need to be flashed (SW or link) ? also it would be great if u can share the flashing procedure for that as well .&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 03:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620436#M2587</guid>
      <dc:creator>NP1</dc:creator>
      <dc:date>2023-03-23T03:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620453#M2588</link>
      <description>&lt;P&gt;HSE Firmware is not needed if you are using it for ethernet development, as mentioned above just comment the mentioned lines , ethernet will work&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 04:19:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620453#M2588</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2023-03-23T04:19:49Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Bring up</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620848#M2602</link>
      <description>&lt;P&gt;we are using baremetal configuration in that we don't have&amp;nbsp;&lt;SPAN&gt;sdk_port.c file . So for that do we need HSE firmware or will it work without that&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 12:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-Bring-up/m-p/1620848#M2602</guid>
      <dc:creator>NP1</dc:creator>
      <dc:date>2023-03-23T12:07:23Z</dc:date>
    </item>
  </channel>
</rss>