<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: How to can to eth?</title>
    <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620531#M2589</link>
    <description>If a time trigger mechanism exists, which file should be modified?or how to modify ?</description>
    <pubDate>Thu, 23 Mar 2023 06:16:56 GMT</pubDate>
    <dc:creator>fenghua_jiang</dc:creator>
    <dc:date>2023-03-23T06:16:56Z</dc:date>
    <item>
      <title>How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1619077#M2546</link>
      <description>&lt;P&gt;Hi Teams,&lt;/P&gt;&lt;P&gt;&amp;nbsp; The CAN2ETH feature performs the off-loaded encapsulation which packs configured CAN frames into&lt;BR /&gt;Ethernet frames in IEEE1722 format. The following steps are taken by CAN2ETH for encapsulations of&lt;BR /&gt;the CAN frames:&lt;BR /&gt;• CAN frames are packed into IEEE1722 packet (Compliant to AVTP Time-Synchronous / Non&lt;BR /&gt;time synchronous control format. Packed as ACF CAN Brief /Full messages) or packed into&lt;BR /&gt;UDP packet.&lt;BR /&gt;• LLCE packs the message and put it on the buffers in the SRAM.&lt;BR /&gt;&lt;EM&gt;The packet length is controlled by the configuration of the buffer size.&lt;/EM&gt;&lt;BR /&gt;• Stream ID is constant, Not configurable.&lt;/P&gt;&lt;P&gt;When the buffer size set 134, 7 can frames&amp;nbsp; are packed into AVTP packet(UDP packet) is sent.&lt;/P&gt;&lt;P&gt;If the size of can frames less than seven, the can frames are saved in the buffer.&lt;/P&gt;&lt;P&gt;Can the LLCE send AVTP packet every 1ms?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Mar 2023 09:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1619077#M2546</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2023-03-21T09:41:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1619472#M2561</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We may not be understanding your specific question. If provided with enough information, should be able to.&lt;/P&gt;
&lt;P&gt;Please, help us elaborate more on the specifics of what you are looking for.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Mar 2023 19:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1619472#M2561</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-03-21T19:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1619557#M2567</link>
      <description>Hi,&lt;BR /&gt;CAN2ETH: When the configured frame ID is coming&lt;BR /&gt;into the configured CAN channels, LLCE encapsulates&lt;BR /&gt;the CAN frame into the Ethernet frame in IEEE1722&lt;BR /&gt;format and UDP packet. PFE sends it to the Ethernet.&lt;BR /&gt;The UDP packet length is controlled by the configuration of the buffer size.&lt;BR /&gt;&lt;BR /&gt;Now,the buffer size is full,then the UDP packet will be sent out.&lt;BR /&gt;Is there a time trigger for each MS to send an UDP packet?&lt;BR /&gt;regards,&lt;BR /&gt;jiang&lt;BR /&gt;</description>
      <pubDate>Wed, 22 Mar 2023 00:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1619557#M2567</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2023-03-22T00:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620228#M2583</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The time trigger can be programmed to be done with the FTM module inside the S32G, which then should be able to issue the command to send a UDP packet every ms, if that is the intend of the application.&lt;/P&gt;
&lt;P&gt;Again, could be that we are misunderstanding your requirement, for which we apologize.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Mar 2023 21:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620228#M2583</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-03-22T21:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620340#M2584</link>
      <description>HI，&lt;BR /&gt;CAN to ETH：frame routing on LLCE (CAN to Ethernet Route).&lt;BR /&gt;The CAN packets are sent from Linux and received on the LLCE. The packet&lt;BR /&gt;will then be routed by the LLCE firmware to the output LLCE CAN instance.&lt;BR /&gt;The packet will then be formatted into AVTP format and sent to the PFE. The&lt;BR /&gt;packets sent to the PFE firmware are then captured on the AUX0 interface&lt;BR /&gt;as inbound traffic.&lt;BR /&gt;How many can frames are packed into UDP packet depends on the size of the buffer(or&lt;BR /&gt;The packet length is controlled by the configuration of the buffer size).Is there a time trigger mechanism?&lt;BR /&gt;When 1ms is up, all the can frames packed into the UDP packet and send the UDP packet.&lt;BR /&gt;for example, there is 10 can frames in buffer, 1ms is up ,then send them as one UDP packet,but the buffer size is 1314.&lt;BR /&gt;for example,there is 2 can frames in buffer,1ms is up,then send them as one UDP packet,but the buffer size is 1314.</description>
      <pubDate>Thu, 23 Mar 2023 02:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620340#M2584</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2023-03-23T02:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620531#M2589</link>
      <description>If a time trigger mechanism exists, which file should be modified?or how to modify ?</description>
      <pubDate>Thu, 23 Mar 2023 06:16:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1620531#M2589</guid>
      <dc:creator>fenghua_jiang</dc:creator>
      <dc:date>2023-03-23T06:16:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to can to eth?</title>
      <link>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1621233#M2614</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;We have misunderstood the original request. We apologize for it.&lt;/P&gt;
&lt;P&gt;Under LLCE itself, there is no time mechanism that can be set to send the information on the buffer. Under the current standard firmware, there are only rules that are to be applied (look-up tables) that the module itself will follow. Under the LLCE Firmware User Guide there is no command that the host can send (from what we can see) to apply certain rule on a time basis or simply to activate a rule.&lt;/P&gt;
&lt;P&gt;Still, the following is provided on the LLCE Firmware User Guide [Page 30]:&lt;/P&gt;
&lt;P&gt;"Custom commands from the host may be used to trigger on-demand special actions inside LLCE."&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which are provided on the LLCE FDK, which is a Premium Software. If needed, help us sending this inquiry to your local NXP representative.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 23:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-can-to-eth/m-p/1621233#M2614</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-03-23T23:17:31Z</dc:date>
    </item>
  </channel>
</rss>