<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G POWER UP in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1373104#M252</link>
    <description>&lt;P&gt;We encountered a problem. The communication rate between S32G and SJA1110 was changed to 1G on the RDB2 development board. After a period of normal operation, it was inexplicably unreasonable. I couldn't find the reason. Then I remembered the EVB development board. For the problem, I unplug the 12V power connector of the RDB2 development board and leave it for a while, then plug it in and power it up and the communication is normal.&lt;/P&gt;</description>
    <pubDate>Thu, 18 Nov 2021 03:06:40 GMT</pubDate>
    <dc:creator>longfeiwang</dc:creator>
    <dc:date>2021-11-18T03:06:40Z</dc:date>
    <item>
      <title>S32G POWER UP</title>
      <link>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1373104#M252</link>
      <description>&lt;P&gt;We encountered a problem. The communication rate between S32G and SJA1110 was changed to 1G on the RDB2 development board. After a period of normal operation, it was inexplicably unreasonable. I couldn't find the reason. Then I remembered the EVB development board. For the problem, I unplug the 12V power connector of the RDB2 development board and leave it for a while, then plug it in and power it up and the communication is normal.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Nov 2021 03:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1373104#M252</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-11-18T03:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32G POWER UP</title>
      <link>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1374218#M257</link>
      <description>&lt;P&gt;&lt;BR /&gt;It is not fully clear what exactly was meant with "inexplicably unreasonable" as&lt;BR /&gt;this does not give any hint about what was actually observed. Also, what occurs&lt;BR /&gt;after you power cycle the board depends on the way you updated SJA1110 firmware, &lt;BR /&gt;it can start either 1G or the default 2.5G if you did not program the updates&lt;BR /&gt;FW into the Flash. If you wish more suggestions in regards to the described&lt;BR /&gt;problem, please provide more details on how exactly is was determined that &lt;BR /&gt;it is related to the data rate modifications you have done and what are the&lt;BR /&gt;actually observed symptoms.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Nov 2021 09:14:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1374218#M257</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-11-19T09:14:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32G POWER UP</title>
      <link>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1375501#M266</link>
      <description>&lt;P&gt;If I start with the A core, I can start after the first power-on, but I have to power off for a long time when I start the second time.Or Unplug the DC terminal and plug it in again,it&amp;nbsp;can still start.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Nov 2021 09:03:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-POWER-UP/m-p/1375501#M266</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-11-23T09:03:48Z</dc:date>
    </item>
  </channel>
</rss>