<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Gのトピックbsp build SDK 5.10 for Board:  NXP S32G274A-RDB</title>
    <link>https://community.nxp.com/t5/S32G/bsp-build-SDK-5-10-for-Board-NXP-S32G274A-RDB/m-p/1372335#M248</link>
    <description>&lt;P&gt;hello commuity:&lt;/P&gt;&lt;P&gt;i have a problem :&lt;/P&gt;&lt;P&gt;when i bitbake&amp;nbsp;fsl-image-auto , the bsp yocoto comes out an eorror :&lt;/P&gt;&lt;P&gt;ERROR: ExpansionError during parsing /usr1/bsp1116/fsl-auto-yocto-bsp/sources/meta-alb/recipes-extended/opendds/opendds_git.bb#&lt;/P&gt;&lt;P&gt;bb.data_smart.ExpansionError: Failure expanding variable SRCPV, expression was ${@bb.fetch2.get_srcrev(d)} which triggered exception FetchError: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/usr1/bsp1116/fsl-auto-yocto-bsp/sources/poky/scripts:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/usr/bin/aarch64-fsl-linux:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot/usr/bin/crossscripts:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/usr/sbin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/usr/bin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/sbin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/bin:/usr1/bsp1116/fsl-auto-yocto-bsp/sources/poky/bitbake/bin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/hosttools"; export HOME="/home/ci_proj"; git -c core.fsyncobjectfiles=0 ls-remote &lt;A href="https://github.com/objectcomputing/OpenDDS.git" target="_blank"&gt;https://github.com/objectcomputing/OpenDDS.git&lt;/A&gt; failed with exit code 128, output:&lt;BR /&gt;fatal: unable to access '&lt;A href="https://github.com/objectcomputing/OpenDDS.git/" target="_blank"&gt;https://github.com/objectcomputing/OpenDDS.git/&lt;/A&gt;': Operation timed out after 300024 milliseconds with 0 out of 0 bytes received&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have tried that i can clone the git, ihave no idea why it seems i can not access the git url.&lt;/P&gt;&lt;P&gt;the commands i used here:&lt;/P&gt;&lt;P&gt;mkdir ~/bin&lt;BR /&gt;$: curl &lt;A href="http://commondatastorage.googleapis.com/git-repo-downloads/repo" target="_blank"&gt;http://commondatastorage.googleapis.com/git-repo-downloads/repo&lt;/A&gt; &amp;gt; ~/bin/repo&lt;BR /&gt;$: chmod a+x ~/bin/repo&lt;BR /&gt;$: PATH=${PATH}:~/bin&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Download the Yocto Project Environment into your directory:&lt;BR /&gt;-----------------------------------------------------------&lt;/P&gt;&lt;P&gt;$: mkdir fsl-auto-yocto-bsp&lt;BR /&gt;$: cd fsl-auto-yocto-bsp&lt;BR /&gt;$: repo init -u &lt;A href="https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp" target="_blank"&gt;https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp&lt;/A&gt; -b &lt;SPAN&gt;release/bsp30.0&lt;/SPAN&gt;&lt;BR /&gt;$: repo sync&lt;/P&gt;&lt;P&gt;./sources/meta-alb/scripts/host-prepare.sh&lt;/P&gt;&lt;P&gt;. nxp-setup-alb.sh -m s32g274ardb&lt;/P&gt;&lt;P&gt;bitbake&amp;nbsp;fsl-image-auto&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;what can i do next?&lt;/P&gt;&lt;P&gt;THANKS for any suggestion!&lt;/P&gt;</description>
    <pubDate>Wed, 17 Nov 2021 02:52:41 GMT</pubDate>
    <dc:creator>lily95</dc:creator>
    <dc:date>2021-11-17T02:52:41Z</dc:date>
    <item>
      <title>bsp build SDK 5.10 for Board:  NXP S32G274A-RDB</title>
      <link>https://community.nxp.com/t5/S32G/bsp-build-SDK-5-10-for-Board-NXP-S32G274A-RDB/m-p/1372335#M248</link>
      <description>&lt;P&gt;hello commuity:&lt;/P&gt;&lt;P&gt;i have a problem :&lt;/P&gt;&lt;P&gt;when i bitbake&amp;nbsp;fsl-image-auto , the bsp yocoto comes out an eorror :&lt;/P&gt;&lt;P&gt;ERROR: ExpansionError during parsing /usr1/bsp1116/fsl-auto-yocto-bsp/sources/meta-alb/recipes-extended/opendds/opendds_git.bb#&lt;/P&gt;&lt;P&gt;bb.data_smart.ExpansionError: Failure expanding variable SRCPV, expression was ${@bb.fetch2.get_srcrev(d)} which triggered exception FetchError: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/usr1/bsp1116/fsl-auto-yocto-bsp/sources/poky/scripts:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/usr/bin/aarch64-fsl-linux:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot/usr/bin/crossscripts:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/usr/sbin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/usr/bin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/sbin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/work/aarch64-fsl-linux/opendds/fetcheravoidrecurse-fetcheravoidrecurse/recipe-sysroot-native/bin:/usr1/bsp1116/fsl-auto-yocto-bsp/sources/poky/bitbake/bin:/usr1/bsp1116/fsl-auto-yocto-bsp/build_s32g274ardb/tmp/hosttools"; export HOME="/home/ci_proj"; git -c core.fsyncobjectfiles=0 ls-remote &lt;A href="https://github.com/objectcomputing/OpenDDS.git" target="_blank"&gt;https://github.com/objectcomputing/OpenDDS.git&lt;/A&gt; failed with exit code 128, output:&lt;BR /&gt;fatal: unable to access '&lt;A href="https://github.com/objectcomputing/OpenDDS.git/" target="_blank"&gt;https://github.com/objectcomputing/OpenDDS.git/&lt;/A&gt;': Operation timed out after 300024 milliseconds with 0 out of 0 bytes received&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have tried that i can clone the git, ihave no idea why it seems i can not access the git url.&lt;/P&gt;&lt;P&gt;the commands i used here:&lt;/P&gt;&lt;P&gt;mkdir ~/bin&lt;BR /&gt;$: curl &lt;A href="http://commondatastorage.googleapis.com/git-repo-downloads/repo" target="_blank"&gt;http://commondatastorage.googleapis.com/git-repo-downloads/repo&lt;/A&gt; &amp;gt; ~/bin/repo&lt;BR /&gt;$: chmod a+x ~/bin/repo&lt;BR /&gt;$: PATH=${PATH}:~/bin&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Download the Yocto Project Environment into your directory:&lt;BR /&gt;-----------------------------------------------------------&lt;/P&gt;&lt;P&gt;$: mkdir fsl-auto-yocto-bsp&lt;BR /&gt;$: cd fsl-auto-yocto-bsp&lt;BR /&gt;$: repo init -u &lt;A href="https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp" target="_blank"&gt;https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp&lt;/A&gt; -b &lt;SPAN&gt;release/bsp30.0&lt;/SPAN&gt;&lt;BR /&gt;$: repo sync&lt;/P&gt;&lt;P&gt;./sources/meta-alb/scripts/host-prepare.sh&lt;/P&gt;&lt;P&gt;. nxp-setup-alb.sh -m s32g274ardb&lt;/P&gt;&lt;P&gt;bitbake&amp;nbsp;fsl-image-auto&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;what can i do next?&lt;/P&gt;&lt;P&gt;THANKS for any suggestion!&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 02:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/bsp-build-SDK-5-10-for-Board-NXP-S32G274A-RDB/m-p/1372335#M248</guid>
      <dc:creator>lily95</dc:creator>
      <dc:date>2021-11-17T02:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: bsp build SDK 5.10 for Board:  NXP S32G274A-RDB</title>
      <link>https://community.nxp.com/t5/S32G/bsp-build-SDK-5-10-for-Board-NXP-S32G274A-RDB/m-p/1374506#M259</link>
      <description>&lt;P&gt;Well, a connection timeout means problems with connection to the remote repository.&lt;BR /&gt;It is not possible to tell why it fails in this way in your case, but it is&lt;BR /&gt;not necessarily a problem with the local machine. I have seen&lt;BR /&gt;other intermittent problems with github. Not exactly like this,&lt;BR /&gt;but similar. What can be suggested here is, try later, try from another machine&lt;BR /&gt;or network. Using 'btibake -c fetch opendds' instead of initiating a full target&lt;BR /&gt;build can save you time. Once it completes the fetch, it works with the local&lt;BR /&gt;copy which should be sufficient proceed with building fsl-image-auto. If the &lt;BR /&gt;problem persists, ask your organization network administrator for help in diagnostics.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Nov 2021 17:57:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/bsp-build-SDK-5-10-for-Board-NXP-S32G274A-RDB/m-p/1374506#M259</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-11-19T17:57:38Z</dc:date>
    </item>
  </channel>
</rss>