<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G2: handling the LLCE AIPS RX and TX</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-handling-the-LLCE-AIPS-RX-and-TX/m-p/1615064#M2460</link>
    <description>&lt;P&gt;We are currently working on a custom Firmware for the LLCE on the S32G2, and I have a couple of questions about the AIPS RX and TX modules :&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&amp;nbsp;The actual depth of the FIFOs (i.e., how many elements it can hold) is not mentioned in the RM (e.g.&amp;nbsp;LLCE_BLR_OUT_FIFO_n and TX_ACK_FIFO).&lt;BR /&gt;I calculated it to be&amp;nbsp;&lt;SPAN&gt;242 elements,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;assuming there any reserved memory after the control block,&lt;BR /&gt;and that the whole FIFO i&lt;/SPAN&gt;s 1024 bytes long and the control block is 56 bytes.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;is this correct?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;Is there any Protection method applied on the FIFOs such as ECC that is used on the RAMs of the 4 cores? If not, how to guarantee its behaviour?&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;The actual depth of the TxLUT is not explicitly mentioned, I assume its the same as the RxLUT at 1024 entries, correct?&lt;/LI&gt;&lt;LI&gt;Is there a way to change the searching priority in TxLUT to refer to another parameter such as time of arrival instead of the CAN ID? If not, and I would like to give priority to another message in the middle of the table, does this mean I will have to pop messages and disregard them until I reach the desired message?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Tue, 14 Mar 2023 14:41:12 GMT</pubDate>
    <dc:creator>Mohamed_Abdelalim</dc:creator>
    <dc:date>2023-03-14T14:41:12Z</dc:date>
    <item>
      <title>S32G2: handling the LLCE AIPS RX and TX</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-handling-the-LLCE-AIPS-RX-and-TX/m-p/1615064#M2460</link>
      <description>&lt;P&gt;We are currently working on a custom Firmware for the LLCE on the S32G2, and I have a couple of questions about the AIPS RX and TX modules :&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&amp;nbsp;The actual depth of the FIFOs (i.e., how many elements it can hold) is not mentioned in the RM (e.g.&amp;nbsp;LLCE_BLR_OUT_FIFO_n and TX_ACK_FIFO).&lt;BR /&gt;I calculated it to be&amp;nbsp;&lt;SPAN&gt;242 elements,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;assuming there any reserved memory after the control block,&lt;BR /&gt;and that the whole FIFO i&lt;/SPAN&gt;s 1024 bytes long and the control block is 56 bytes.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;is this correct?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;Is there any Protection method applied on the FIFOs such as ECC that is used on the RAMs of the 4 cores? If not, how to guarantee its behaviour?&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;The actual depth of the TxLUT is not explicitly mentioned, I assume its the same as the RxLUT at 1024 entries, correct?&lt;/LI&gt;&lt;LI&gt;Is there a way to change the searching priority in TxLUT to refer to another parameter such as time of arrival instead of the CAN ID? If not, and I would like to give priority to another message in the middle of the table, does this mean I will have to pop messages and disregard them until I reach the desired message?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Mar 2023 14:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-handling-the-LLCE-AIPS-RX-and-TX/m-p/1615064#M2460</guid>
      <dc:creator>Mohamed_Abdelalim</dc:creator>
      <dc:date>2023-03-14T14:41:12Z</dc:date>
    </item>
  </channel>
</rss>