<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 S32G BSP v28.0 bitbake Error</title>
    <link>https://community.nxp.com/t5/S32G/S32G-BSP-v28-0-bitbake-Error/m-p/1371575#M244</link>
    <description>&lt;P&gt;Dear NXP support:&lt;/P&gt;&lt;P&gt;When I do bitbake fsl-image-base following the BSP user manual . The error below occurs. Could you please help check this? And Thank you in advance.&lt;/P&gt;&lt;P&gt;ERROR: glibc-2.32-r0 do_compile: oe_runmake failed&lt;/P&gt;&lt;P&gt;ERROR: glibc-2.32-r0 do_compile: Execution of '/media/zhuliya/Local/01_S32G/01_BSP/fsl-auto-yocto-bsp/build_s32g274ardb2/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_compile.29378' failed with exit code 1:&lt;/P&gt;&lt;P&gt;make -r PARALLELMFLAGS="-j 24" -C ../git objdir=`pwd` all&lt;/P&gt;&lt;P&gt;make[1]: Entering directory '/media/zhuliya/Local/01_S32G/01_BSP/fsl-auto-yocto-bsp/build_s32g274ardb2/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/git'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Nov 2021 02:45:14 GMT</pubDate>
    <dc:creator>zhuliya</dc:creator>
    <dc:date>2021-11-16T02:45:14Z</dc:date>
    <item>
      <title>S32G BSP v28.0 bitbake Error</title>
      <link>https://community.nxp.com/t5/S32G/S32G-BSP-v28-0-bitbake-Error/m-p/1371575#M244</link>
      <description>&lt;P&gt;Dear NXP support:&lt;/P&gt;&lt;P&gt;When I do bitbake fsl-image-base following the BSP user manual . The error below occurs. Could you please help check this? And Thank you in advance.&lt;/P&gt;&lt;P&gt;ERROR: glibc-2.32-r0 do_compile: oe_runmake failed&lt;/P&gt;&lt;P&gt;ERROR: glibc-2.32-r0 do_compile: Execution of '/media/zhuliya/Local/01_S32G/01_BSP/fsl-auto-yocto-bsp/build_s32g274ardb2/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_compile.29378' failed with exit code 1:&lt;/P&gt;&lt;P&gt;make -r PARALLELMFLAGS="-j 24" -C ../git objdir=`pwd` all&lt;/P&gt;&lt;P&gt;make[1]: Entering directory '/media/zhuliya/Local/01_S32G/01_BSP/fsl-auto-yocto-bsp/build_s32g274ardb2/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/git'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 02:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-BSP-v28-0-bitbake-Error/m-p/1371575#M244</guid>
      <dc:creator>zhuliya</dc:creator>
      <dc:date>2021-11-16T02:45:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32G BSP v28.0 bitbake Error</title>
      <link>https://community.nxp.com/t5/S32G/S32G-BSP-v28-0-bitbake-Error/m-p/1372113#M247</link>
      <description>&lt;P&gt;&lt;BR /&gt;The message you quoted only indicates that glibc failed at the compile stage.&lt;BR /&gt;There must be more errors in the preceding output. Look into &lt;BR /&gt;build_&amp;lt;your_target_board_name&amp;gt;/tmp/log/ to identify the root cause. bitbake&lt;BR /&gt;normally tells you which exactly log file to look at for errors.&lt;/P&gt;
&lt;P&gt;There are no known problems with glibc in BSP 28.0. It is a fundamental &lt;BR /&gt;package everything in the target userspace depends on. Any problem with it&lt;BR /&gt;would have been noticed and fixed long ago.&lt;/P&gt;
&lt;P&gt;If you are just trying to build in a default configuration and with no code &lt;BR /&gt;changes, make sure you are building on a supported Linux host distribution. &lt;BR /&gt;Check the output of host-prepare.sh script to ensure your host is ready to &lt;BR /&gt;build the BSP. If that script completes with no errors, try 'bitbake -c &lt;BR /&gt;cleanall glibc' followed by 'bitbake -c build glibc'. If nothing helps, remove &lt;BR /&gt;all BSP files and directories and install everything anew.&lt;/P&gt;
&lt;P&gt;Note that the BSP 28.0 is obsolete. Consider moving to the most recent BSP 30.0&lt;BR /&gt;Use &lt;A href="https://www.nxp.com/app-autopackagemgr/software-package-manager:AUTO-SW-PACKAGE-MANAGER" target="_self"&gt;Automotive Package Manager&lt;/A&gt; to download it.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 15:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-BSP-v28-0-bitbake-Error/m-p/1372113#M247</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-11-16T15:45:39Z</dc:date>
    </item>
  </channel>
</rss>