<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G2 LLCE-1.0.4 can2eth</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1604166#M2296</link>
    <description>I have tried can2eth in "\S32G_LLCE_1_0_4\sample_app_llce\llce_sample_app_pfe", but still have the same problem</description>
    <pubDate>Thu, 23 Feb 2023 01:52:03 GMT</pubDate>
    <dc:creator>shanlan123</dc:creator>
    <dc:date>2023-02-23T01:52:03Z</dc:date>
    <item>
      <title>S32G2 LLCE-1.0.4 can2eth</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1603565#M2286</link>
      <description>&lt;P&gt;I use the demo "S32G_LLCE_1.0.2-&amp;gt;llce_sample_app_pfe" and Bridge Can0 and Can1 busses on S32G2-rdb2. The project can be compiled normally.However, the code is always waiting for the transmission completion of llce can.&lt;/P&gt;&lt;P&gt;"while(txConfirmationCount &amp;lt; (4 * frame_ctr)) ; /* Wait for TX to avoid overloading the TX buffer */"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 09:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1603565#M2286</guid>
      <dc:creator>shanlan123</dc:creator>
      <dc:date>2023-02-22T09:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 LLCE-1.0.4 can2eth</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1603935#M2291</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We could recommend upgrading to the LLCE v1.0.4, given it could have fixed bugs of the previous version.&lt;/P&gt;
&lt;P&gt;There seems to be a known-issue under the Eth2Can buffer. Can you help us verify if changing "Llce_Af &amp;gt; Eth2Can &amp;gt; Number of Eth2Can Buffer (72 -&amp;gt; 255)" to 73 (default should be 72) and verify you can proceed on the execution of the code?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 17:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1603935#M2291</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-02-22T17:50:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 LLCE-1.0.4 can2eth</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1604166#M2296</link>
      <description>I have tried can2eth in "\S32G_LLCE_1_0_4\sample_app_llce\llce_sample_app_pfe", but still have the same problem</description>
      <pubDate>Thu, 23 Feb 2023 01:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1604166#M2296</guid>
      <dc:creator>shanlan123</dc:creator>
      <dc:date>2023-02-23T01:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 LLCE-1.0.4 can2eth</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1604679#M2303</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Have you tried the provided fix?&lt;/P&gt;&lt;P&gt;As said before, there is a known-issue under that specific example.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Feb 2023 15:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1604679#M2303</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-02-23T15:21:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 LLCE-1.0.4 can2eth</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1747728#M5158</link>
      <description>&lt;P&gt;hello,when transmitting udp package from pc,the 'pfeRxCtr' parameter was increased,but in ZCANPRO there's no can frames were detected,how to solve this?&lt;/P&gt;</description>
      <pubDate>Fri, 27 Oct 2023 08:49:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-LLCE-1-0-4-can2eth/m-p/1747728#M5158</guid>
      <dc:creator>Edieyeee</dc:creator>
      <dc:date>2023-10-27T08:49:12Z</dc:date>
    </item>
  </channel>
</rss>