<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： CAN / CAN-FD to ETH Routing in S32G</title>
    <link>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602769#M2270</link>
    <description>do you solved the problem?&lt;BR /&gt;问题解决了吗</description>
    <pubDate>Tue, 21 Feb 2023 09:45:15 GMT</pubDate>
    <dc:creator>shanlan123</dc:creator>
    <dc:date>2023-02-21T09:45:15Z</dc:date>
    <item>
      <title>CAN / CAN-FD to ETH Routing</title>
      <link>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1601965#M2253</link>
      <description>&lt;P&gt;How can I configure&amp;nbsp;&lt;STRONG&gt;CAN / CAN-FD to ETH Routing&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;please provide me some information&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 12:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1601965#M2253</guid>
      <dc:creator>gautamvarun23</dc:creator>
      <dc:date>2023-02-20T12:10:59Z</dc:date>
    </item>
    <item>
      <title>Re: CAN / CAN-FD to ETH Routing</title>
      <link>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602182#M2260</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We could recommend first looking into the "AN13423 -&amp;nbsp;Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G", which is available on the S32G2 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g2-processors-for-vehicle-networking:S32G2" target="_blank"&gt;S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;)&lt;/P&gt;
&lt;P&gt;There is an example application for this situation provided on the "LLCE Driver + Firmware" for S32G platform. This should be found (once LLCE Driver + Firmware is installed) on the following address:&lt;/P&gt;
&lt;P&gt;"C:\nxp\S32G_LLCE_1_0_4\sample_app_llce\llce_sample_app_pfe"&lt;/P&gt;
&lt;P&gt;Also, more information is provided on the LLCE Firmware User Guide on chapter 1.3.5 Ethernet Communication [v1.0.4]. This should be available (once LLCE Driver + Firmware is installed) on the following address:&lt;/P&gt;
&lt;P&gt;"C:/nxp/S32G_LLCE_1_0_4/firmware/llce_interface/doc/LLCE_firmware_user_guide.pdf"&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 18:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602182#M2260</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-02-20T18:04:36Z</dc:date>
    </item>
    <item>
      <title>回复： CAN / CAN-FD to ETH Routing</title>
      <link>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602769#M2270</link>
      <description>do you solved the problem?&lt;BR /&gt;问题解决了吗</description>
      <pubDate>Tue, 21 Feb 2023 09:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602769#M2270</guid>
      <dc:creator>shanlan123</dc:creator>
      <dc:date>2023-02-21T09:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: CAN / CAN-FD to ETH Routing</title>
      <link>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602990#M2276</link>
      <description>C:\nxp\S32G_LLCE_1_0_4\sample_app_llce\llce_sample_app_pfe.the config of EB Tresos seems wrong.</description>
      <pubDate>Tue, 21 Feb 2023 14:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CAN-CAN-FD-to-ETH-Routing/m-p/1602990#M2276</guid>
      <dc:creator>shanlan123</dc:creator>
      <dc:date>2023-02-21T14:30:15Z</dc:date>
    </item>
  </channel>
</rss>