<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G-VNP-RDB2 Missing SJA1110 interfaces in linux BSP 33.0</title>
    <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/1599032#M2223</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I'm taking a look to&amp;nbsp; &lt;SPAN class=""&gt;LNX PFE Driver User Manual&lt;/SPAN&gt;&amp;nbsp; R.T.M 1.1.0&amp;nbsp; section 4.3.1 to setup the SJA1110 interfaces for the&amp;nbsp;S32G-VNP-RDB2 board. When I follow the steps mentioned in that section:&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;ip addr add 192.198.100.1 dev pfe0 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;ip link set pfe0 up&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Then, I execute&amp;nbsp;&lt;SPAN class=""&gt;ip addr show, the command only shows pfe0 as available interface but no the other three (&lt;A href="mailto:enet_pX@pefx" target="_blank" rel="noopener"&gt;enet_pX@pefx&lt;/A&gt;&amp;nbsp; as shown in the attached picture), do I need to make any other configuration to have the other three interfaces as available?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;My PFE firmware is 1.3, PFE driver 1.0, sja1110_switch.bin and sja1110_uc.bin (from gold vip 1.5).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nicolasespla93_0-1676397486301.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210884i4CDE2548D010BD08/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nicolasespla93_0-1676397486301.png" alt="nicolasespla93_0-1676397486301.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nico&lt;/P&gt;</description>
    <pubDate>Tue, 14 Feb 2023 18:02:03 GMT</pubDate>
    <dc:creator>nicolasespla93</dc:creator>
    <dc:date>2023-02-14T18:02:03Z</dc:date>
    <item>
      <title>S32G-VNP-RDB2 Missing SJA1110 interfaces in linux BSP 33.0</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/1599032#M2223</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I'm taking a look to&amp;nbsp; &lt;SPAN class=""&gt;LNX PFE Driver User Manual&lt;/SPAN&gt;&amp;nbsp; R.T.M 1.1.0&amp;nbsp; section 4.3.1 to setup the SJA1110 interfaces for the&amp;nbsp;S32G-VNP-RDB2 board. When I follow the steps mentioned in that section:&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;ip addr add 192.198.100.1 dev pfe0 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;ip link set pfe0 up&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Then, I execute&amp;nbsp;&lt;SPAN class=""&gt;ip addr show, the command only shows pfe0 as available interface but no the other three (&lt;A href="mailto:enet_pX@pefx" target="_blank" rel="noopener"&gt;enet_pX@pefx&lt;/A&gt;&amp;nbsp; as shown in the attached picture), do I need to make any other configuration to have the other three interfaces as available?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;My PFE firmware is 1.3, PFE driver 1.0, sja1110_switch.bin and sja1110_uc.bin (from gold vip 1.5).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nicolasespla93_0-1676397486301.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210884i4CDE2548D010BD08/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nicolasespla93_0-1676397486301.png" alt="nicolasespla93_0-1676397486301.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nico&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 18:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/1599032#M2223</guid>
      <dc:creator>nicolasespla93</dc:creator>
      <dc:date>2023-02-14T18:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 Missing SJA1110 interfaces in linux BSP 33.0</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/1600666#M2243</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We recommend creating a ticket inside NXP online service for this kind of inquiries, since possible debugging is needed.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 19:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/1600666#M2243</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-02-16T19:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 Missing SJA1110 interfaces in linux BSP 33.0</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/2095442#M13413</link>
      <description>What was the solution to this problem? It would be nice to have it in the driver. Not working around it with vlans for the interface to the users.</description>
      <pubDate>Mon, 12 May 2025 10:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-Missing-SJA1110-interfaces-in-linux-BSP-33-0/m-p/2095442#M13413</guid>
      <dc:creator>Armin1</dc:creator>
      <dc:date>2025-05-12T10:52:30Z</dc:date>
    </item>
  </channel>
</rss>