<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Processor S32G274AABK0VUCT PWM Output channels</title>
    <link>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1589938#M2106</link>
    <description>&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Mon, 30 Jan 2023 16:13:53 GMT</pubDate>
    <dc:creator>gopalakrishna</dc:creator>
    <dc:date>2023-01-30T16:13:53Z</dc:date>
    <item>
      <title>Processor S32G274AABK0VUCT PWM Output channels</title>
      <link>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1586468#M2066</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The currently selected model for our application is S32G2 is S32G274 (Part No :&amp;nbsp;S32G274AABK0VUCT).&lt;/P&gt;&lt;P&gt;The application requires a minimum of 12 PWM output channels, Duty Cycle 10% to 90% and individual channel variable frequency.&lt;/P&gt;&lt;P&gt;Q1 : The No of PWM output channels can configure of S32G274AABK0VUCT?.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gopal&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 07:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1586468#M2066</guid>
      <dc:creator>gopalakrishna</dc:creator>
      <dc:date>2023-01-23T07:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: Processor S32G274AABK0VUCT PWM Output channels</title>
      <link>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1586843#M2069</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;At this moment, S32G2 platform has 2 FlexTimer Modules (FTM) for which each one can handle up to 6 outputs. This should handle 12 independent PWM signals in regards of the Duty Cycle. As for the Frequency of each PWM channel, given there are only 2 FTM's, there should only be 2 possible frequencies (one for each FTM).&lt;/P&gt;
&lt;P&gt;In Summary, each FTM can only handle 1 fixed frequency, but each of its channels can vary the Duty Cycle independently from each other [Figure 300, Page 2012, S32G2 Reference Manual, Rev. 6, 11/2022].&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 22:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1586843#M2069</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-23T22:12:58Z</dc:date>
    </item>
    <item>
      <title>Re: Processor S32G274AABK0VUCT PWM Output channels</title>
      <link>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1589641#M2103</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205137"&gt;@Daniel-Aguirre&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We need &amp;gt;12 PWM/FTM channels for our application, those should be interfaced with&amp;nbsp;S32G274AABK0VUCT.&lt;/P&gt;&lt;P&gt;We are looking for PWM/FTM expanders to interface with&amp;nbsp;S32G274AABK0VUCT via SPI/I2C/.....&lt;/P&gt;&lt;P&gt;Do you have any suggestions for PWM/FTM expander IC's from NXP !&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Murali penta.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 08:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1589641#M2103</guid>
      <dc:creator>muralipenta</dc:creator>
      <dc:date>2023-01-30T08:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: Processor S32G274AABK0VUCT PWM Output channels</title>
      <link>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1589938#M2106</link>
      <description>&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 16:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Processor-S32G274AABK0VUCT-PWM-Output-channels/m-p/1589938#M2106</guid>
      <dc:creator>gopalakrishna</dc:creator>
      <dc:date>2023-01-30T16:13:53Z</dc:date>
    </item>
  </channel>
</rss>