<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IPCF kernel panic in S32G</title>
    <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1580472#M1955</link>
    <description>&lt;P&gt;Hi NXP:&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;hardware:s32g399&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;ipcf branch:bsp32.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I downloaded the ipcf code from source codeaurora.&lt;/SPAN&gt;&lt;SPAN class=""&gt;Then I built the code with reference to readnme.but when i&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;insmod ipc-shm-sample.ko,then there was the kernel panic.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;root@s32g399ardb3:~# insmod ipc-shm-dev.ko&lt;BR /&gt;root@s32g399ardb3:~# insmod ipc-shm-sample.ko&lt;BR /&gt;[ 1238.737196] SError Interrupt on CPU2, code 0xbf000002 -- SError&lt;BR /&gt;[ 1238.737203] CPU: 2 PID: 419 Comm: insmod Tainted: G O 5.10.90-rt60 #5&lt;BR /&gt;[ 1238.737210] Hardware name: Freescale S32G399A (DT)&lt;BR /&gt;[ 1238.737213] pstate: 40000005 (nZcv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 1238.737219] pc : ipc_shm_init+0x408/0x860 [ipc_shm_dev]&lt;BR /&gt;[ 1238.737237] lr : ipc_shm_init+0x7f4/0x860 [ipc_shm_dev]&lt;BR /&gt;[ 1238.737247] sp : ffffffc01412b890&lt;BR /&gt;[ 1238.737250] x29: ffffffc01412b890 x28: ffffffc0088f7380&lt;BR /&gt;[ 1238.737258] x27: 0000000000000100 x26: ffffffc0088ff080&lt;BR /&gt;[ 1238.737264] x25: ffffffc0100c8620 x24: 000000000000002f&lt;BR /&gt;[ 1238.737271] x23: ffffffc0088f7388 x22: ffffffc01412ba50&lt;BR /&gt;[ 1238.737277] x21: 0000000000000000 x20: ffffffc01412ba10&lt;BR /&gt;[ 1238.737284] x19: ffffffc0088f5108 x18: ffffffc010ca83f0&lt;BR /&gt;[ 1238.737293] x17: 0000000000000001 x16: 0000000034100000&lt;BR /&gt;[ 1238.737299] x15: 0000000000000050 x14: ffffffffffffffff&lt;BR /&gt;[ 1238.737304] x13: ffffffc010d3b051 x12: fffffffffffe6967&lt;BR /&gt;[ 1238.737311] x11: ffffffc010ca8408 x10: ffffffc010cb0c90&lt;BR /&gt;[ 1238.737317] x9 : ffffffc01412b890 x8 : 756f635f78745f6c&lt;BR /&gt;[ 1238.737324] x7 : 61636f6c2a2a2a2a x6 : 00000000fffff98d&lt;BR /&gt;[ 1238.737331] x5 : ffffff885f866888 x4 : 0000000000000003&lt;BR /&gt;[ 1238.737337] x3 : 0000000000000027 x2 : 7858ea17e0618f00&lt;BR /&gt;[ 1238.737344] x1 : 0000000000000000 x0 : 0000000000000001&lt;BR /&gt;[ 1238.737350] Kernel panic - not syncing:&lt;BR /&gt;[ 1238.737353] Asynchronous SError Interrupt&lt;BR /&gt;[ 1239.737466] SMP: stopping secondary CPUs&lt;BR /&gt;[ 1239.881750] Kernel Offset: disabled&lt;BR /&gt;[ 1239.885216] CPU features: 0x0040022,2000200c&lt;BR /&gt;[ 1239.889469] Memory Limit: none&lt;BR /&gt;[ 1239.892513] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jan 2023 03:11:32 GMT</pubDate>
    <dc:creator>Quentin2022</dc:creator>
    <dc:date>2023-01-11T03:11:32Z</dc:date>
    <item>
      <title>IPCF kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1580472#M1955</link>
      <description>&lt;P&gt;Hi NXP:&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;hardware:s32g399&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;ipcf branch:bsp32.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I downloaded the ipcf code from source codeaurora.&lt;/SPAN&gt;&lt;SPAN class=""&gt;Then I built the code with reference to readnme.but when i&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;insmod ipc-shm-sample.ko,then there was the kernel panic.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;root@s32g399ardb3:~# insmod ipc-shm-dev.ko&lt;BR /&gt;root@s32g399ardb3:~# insmod ipc-shm-sample.ko&lt;BR /&gt;[ 1238.737196] SError Interrupt on CPU2, code 0xbf000002 -- SError&lt;BR /&gt;[ 1238.737203] CPU: 2 PID: 419 Comm: insmod Tainted: G O 5.10.90-rt60 #5&lt;BR /&gt;[ 1238.737210] Hardware name: Freescale S32G399A (DT)&lt;BR /&gt;[ 1238.737213] pstate: 40000005 (nZcv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 1238.737219] pc : ipc_shm_init+0x408/0x860 [ipc_shm_dev]&lt;BR /&gt;[ 1238.737237] lr : ipc_shm_init+0x7f4/0x860 [ipc_shm_dev]&lt;BR /&gt;[ 1238.737247] sp : ffffffc01412b890&lt;BR /&gt;[ 1238.737250] x29: ffffffc01412b890 x28: ffffffc0088f7380&lt;BR /&gt;[ 1238.737258] x27: 0000000000000100 x26: ffffffc0088ff080&lt;BR /&gt;[ 1238.737264] x25: ffffffc0100c8620 x24: 000000000000002f&lt;BR /&gt;[ 1238.737271] x23: ffffffc0088f7388 x22: ffffffc01412ba50&lt;BR /&gt;[ 1238.737277] x21: 0000000000000000 x20: ffffffc01412ba10&lt;BR /&gt;[ 1238.737284] x19: ffffffc0088f5108 x18: ffffffc010ca83f0&lt;BR /&gt;[ 1238.737293] x17: 0000000000000001 x16: 0000000034100000&lt;BR /&gt;[ 1238.737299] x15: 0000000000000050 x14: ffffffffffffffff&lt;BR /&gt;[ 1238.737304] x13: ffffffc010d3b051 x12: fffffffffffe6967&lt;BR /&gt;[ 1238.737311] x11: ffffffc010ca8408 x10: ffffffc010cb0c90&lt;BR /&gt;[ 1238.737317] x9 : ffffffc01412b890 x8 : 756f635f78745f6c&lt;BR /&gt;[ 1238.737324] x7 : 61636f6c2a2a2a2a x6 : 00000000fffff98d&lt;BR /&gt;[ 1238.737331] x5 : ffffff885f866888 x4 : 0000000000000003&lt;BR /&gt;[ 1238.737337] x3 : 0000000000000027 x2 : 7858ea17e0618f00&lt;BR /&gt;[ 1238.737344] x1 : 0000000000000000 x0 : 0000000000000001&lt;BR /&gt;[ 1238.737350] Kernel panic - not syncing:&lt;BR /&gt;[ 1238.737353] Asynchronous SError Interrupt&lt;BR /&gt;[ 1239.737466] SMP: stopping secondary CPUs&lt;BR /&gt;[ 1239.881750] Kernel Offset: disabled&lt;BR /&gt;[ 1239.885216] CPU features: 0x0040022,2000200c&lt;BR /&gt;[ 1239.889469] Memory Limit: none&lt;BR /&gt;[ 1239.892513] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 03:11:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1580472#M1955</guid>
      <dc:creator>Quentin2022</dc:creator>
      <dc:date>2023-01-11T03:11:32Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1580714#M1960</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;I tried to use ipcf_shem_us, but it also failed, and kernel panic occurred.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Also used is a branch of bsp32, which is version-dependent or other dependent.&lt;/SPAN&gt;&lt;SPAN class=""&gt; I refer to readme build.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;root@s32g399ardb3:/lib/modules/5.10.90-rt60/extra# ./ipc-shm-sample.elf&lt;BR /&gt;[ 819.361925] ipc-shm-uio 40198000.mscm: GIC Rx IRQ = 26&lt;BR /&gt;[ 819.362209] ipc-shm-uio 40198000.mscm: device ready&lt;BR /&gt;[ 819.363185] SError Interrupt on CPU3, code 0xbf000002 -- SError&lt;BR /&gt;[ 819.363195] CPU: 3 PID: 406 Comm: ipc-shm-sample. Tainted: G O 5.10.90-rt60 #7&lt;BR /&gt;[ 819.363201] Hardware name: Freescale S32G399A (DT)&lt;BR /&gt;[ 819.363205] pstate: 60000000 (nZCv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 819.363211] pc : 00000000004028ec&lt;BR /&gt;[ 819.363213] lr : 0000000000402850&lt;BR /&gt;[ 819.363216] sp : 0000007fd6e89e60&lt;BR /&gt;[ 819.363218] x29: 0000007fd6e89e60 x28: 0000000000000000&lt;BR /&gt;[ 819.363229] x27: 0000000000000000 x26: 0000000000000000&lt;BR /&gt;[ 819.363235] x25: 0000000000000000 x24: 0000000000000000&lt;BR /&gt;[ 819.363241] x23: 0000000000000000 x22: 0000000000000000&lt;BR /&gt;[ 819.363250] x21: 00000000004011d0 x20: 0000000000000000&lt;BR /&gt;[ 819.363256] x19: 00000000004046f8 x18: 0000000000000080&lt;BR /&gt;[ 819.363262] x17: 0000007fba31a2c0 x16: 0000007fba3faf18&lt;BR /&gt;[ 819.363268] x15: 0000000000000000 x14: 0000000000000120&lt;BR /&gt;[ 819.363275] x13: 0000007fba3b7108 x12: 0000007fba048150&lt;BR /&gt;[ 819.363281] x11: 00000000003d0f00 x10: 0000007fba3d7e80&lt;BR /&gt;[ 819.363287] x9 : 000000003c0da470 x8 : 0000000000000087&lt;BR /&gt;[ 819.363293] x7 : 0000000000000000 x6 : 0000007fba048220&lt;BR /&gt;[ 819.363299] x5 : 0000007fba0488e0 x4 : 00000000004161c8&lt;BR /&gt;[ 819.363305] x3 : 0000007fba049008 x2 : 0000000000000000&lt;BR /&gt;[ 819.363311] x1 : 0000000000000000 x0 : 0000000000000048&lt;BR /&gt;[ 819.363319] Kernel panic - not syncing:&lt;BR /&gt;[ 819.363321] Asynchronous SError Interrupt&lt;BR /&gt;[ 820.363445] SMP: stopping secondary CPUs&lt;BR /&gt;[ 820.499222] Kernel Offset: disabled&lt;BR /&gt;[ 820.502688] CPU features: 0x0040022,2000200c&lt;BR /&gt;[ 820.506940] Memory Limit: none&lt;BR /&gt;[ 820.509984] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 09:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1580714#M1960</guid>
      <dc:creator>Quentin2022</dc:creator>
      <dc:date>2023-01-11T09:34:57Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581084#M1972</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We assume you are trying to run the IPCF example provided from NXP. Have you done the u-boot configurations explained in the "description.txt" provided in the example?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 19:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581084#M1972</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-11T19:29:03Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581325#M1977</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The uboot is not &lt;SPAN&gt;configurations&amp;nbsp;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;I have a question, do I have to start M core to run sample on linux?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; I just want to see if I can run on linux, I don't care if I can communicate with M core.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jan 2023 03:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581325#M1977</guid>
      <dc:creator>Quentin2022</dc:creator>
      <dc:date>2023-01-12T03:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581338#M1978</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I disable dcach and cleare sram.then i can run sample in linux.&lt;/P&gt;&lt;P&gt;very thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jan 2023 03:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581338#M1978</guid>
      <dc:creator>Quentin2022</dc:creator>
      <dc:date>2023-01-12T03:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF kernel panic</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581826#M1985</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Good to know you got it working.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jan 2023 15:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-kernel-panic/m-p/1581826#M1985</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-12T15:29:52Z</dc:date>
    </item>
  </channel>
</rss>