<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G2 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G2/m-p/1580209#M1949</link>
    <description>&lt;P&gt;Thanks for the information.&lt;/P&gt;
&lt;P&gt;What preparations have you done for the ones that do not work? You can also use S32DS v3.4 to flash the image directly to NOR Flash. Have you tried this option?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Tue, 10 Jan 2023 16:21:32 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-01-10T16:21:32Z</dc:date>
    <item>
      <title>S32G2</title>
      <link>https://community.nxp.com/t5/S32G/S32G2/m-p/1575458#M1878</link>
      <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; When I programmed the NORFlash of S32G2 through flashtool, the following screenshot appeared. I don’t know why?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 07:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2/m-p/1575458#M1878</guid>
      <dc:creator>mudi69</dc:creator>
      <dc:date>2022-12-29T07:45:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2</title>
      <link>https://community.nxp.com/t5/S32G/S32G2/m-p/1576155#M1887</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Which platform are you using? Have you verified that the UART connection is being done through UART0?&lt;/P&gt;
&lt;P&gt;Is this error happening after the algorithm is being uploaded to the platform? Or when it is being returned?&lt;/P&gt;
&lt;P&gt;How have you configured your platform for the Flashing of the external NOR Flash?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 17:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2/m-p/1576155#M1887</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-02T17:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2</title>
      <link>https://community.nxp.com/t5/S32G/S32G2/m-p/1579655#M1940</link>
      <description>Hi NXP&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I am using win10. The problem is that some computers can be programmed, and some computers will have the error in the above picture. We have confirmed that the UART connection is fine. The board we use is S32G-VNP-RDB2.&amp;nbsp;The problem is reported when the algorithm is programmed.</description>
      <pubDate>Tue, 10 Jan 2023 02:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2/m-p/1579655#M1940</guid>
      <dc:creator>mudi69</dc:creator>
      <dc:date>2023-01-10T02:11:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2</title>
      <link>https://community.nxp.com/t5/S32G/S32G2/m-p/1580209#M1949</link>
      <description>&lt;P&gt;Thanks for the information.&lt;/P&gt;
&lt;P&gt;What preparations have you done for the ones that do not work? You can also use S32DS v3.4 to flash the image directly to NOR Flash. Have you tried this option?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jan 2023 16:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2/m-p/1580209#M1949</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-10T16:21:32Z</dc:date>
    </item>
  </channel>
</rss>