<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G Use Case Project FreeRTOS Compilation Error</title>
    <link>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1577657#M1908</link>
    <description>Thank you. After generating the code, it can be compiled normally ~</description>
    <pubDate>Thu, 05 Jan 2023 05:25:54 GMT</pubDate>
    <dc:creator>shoupengchen</dc:creator>
    <dc:date>2023-01-05T05:25:54Z</dc:date>
    <item>
      <title>S32G Use Case Project FreeRTOS Compilation Error</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1564898#M1802</link>
      <description>&lt;P&gt;I create a &amp;nbsp;&lt;STRONG&gt;FreeRTOS_Toggle_Led_Example_S32G399A_M7&lt;/STRONG&gt; project from example.&lt;/P&gt;&lt;P&gt;When I click Compile Project, the error&amp;nbsp;&lt;STRONG&gt;Platform_Types.h ,&amp;nbsp;Clock_Ip.h and&amp;nbsp;Platform_Types.h &lt;FONT color="#FF0000"&gt;does not exist.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I found click project -- properties -- SDKs Pop the &lt;STRONG&gt;tips:&lt;/STRONG&gt;&lt;BR /&gt;&lt;EM&gt;“One or more files from attached SDK， Platform SDK_32XX_2022_03_S32G399A_M7_0 V 3.0.2 are missed in project ”&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know whether the compilation error is related to the SDK. How can I solve this problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;My software is as follows:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;1.S32DS.3.5_b220726_linux.x86_64.bin&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;2. SW32_FreeRTOS_10_4_6_UOS_3_0_2_DS_updatesite_D2204.zip&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;3. SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;4. S32 Design Studile Platform package 3.5.1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;5. S32G development package 3.5.1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;6. S32 Design Studio Platform Tools package.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 04:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1564898#M1802</guid>
      <dc:creator>shoupengchen</dc:creator>
      <dc:date>2022-12-06T04:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32G Use Case Project FreeRTOS Compilation Error</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1565417#M1805</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Have you generated the code with config tools prior to compiling the project? You can right-click on the project itself and go to "S32 Configuration Tools &amp;gt; Open Pins" and should redirect you to another window. Up in the tool bar you should see an "Update Code" option, clicking it should generate the needed files for the project to compile successfully.&lt;/P&gt;
&lt;P&gt;The generated code adds missing modules to the project for it to work. We recommend to import the example again (deleting the previous) and generate the code with config tools.&lt;/P&gt;
&lt;P&gt;At this moment, we have one working platform with that example, meaning should work out of the box.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 20:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1565417#M1805</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2022-12-06T20:20:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32G Use Case Project FreeRTOS Compilation Error</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1577657#M1908</link>
      <description>Thank you. After generating the code, it can be compiled normally ~</description>
      <pubDate>Thu, 05 Jan 2023 05:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/m-p/1577657#M1908</guid>
      <dc:creator>shoupengchen</dc:creator>
      <dc:date>2023-01-05T05:25:54Z</dc:date>
    </item>
  </channel>
</rss>