<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic sja1105p_1-1_cfg.bin in S32G</title>
    <link>https://community.nxp.com/t5/S32G/sja1105p-1-1-cfg-bin/m-p/1362116#M187</link>
    <description>&lt;P&gt;Hi, Community.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am using S32G-PROCEVB-S and S32GRV-PLATEVB in stacked mode. I am testing sja1105 switch. I know that pfe2 is MAC_2 which is connected to sja1105 switch. I think that devices connected with 'A' and 'B' can be communicated. But not communicated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Inchul_1-1635313797400.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160319i0365454BACB3EBC7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Inchul_1-1635313797400.png" alt="Inchul_1-1635313797400.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For your reference, The IP of PC attached 'A' is 169.254.xxx.xxx. I know that this ip address means just linked and doesn't assigned IP address. So, I think that sja1105 is not worked correctly. But as&amp;nbsp;boot log message, I confirmed sja1105 initialization log message.&amp;nbsp;&lt;SPAN&gt;Can I determine that sja1105 is operated with the boot log?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Inchul_2-1635314386779.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160321i5AEB65A144652E3D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Inchul_2-1635314386779.png" alt="Inchul_2-1635314386779.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I need to modify sja1105 configuration, I think that sja1105p_1-1_cfg.bin should is modified. Is it right?&amp;nbsp;If yes, how can I modify sja1105p_1-1_cfg.bin?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Inchul_0-1635313257251.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160318iC347DE762B946F8C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Inchul_0-1635313257251.png" alt="Inchul_0-1635313257251.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you and best regards.&lt;/P&gt;&lt;P&gt;Inchul Lee.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Oct 2021 06:08:30 GMT</pubDate>
    <dc:creator>Inchul</dc:creator>
    <dc:date>2021-10-27T06:08:30Z</dc:date>
    <item>
      <title>sja1105p_1-1_cfg.bin</title>
      <link>https://community.nxp.com/t5/S32G/sja1105p-1-1-cfg-bin/m-p/1362116#M187</link>
      <description>&lt;P&gt;Hi, Community.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am using S32G-PROCEVB-S and S32GRV-PLATEVB in stacked mode. I am testing sja1105 switch. I know that pfe2 is MAC_2 which is connected to sja1105 switch. I think that devices connected with 'A' and 'B' can be communicated. But not communicated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Inchul_1-1635313797400.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160319i0365454BACB3EBC7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Inchul_1-1635313797400.png" alt="Inchul_1-1635313797400.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For your reference, The IP of PC attached 'A' is 169.254.xxx.xxx. I know that this ip address means just linked and doesn't assigned IP address. So, I think that sja1105 is not worked correctly. But as&amp;nbsp;boot log message, I confirmed sja1105 initialization log message.&amp;nbsp;&lt;SPAN&gt;Can I determine that sja1105 is operated with the boot log?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Inchul_2-1635314386779.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160321i5AEB65A144652E3D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Inchul_2-1635314386779.png" alt="Inchul_2-1635314386779.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I need to modify sja1105 configuration, I think that sja1105p_1-1_cfg.bin should is modified. Is it right?&amp;nbsp;If yes, how can I modify sja1105p_1-1_cfg.bin?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Inchul_0-1635313257251.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160318iC347DE762B946F8C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Inchul_0-1635313257251.png" alt="Inchul_0-1635313257251.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you and best regards.&lt;/P&gt;&lt;P&gt;Inchul Lee.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 06:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/sja1105p-1-1-cfg-bin/m-p/1362116#M187</guid>
      <dc:creator>Inchul</dc:creator>
      <dc:date>2021-10-27T06:08:30Z</dc:date>
    </item>
    <item>
      <title>Re: sja1105p_1-1_cfg.bin</title>
      <link>https://community.nxp.com/t5/S32G/sja1105p-1-1-cfg-bin/m-p/1362452#M189</link>
      <description>&lt;P&gt;Instructions on enabling SJA1105 switch on S32G2-VNP-EVB board can be found&lt;BR /&gt;in NXP Automotive BSP 29.0-HF1 User Guide, Sections 5.2.1 and 5.2.3. Pay&lt;BR /&gt;attention to the Note 7 to the port mapping table in Section 5.2.3 which &lt;BR /&gt;directly applies to your test setup.&lt;/P&gt;
&lt;P&gt;The proper way to verify SJA1105 switch operation is to exchange network traffic &lt;BR /&gt;over any subset of it's ports. If you want to use S32G2 on PROCEVB as one of the test&lt;BR /&gt;traffic endpoints, PFE driver has to be loaded. The driver along with it's &lt;BR /&gt;documentation can be found at &lt;A href="https://source.codeaurora.org/external/autobsps32/extra/pfeng" target="_self"&gt;this link.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;you can use any generic Linux network diagnostic utility you are familiar with, &lt;BR /&gt;e.g. &lt;A href="https://man7.org/linux/man-pages/man8/ping.8.html" target="_self"&gt;ping&lt;/A&gt;, &lt;A href="https://man7.org/linux/man-pages/man8/arping.8.html" target="_self"&gt;arping&lt;/A&gt; or &lt;A href="https://man7.org/linux/man-pages/man1/ncat.1.html" target="_self"&gt;ncat&lt;/A&gt; to exchange traffic.&lt;/P&gt;
&lt;P&gt;Reading assigned IP addresses on a connected equipment is not a valid way to&lt;BR /&gt;verify the switch operation because IP assignment mechanisms are OS and configuration&lt;BR /&gt;specific and may or may not involve packet exchange depending on either &lt;BR /&gt;host setup. The simplest approach is probably to connect two Linux hosts to&lt;BR /&gt;the switch ports, configure their network interfaces fully statically and&lt;BR /&gt;use one of the utilities mentioned above. Refer to your host Linux distribution&lt;BR /&gt;documentation on how to configure network interfaces.&lt;/P&gt;
&lt;P&gt;If you need more help with setting up SJA1105 switch on your board, please be sure&lt;BR /&gt;to open a &lt;A href="https://support.nxp.com" target="_self"&gt;Support Case&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 12:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/sja1105p-1-1-cfg-bin/m-p/1362452#M189</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-10-27T12:59:08Z</dc:date>
    </item>
  </channel>
</rss>