<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Implementation IEEE 802.1AS (version 2020) using gPTP at S32G in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Implementation-IEEE-802-1AS-version-2020-using-gPTP-at-S32G/m-p/1570466#M1836</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207880"&gt;@janssen135&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;For the implementation of IEEE 802.1AS, there were no separate applications available but you can refer GMAC loopback example and GMAC reference manual for the same.&lt;/P&gt;
&lt;P&gt;For enabling the 802.1AS, you need to enable the PTP Timestamp offload feature using the "MAC_PTO_Control" register and then after set the 28th bit of the "MAC_Timestamp_Control" register.&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mayank s Patel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 15 Dec 2022 13:00:27 GMT</pubDate>
    <dc:creator>MayanksPatel</dc:creator>
    <dc:date>2022-12-15T13:00:27Z</dc:date>
    <item>
      <title>Implementation IEEE 802.1AS (version 2020) using gPTP at S32G</title>
      <link>https://community.nxp.com/t5/S32G/Implementation-IEEE-802-1AS-version-2020-using-gPTP-at-S32G/m-p/1542460#M1581</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking the NXP documentation for the implementation IEEE 802.1AS (version 2020) using gPTP at S32G.&lt;/P&gt;&lt;P&gt;Can someone tell me where is the documentation?&lt;/P&gt;&lt;P&gt;I am wondering how to implement this topic:&lt;/P&gt;&lt;P&gt;1. using current AUTOSAR version, because the current AUTOSAR version only supports&amp;nbsp;IEEE 802.1AS (version 2011)&lt;/P&gt;&lt;P&gt;2. using non AUTOSAR solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 06:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Implementation-IEEE-802-1AS-version-2020-using-gPTP-at-S32G/m-p/1542460#M1581</guid>
      <dc:creator>janssen135</dc:creator>
      <dc:date>2022-10-24T06:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: Implementation IEEE 802.1AS (version 2020) using gPTP at S32G</title>
      <link>https://community.nxp.com/t5/S32G/Implementation-IEEE-802-1AS-version-2020-using-gPTP-at-S32G/m-p/1570466#M1836</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207880"&gt;@janssen135&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;For the implementation of IEEE 802.1AS, there were no separate applications available but you can refer GMAC loopback example and GMAC reference manual for the same.&lt;/P&gt;
&lt;P&gt;For enabling the 802.1AS, you need to enable the PTP Timestamp offload feature using the "MAC_PTO_Control" register and then after set the 28th bit of the "MAC_Timestamp_Control" register.&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mayank s Patel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 13:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Implementation-IEEE-802-1AS-version-2020-using-gPTP-at-S32G/m-p/1570466#M1836</guid>
      <dc:creator>MayanksPatel</dc:creator>
      <dc:date>2022-12-15T13:00:27Z</dc:date>
    </item>
  </channel>
</rss>