<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックDeveloping UART driver in LLCE</title>
    <link>https://community.nxp.com/t5/S32G/Developing-UART-driver-in-LLCE/m-p/1565627#M1807</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on Developing the UART Driver for LLCE,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have few doubts with respect to the LLCE, i have installed LLCE Package in the s32 design studio and i have installed the .exe file also, so i get example of LIN, CAN, SPI,FLEXRAY in the Package.&lt;/P&gt;&lt;P&gt;in LIN example, it seen that there is function called llce_firmware_load which loads the LLCE enablement bin releases to the SRAM memory.&lt;/P&gt;&lt;P&gt;in case if i am developing my own driver for UART in LLCE, is it needed to load the binary given in example to my project as well?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205137"&gt;@Daniel-Aguirre&lt;/a&gt;#LLCE #S32G274A&lt;/P&gt;&lt;P&gt;&lt;LI-MESSAGE title="Using LLCE as UART in S32G2RM" uid="1545514" url="https://community.nxp.com/t5/S32G/Using-LLCE-as-UART-in-S32G2RM/m-p/1545514#U1545514" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-forum-thread lia-fa-icon lia-fa-forum lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and regarding the UART Driver,&amp;nbsp;&lt;/P&gt;&lt;P&gt;if i am accessing the LINflexD registers in LLCE for UART configuration, we have BDRL registers for data transfer,&lt;/P&gt;&lt;P&gt;will it be okay to use the same for data transfer, or else i need to use the FIFO available in LLCE&lt;/P&gt;</description>
    <pubDate>Wed, 07 Dec 2022 05:53:13 GMT</pubDate>
    <dc:creator>Naveenkumar_Muthusamy</dc:creator>
    <dc:date>2022-12-07T05:53:13Z</dc:date>
    <item>
      <title>Developing UART driver in LLCE</title>
      <link>https://community.nxp.com/t5/S32G/Developing-UART-driver-in-LLCE/m-p/1565627#M1807</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on Developing the UART Driver for LLCE,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have few doubts with respect to the LLCE, i have installed LLCE Package in the s32 design studio and i have installed the .exe file also, so i get example of LIN, CAN, SPI,FLEXRAY in the Package.&lt;/P&gt;&lt;P&gt;in LIN example, it seen that there is function called llce_firmware_load which loads the LLCE enablement bin releases to the SRAM memory.&lt;/P&gt;&lt;P&gt;in case if i am developing my own driver for UART in LLCE, is it needed to load the binary given in example to my project as well?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205137"&gt;@Daniel-Aguirre&lt;/a&gt;#LLCE #S32G274A&lt;/P&gt;&lt;P&gt;&lt;LI-MESSAGE title="Using LLCE as UART in S32G2RM" uid="1545514" url="https://community.nxp.com/t5/S32G/Using-LLCE-as-UART-in-S32G2RM/m-p/1545514#U1545514" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-forum-thread lia-fa-icon lia-fa-forum lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and regarding the UART Driver,&amp;nbsp;&lt;/P&gt;&lt;P&gt;if i am accessing the LINflexD registers in LLCE for UART configuration, we have BDRL registers for data transfer,&lt;/P&gt;&lt;P&gt;will it be okay to use the same for data transfer, or else i need to use the FIFO available in LLCE&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 05:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Developing-UART-driver-in-LLCE/m-p/1565627#M1807</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2022-12-07T05:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: Developing UART driver in LLCE</title>
      <link>https://community.nxp.com/t5/S32G/Developing-UART-driver-in-LLCE/m-p/1566360#M1815</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We have answered through the internal channel.&lt;/P&gt;
&lt;P&gt;Have a great day.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 21:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Developing-UART-driver-in-LLCE/m-p/1566360#M1815</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2022-12-07T21:59:23Z</dc:date>
    </item>
  </channel>
</rss>