<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LLCE CAN/CANFD General Driver(non Autosar) for M7 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-CAN-CANFD-General-Driver-non-Autosar-for-M7/m-p/1557277#M1736</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;At this point in time, only the "LLCE Driver + Firmware" is available under the NXP site. As you are saying, the CAN driver is only available with AUTOSAR compliance.&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
    <pubDate>Mon, 21 Nov 2022 16:35:43 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2022-11-21T16:35:43Z</dc:date>
    <item>
      <title>LLCE CAN/CANFD General Driver(non Autosar) for M7</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-CAN-CANFD-General-Driver-non-Autosar-for-M7/m-p/1556951#M1728</link>
      <description>&lt;P&gt;I'm working on the LLCE CAN/CANFD communication implement in a project for the M7 cores. I installed&amp;nbsp;S32DS.3.4_LLCE_Addon_updatesite_1.0.4_signed.zip in the S32DS 3.4. I created a llce CAN project from the sdk, but I can only find the example for autosar. The llce driver is included in the MCAL.&lt;/P&gt;&lt;P&gt;Is there a general LLCE CAN/CANFD demo (non Autosar)for M7 core? Or how can I add the driver in the drivers component for a non Autosar application ?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 06:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-CAN-CANFD-General-Driver-non-Autosar-for-M7/m-p/1556951#M1728</guid>
      <dc:creator>yqlau</dc:creator>
      <dc:date>2022-11-21T06:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE CAN/CANFD General Driver(non Autosar) for M7</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-CAN-CANFD-General-Driver-non-Autosar-for-M7/m-p/1557277#M1736</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;At this point in time, only the "LLCE Driver + Firmware" is available under the NXP site. As you are saying, the CAN driver is only available with AUTOSAR compliance.&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 16:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-CAN-CANFD-General-Driver-non-Autosar-for-M7/m-p/1557277#M1736</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2022-11-21T16:35:43Z</dc:date>
    </item>
  </channel>
</rss>