<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： S32G2 Enabling Multicore Application in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408309#M16739</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;1. Yes, only ATF and u-boot were booted on the A core. The UART did not have any output.&lt;/P&gt;&lt;P&gt;2. The M core ran the LLCE_CAN and Lpspi programs, integrating the "Can_Llce_DS_Loopback_S32G274A_M7" and "Lpspi_Ip_Transfer_S32G274A_M7" routines. It first used SPI communication and then ran LLCE_CAN.&lt;/P&gt;&lt;P&gt;I would like to add some more information:&lt;/P&gt;&lt;P&gt;1. The entire process was carried out according to AN13750, with only a few differences: I used BSP42 and S32DS3.5 versions; I replaced the IPCF routines with LLCE_CAN and only configured M7_0.&lt;/P&gt;&lt;P&gt;2. I compiled BSP42 using Yocto and generated the.sdcard. After importing the SD card, Linux could be started.&lt;/P&gt;&lt;P&gt;3. I compiled the u-boot and ATF of BSP42 according to the "AN13750, 4. Prepare images for Cortex-A53 cores" section. After re-importing the.sdcard and fip.s32 into the SD card, Linux could still be started in SD mode. However, when importing the bootloader and fip.bin into the norflash, no output was obtained.&lt;/P&gt;&lt;P&gt;4. I burned a UART routine for the M7 core separately in the norflash, and Linux could be started and outputted. This proved that the burning tool and norflash were normal.&lt;/P&gt;&lt;P&gt;5. I burned the LLCE_CAN program separately in the norflash. The program did not run, and there was no CAN output.&lt;/P&gt;&lt;P&gt;6. I attempted to configure the EB bootloader to start A53 separately, but re-burning the norflash still did not result in any output.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Aug 2026 02:30:23 GMT</pubDate>
    <dc:creator>zhipeng</dc:creator>
    <dc:date>2026-08-26T02:30:23Z</dc:date>
    <item>
      <title>S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403079#M16725</link>
      <description>&lt;P&gt;Hi, nxp&amp;nbsp;fellows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are preparing to use multi-core to run programs in the S32G274A chip, using A53 to run Linux and M7 to run LLCE_CAN.&lt;/P&gt;&lt;P&gt;We referred to "Enabling Multicore Application on S32G2 using S32G2 Platform Software Integration", according to 5.2. Configure the bootloader, installed the recommended software packages, and configured them following the steps.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_7-1786181958976.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394034i7FC881D235D6A1A0/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_7-1786181958976.png" alt="zhipeng_7-1786181958976.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There is an error in 5.3. Build The Bootloader during compilation.&lt;/P&gt;&lt;P&gt;The launch.bat file was edited.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_0-1786182860528.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394035iBABD3835BE1E4364/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_0-1786182860528.png" alt="zhipeng_0-1786182860528.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;An error occurred after running launch.bat. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_0-1786180508617.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394026iFD0C0B33356DC106/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_0-1786180508617.png" alt="zhipeng_0-1786180508617.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After commenting out the relevant code.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_5-1786181360466.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394032i8F6220B9AE4555F2/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_5-1786181360466.png" alt="zhipeng_5-1786181360466.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_2-1786180921774.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394029iB2667C5AC086A76E/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_2-1786180921774.png" alt="zhipeng_2-1786180921774.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I found the CryptoDal.h file in the installation directory.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_4-1786181305215.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394031i9A78379D98315D4B/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_4-1786181305215.png" alt="zhipeng_4-1786181305215.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_6-1786181450684.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394033iE5EC95B5CCCB994F/image-size/small?v=v2&amp;amp;px=200" role="button" title="zhipeng_6-1786181450684.png" alt="zhipeng_6-1786181450684.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Where could there be any mistakes?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 08 Aug 2026 09:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403079#M16725</guid>
      <dc:creator>zhipeng</dc:creator>
      <dc:date>2026-08-08T09:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403132#M16726</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;zhipeng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For your issue, will there be an error if the following contents are added? Is it commenting out won't cause an error?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joey_z_0-1786328574726.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394045iA063ACB7F8AE2FA0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joey_z_0-1786328574726.png" alt="Joey_z_0-1786328574726.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Joey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Aug 2026 02:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403132#M16726</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-08-10T02:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403200#M16728</link>
      <description>&lt;P&gt;Hi, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, after adding, it will show "undeclared" on the third image.&lt;/P&gt;&lt;P&gt;Commenting out will show "No such file or directory", on the fifth image.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_1-1786347067301.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394063i5D0CF48B98CEDECB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_1-1786347067301.png" alt="zhipeng_1-1786347067301.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;"CryptoDal.h" is located in D:\NXP\Integration_Reference_Examples_S32G2_2022_06\code\framework\realtime\bsw\dal\cryptodal\generic\include&lt;/P&gt;&lt;P&gt;"Hse_Ip.h" is located in D:\NXP\SW32G_RTD_4.4_3.0.2_HF01\eclipse\plugins\Crypto_TS_T40D11M30I2R0\include&lt;/P&gt;&lt;P&gt;I have found both files in their respective folders, and the file paths are also written in launch.bat.&lt;/P&gt;&lt;P&gt;The current problem feels like the plugin path was not included during the compilation process.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
      <pubDate>Mon, 10 Aug 2026 07:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403200#M16728</guid>
      <dc:creator>zhipeng</dc:creator>
      <dc:date>2026-08-10T07:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403257#M16730</link>
      <description>&lt;P&gt;Hi，&lt;SPAN&gt;zhipeng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Is Secure Boot enabled in the configuration? Try to enable the Secure boot, check if the issue will&amp;nbsp;disappear.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joey_z_2-1786353784256.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394079iD96FF2822F40DD41/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joey_z_2-1786353784256.png" alt="Joey_z_2-1786353784256.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Aug 2026 09:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2403257#M16730</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-08-10T09:46:54Z</dc:date>
    </item>
    <item>
      <title>回复： S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408106#M16737</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The previous bootloader compilation was successful. Now, I have written the image into the NOR flash and after booting, there is no output on the UART.&lt;/P&gt;&lt;P&gt;I referred to AN13750. Here are my operation steps:&lt;/P&gt;&lt;P&gt;I followed the "S32G2_LinuxBSP_42.0_User_Manual.pdf", and installed u-boot bsp42.0-2022.04 and ATF bsp42.0-2.10 in Ubuntu 20.&lt;/P&gt;&lt;P&gt;I modified s32_mmc.c and s32_common.mk according to 0001-fip-align-and-mmc-init.patch.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_0-1787646642108.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395291iB07CCA25C7B096F1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_0-1787646642108.png" alt="zhipeng_0-1787646642108.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_1-1787646670172.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395292iA140460B1922588C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_1-1787646670172.png" alt="zhipeng_1-1787646670172.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_2-1787646683855.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395293iEF88B742A45D0662/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_2-1787646683855.png" alt="zhipeng_2-1787646683855.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I compiled u-boot and ATF.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;make CROSS_COMPILE=/opt/S32G/arm-gnu-toolchain-11.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- ARCH=aarch64 PLAT=s32g274ardb2 BL33=../u-boot/u-boot-nodtb.bin

Image Layout
DCD: Offset: 0x200 Size: 0x1c
IVT: Offset: 0x1000 Size: 0x100
AppBootCode Header: Offset: 0x1200 Size: 0x40
Application: Offset: 0x1240 Size: 0x33e00

Boot Core: A53_0
IVT Location: SD/eMMC
Load address: 0x342f8f00
Entry point: 0x34302000&lt;/LI-CODE&gt;&lt;P&gt;I wrote the fip.s32 onto the SD card. After replacing the fip, the SD card was still able to boot, and the date of the u-boot changed.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot 2022.04-00213-g5a6f62071f (Aug 24 2026 - 10:35:21 +0800)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Configure the bootloader.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_3-1787647428751.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395294i69C102778826AD2A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_3-1787647428751.png" alt="zhipeng_3-1787647428751.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_4-1787647490093.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395295iAEA9616373378535/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_4-1787647490093.png" alt="zhipeng_4-1787647490093.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_5-1787647533346.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395296i59C4D986EA6CB522/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_5-1787647533346.png" alt="zhipeng_5-1787647533346.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_6-1787647547310.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395297i1673AC94541DAB94/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_6-1787647547310.png" alt="zhipeng_6-1787647547310.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Generate S32G Boot Image&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_7-1787647657415.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395298iA159AD1CC1646987/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_7-1787647657415.png" alt="zhipeng_7-1787647657415.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;select the bt_m7_blob.bin to write it to the address 0x0.&lt;BR /&gt;select the fip.bin to write it to the address 0x100000.&lt;BR /&gt;select theS32G274A_M7.bin to write it to the address 0x200000.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhipeng_8-1787647865193.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395299i7CBECD21737C63CD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zhipeng_8-1787647865193.png" alt="zhipeng_8-1787647865193.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now neither the UART nor the CAN is responding. Please help me analyze the situation.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 08:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408106#M16737</guid>
      <dc:creator>zhipeng</dc:creator>
      <dc:date>2026-08-25T08:57:05Z</dc:date>
    </item>
    <item>
      <title>回复： S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408179#M16738</link>
      <description>&lt;P&gt;Hi,ZhiPeng&lt;/P&gt;
&lt;P&gt;Thank you for your information.&lt;/P&gt;
&lt;P&gt;Could you share more information with me?&lt;/P&gt;
&lt;P&gt;1.Do you only boot ATF and uboot on A core? Have any output on the UART of A core?&lt;/P&gt;
&lt;P&gt;2.What is the M core function? is it about the UART/CAN function?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 10:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408179#M16738</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-08-25T10:10:49Z</dc:date>
    </item>
    <item>
      <title>回复： S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408309#M16739</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;1. Yes, only ATF and u-boot were booted on the A core. The UART did not have any output.&lt;/P&gt;&lt;P&gt;2. The M core ran the LLCE_CAN and Lpspi programs, integrating the "Can_Llce_DS_Loopback_S32G274A_M7" and "Lpspi_Ip_Transfer_S32G274A_M7" routines. It first used SPI communication and then ran LLCE_CAN.&lt;/P&gt;&lt;P&gt;I would like to add some more information:&lt;/P&gt;&lt;P&gt;1. The entire process was carried out according to AN13750, with only a few differences: I used BSP42 and S32DS3.5 versions; I replaced the IPCF routines with LLCE_CAN and only configured M7_0.&lt;/P&gt;&lt;P&gt;2. I compiled BSP42 using Yocto and generated the.sdcard. After importing the SD card, Linux could be started.&lt;/P&gt;&lt;P&gt;3. I compiled the u-boot and ATF of BSP42 according to the "AN13750, 4. Prepare images for Cortex-A53 cores" section. After re-importing the.sdcard and fip.s32 into the SD card, Linux could still be started in SD mode. However, when importing the bootloader and fip.bin into the norflash, no output was obtained.&lt;/P&gt;&lt;P&gt;4. I burned a UART routine for the M7 core separately in the norflash, and Linux could be started and outputted. This proved that the burning tool and norflash were normal.&lt;/P&gt;&lt;P&gt;5. I burned the LLCE_CAN program separately in the norflash. The program did not run, and there was no CAN output.&lt;/P&gt;&lt;P&gt;6. I attempted to configure the EB bootloader to start A53 separately, but re-burning the norflash still did not result in any output.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Aug 2026 02:30:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2408309#M16739</guid>
      <dc:creator>zhipeng</dc:creator>
      <dc:date>2026-08-26T02:30:23Z</dc:date>
    </item>
    <item>
      <title>回复： S32G2 Enabling Multicore Application</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2409170#M16745</link>
      <description>&lt;P&gt;Hi，zhipeng&lt;/P&gt;
&lt;P&gt;1. I understand that your LLCE_CAN is running on the M core. Please test the bootloader's startup of this program M core independently. During the startup process, do not load the A core Image.&lt;BR /&gt;2. In your testing, the bootloader can start the UART program of M7, but can it cannot start the LLCE_CAN?&lt;BR /&gt;3. Have you tried using the bootloader to only boot the A53?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have created a new case for this issue in the system in Chinese, the case number is the: 01000969. This will facilitate communication.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 09:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Enabling-Multicore-Application/m-p/2409170#M16745</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-08-28T09:35:16Z</dc:date>
    </item>
  </channel>
</rss>