<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: llcecan question</title>
    <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2376345#M16405</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. LLCE FW version is&amp;nbsp;HHFF_2A [REL_LLCE1_0_6|BLD_RDC2303221606].&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Tests were only conducted on the bsp38.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.&amp;nbsp;Only the llcecan was subjected to stress testing without frame loss. However, when stress testing all 8 can channels simultaneously, frame loss occurred (the software used for the 4-channel llce test and the 8-channel can test is the same).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4. canoe busload is 55%,&amp;nbsp;&amp;nbsp;the average CPU load during&amp;nbsp;8-channel can test is 60%, and during4-channel llce test is37%&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jun 2026 02:29:02 GMT</pubDate>
    <dc:creator>ZHANGBOWEN</dc:creator>
    <dc:date>2026-06-04T02:29:02Z</dc:date>
    <item>
      <title>llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2374717#M16389</link>
      <description>&lt;P&gt;hi nxp team:&lt;/P&gt;&lt;P&gt;Test hardware: s32g274&lt;BR /&gt;Software version: bsp38&lt;/P&gt;&lt;P&gt;can setting： ip link set llcecan（0~3） type can \&lt;BR /&gt;bitrate 500000 \&lt;BR /&gt;sample-point 0.8 \&lt;BR /&gt;dbitrate 2000000 \&lt;BR /&gt;dsample-point 0.7 \&lt;BR /&gt;fd on&lt;BR /&gt;test case：&lt;BR /&gt;1: Vector v1640 can1 can be connected to can0~can3 of s32g, and can2 can be connected to llce_can0~llce_can3 of s32g&lt;BR /&gt;2: vector1640 sends can data, and s32g receives can data.&lt;BR /&gt;3: Check whether the sent and received data frames are consistent.&lt;BR /&gt;Test results：&lt;BR /&gt;1: Data frames are lost in llce_can0~llce_can3, but not in can0~can3.&lt;BR /&gt;The reference image is as follows&lt;BR /&gt;Figure 1: We can see that v1640 can1 sent a total of 1,823,705 frames, and in Figure 2, s32g274 can0~can3 received 1,823,705 frames without any frame loss.&lt;BR /&gt;We can observe that the total number of frames sent by v1640 can2 is 1,845,947, while the corresponding number of frames received by s32g274 llce_can0~llce_can3 is approximately 1,845,887. There is a loss of 60 frames.&lt;/P&gt;&lt;P&gt;When the CPU load is relatively high, the frame loss situation worsens. Is it possible to increase LLCE_CAN_MAX_RX_MB to reduce the cpu load. as the same time, How to solve the frame loss problem? Are there any optimization items?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZHANGBOWEN_0-1780368083252.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387473i242807587E68B6B7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZHANGBOWEN_0-1780368083252.png" alt="ZHANGBOWEN_0-1780368083252.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZHANGBOWEN_1-1780368090168.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387474i4EAEA9D5CE9FBFC1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZHANGBOWEN_1-1780368090168.png" alt="ZHANGBOWEN_1-1780368090168.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jun 2026 02:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2374717#M16389</guid>
      <dc:creator>ZHANGBOWEN</dc:creator>
      <dc:date>2026-06-02T02:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2374869#M16392</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259184"&gt;@ZHANGBOWEN&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;From the description shared, seems the frames lost when system load is high.&lt;/P&gt;
&lt;P&gt;I suggest&amp;nbsp;&lt;SPAN&gt;trying to change the value of&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;LLCE_CAN_MAX_RX_MB in&lt;/SPAN&gt;&lt;/P&gt;
&lt;ARTICLE data-content="[{&amp;quot;type&amp;quot;:&amp;quot;block&amp;quot;,&amp;quot;id&amp;quot;:&amp;quot;mYvj-1780372440423&amp;quot;,&amp;quot;name&amp;quot;:&amp;quot;paragraph&amp;quot;,&amp;quot;data&amp;quot;:{},&amp;quot;nodes&amp;quot;:[{&amp;quot;type&amp;quot;:&amp;quot;text&amp;quot;,&amp;quot;id&amp;quot;:&amp;quot;n4Qj-1780372440421&amp;quot;,&amp;quot;leaves&amp;quot;:[{&amp;quot;text&amp;quot;:&amp;quot;drivers/net/can/llce/llce_can_common.c&amp;quot;,&amp;quot;marks&amp;quot;:[{&amp;quot;type&amp;quot;:&amp;quot;bold&amp;quot;},{&amp;quot;type&amp;quot;:&amp;quot;color&amp;quot;,&amp;quot;value&amp;quot;:&amp;quot;#333f48&amp;quot;},{&amp;quot;type&amp;quot;:&amp;quot;backgroundColor&amp;quot;,&amp;quot;value&amp;quot;:&amp;quot;rgb(255,&amp;nbsp;255,&amp;nbsp;255)&amp;quot;},{&amp;quot;type&amp;quot;:&amp;quot;fontSize&amp;quot;,&amp;quot;value&amp;quot;:16}]}]}],&amp;quot;state&amp;quot;:{}}]"&gt;
&lt;DIV&gt;&lt;SPAN&gt;drivers/net/can/llce/llce_can_common.c&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp; with new value such as&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;32 or 64, then rebuild the kernel to have another test, to check if there are still issues existed in your test.&lt;/SPAN&gt;&lt;/DIV&gt;
&lt;/ARTICLE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jun 2026 07:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2374869#M16392</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-06-02T07:46:22Z</dc:date>
    </item>
    <item>
      <title>Re: llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2375388#M16396</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;After I modified LLCE_CAN_MAX_RX_MB to 64 and 128, the CPU load did not decrease or the decrease was not noticeable, making it difficult to observe.&amp;nbsp;And the frame loss phenomenon of llcecan still exists&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jun 2026 01:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2375388#M16396</guid>
      <dc:creator>ZHANGBOWEN</dc:creator>
      <dc:date>2026-06-03T01:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2375616#M16398</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259184"&gt;@ZHANGBOWEN&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;In order for investigating on the issue further, firstly I wish reproducing it on local RDB2.&lt;/P&gt;
&lt;P&gt;Would you mind clarifying the following:&lt;/P&gt;
&lt;P&gt;1. Which version LLCE FW is used in your test?&lt;/P&gt;
&lt;P&gt;2. Have you ever tested it with other version BSP? If so, same results?&lt;/P&gt;
&lt;P&gt;3. Could the frame loss only occurred when doing benchmark via 8 CAN channels as described? May I know if you had done some pressure test on only LLCE CAN interfaces? Any simplified testing setup existed that could reproduce the issue?&lt;/P&gt;
&lt;P&gt;4. What is the test load for the test? What is the throughput value when frame loss are found? What is the average CPU load during the test?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jun 2026 08:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2375616#M16398</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-06-03T08:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2376345#M16405</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. LLCE FW version is&amp;nbsp;HHFF_2A [REL_LLCE1_0_6|BLD_RDC2303221606].&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Tests were only conducted on the bsp38.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.&amp;nbsp;Only the llcecan was subjected to stress testing without frame loss. However, when stress testing all 8 can channels simultaneously, frame loss occurred (the software used for the 4-channel llce test and the 8-channel can test is the same).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4. canoe busload is 55%,&amp;nbsp;&amp;nbsp;the average CPU load during&amp;nbsp;8-channel can test is 60%, and during4-channel llce test is37%&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 02:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2376345#M16405</guid>
      <dc:creator>ZHANGBOWEN</dc:creator>
      <dc:date>2026-06-04T02:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2377188#M16416</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259184"&gt;@ZHANGBOWEN&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1. Would you please help to check if there is simpler way for reproducing the issue?&lt;/P&gt;
&lt;P&gt;2. I understand that currently it only occurred on 8 channel test, may I know if you have only 4+4 CAN interface on your board? is it possible only testing on LLCE to reproduce the issue?(say 4+ channels on LLCE interface)&lt;/P&gt;
&lt;P&gt;On RDB2, there are only 2 FlexCAN, but with 16 LLCE CAN available, if a simplified test method would be provided, then it would be very helpful.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jun 2026 03:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2377188#M16416</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-06-05T03:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: llcecan question</title>
      <link>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2378286#M16427</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;(1)&amp;nbsp;I ran our project program on the development board. It's not very convenient for me to send you the entire file for testing. You can directly use canoe to connect llcecan0 to llcecan3 without running any programs to conduct a streaming test at 8,000 frames per second.&lt;/P&gt;&lt;P&gt;(2)&amp;nbsp;It only streams 4 channels of llcecan at 8,000 frames per second. Even after sending 10 million frames, there will be no frame loss&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 10:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llcecan-question/m-p/2378286#M16427</guid>
      <dc:creator>ZHANGBOWEN</dc:creator>
      <dc:date>2026-06-08T10:07:44Z</dc:date>
    </item>
  </channel>
</rss>