<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multicore boot on S32G3 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2366615#M16342</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252302"&gt;@wael_b&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply&lt;/P&gt;
&lt;P&gt;The GVIP you tested are not compatible with the RTD used, as what I mentioned, GVIP1.12 is compatible with the RTD you tried.&lt;/P&gt;
&lt;P&gt;If using GVIP1.13. then the suggested RTD is 5.0 version, while BSP43 is used, for details of the software dependency, I suggest referencing the release notes and user guide of the GoldVIP version you tested.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 18 May 2026 02:46:39 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2026-05-18T02:46:39Z</dc:date>
    <item>
      <title>Multicore boot on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2364775#M16327</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to boot both M7 and A53.&amp;nbsp;&lt;BR /&gt;What are the required packages for this?&lt;BR /&gt;Is there a documentation I can follow?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dhafer&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 09:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2364775#M16327</guid>
      <dc:creator>dhafer_benchikha</dc:creator>
      <dc:date>2026-05-13T09:44:15Z</dc:date>
    </item>
    <item>
      <title>Re: Multicore boot on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2364924#M16330</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262710"&gt;@dhafer_benchikha&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. For booting A53 cores, Linux BSP is provisioned by NXP.&lt;/P&gt;
&lt;P&gt;2. For M7 usage, the RTD(and also some other related software packages including PFE driver) is provided by NXP.&lt;/P&gt;
&lt;P&gt;For simultaneously booting the system with both A53 and M7 core brought up.&lt;/P&gt;
&lt;P&gt;I suggest directly following the way introduced from&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13750" rel="nofollow noopener noreferrer" target="_blank"&gt;AN13750&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 13:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2364924#M16330</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-13T13:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: Multicore boot on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2364951#M16331</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We are working with &lt;STRONG&gt;S32DS 3.5&lt;/STRONG&gt; on &lt;STRONG&gt;S32G399&lt;/STRONG&gt;! my application on M7 was made using the &lt;STRONG&gt;SW32G_RTD_4.4_4.0.2_P10_D2405&lt;/STRONG&gt;!&lt;BR /&gt;I followed that pdf and I downloaded &lt;STRONG&gt;SW32G_RTD_4.4_3.0.2_HF01_D2204.exe&lt;/STRONG&gt; and installed it and added the updatesite zip to s32ds.&lt;BR /&gt;I added the plugins from &lt;STRONG&gt;SW32G_RTD_4.4_3.0.2_HF01&lt;/STRONG&gt; and added it to EB tresos plugins!&lt;BR /&gt;I downloaded and installed &lt;STRONG&gt;Platform_Software_Integration_S32G3_2023_02.exe&lt;/STRONG&gt; but when i imported the bootloader project in tresos, when loading the configuration I got plugin not installed error "&lt;STRONG&gt;*_TS_T40D11M&lt;U&gt;40I0R0&lt;/U&gt;&lt;/STRONG&gt;".&lt;BR /&gt;If i uninstall &lt;STRONG&gt;Platform_Software_Integration_S32G3_2023_02&lt;/STRONG&gt; and install &lt;STRONG&gt;Platform_Software_Integration_S32G3_2022_12.exe&lt;/STRONG&gt;! i got the same errors on modules but with different reference "&lt;STRONG&gt;*_TS_T40D11M&lt;U&gt;30I4R0&lt;/U&gt;&lt;/STRONG&gt;".&lt;BR /&gt;the plugins i have in EB Tresos are referenced "&lt;STRONG&gt;*_TS_T40D11M&lt;U&gt;30I2R0&lt;/U&gt;&lt;/STRONG&gt;" and "&lt;STRONG&gt;*_TS_T40D11M&lt;U&gt;40I2R0&lt;/U&gt;&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;what do you suggest in this case?&lt;BR /&gt;Many thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 14:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2364951#M16331</guid>
      <dc:creator>wael_b</dc:creator>
      <dc:date>2026-05-13T14:04:49Z</dc:date>
    </item>
    <item>
      <title>Re: Multicore boot on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2365329#M16335</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252302"&gt;@wael_b&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your clarification.&lt;/P&gt;
&lt;P&gt;1. AN13750 is originally released several years ago, which is targeted with S32G2 and specified software packages version.&lt;/P&gt;
&lt;P&gt;2. With the specified software version and RDB2, it could be also be regarded as a hands-on guide, however, for S32G3(RDB3 for example), it may not be directly followed since the SW/HW differences. But the operation method/booting steps are the same for S32G3, you may need reference the AN13750 and made some changes to make it compatible to the S32G3 related software packages used.&lt;/P&gt;
&lt;P&gt;3. From my experience, I suggest directly referencing the ways/steps provided by AN13750 on your S32G3 case, and try using the following software packages: the Bootloader from GoldVIP1.12, with&amp;nbsp;&lt;STRONG&gt;SW32G_RTD_4.4_4.0.2_HF03,&amp;nbsp; IPCF4.10, BSP41/42&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;to have another try.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 08:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2365329#M16335</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-14T08:08:49Z</dc:date>
    </item>
    <item>
      <title>Re: Multicore boot on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2365434#M16336</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your response!&lt;/P&gt;&lt;P&gt;I tried with SW32G_RTD_4.4_4.0.2_HF03 and &lt;STRONG&gt;GoldVIP1.13&lt;/STRONG&gt;, &lt;STRONG&gt;GoldVIP1.14&lt;/STRONG&gt; and &lt;STRONG&gt;GoldVIP1.15&lt;/STRONG&gt; because I couldn't find GoldVIP1.12 but still facing the same issues in EB Tresos as shown in the screenshots.&lt;/P&gt;&lt;P&gt;Also, IPCF4.10 doesn't exist, so I have the&amp;nbsp;IPCF4.11.&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 10:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2365434#M16336</guid>
      <dc:creator>wael_b</dc:creator>
      <dc:date>2026-05-14T10:16:40Z</dc:date>
    </item>
    <item>
      <title>Re: Multicore boot on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2366615#M16342</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252302"&gt;@wael_b&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply&lt;/P&gt;
&lt;P&gt;The GVIP you tested are not compatible with the RTD used, as what I mentioned, GVIP1.12 is compatible with the RTD you tried.&lt;/P&gt;
&lt;P&gt;If using GVIP1.13. then the suggested RTD is 5.0 version, while BSP43 is used, for details of the software dependency, I suggest referencing the release notes and user guide of the GoldVIP version you tested.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 May 2026 02:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Multicore-boot-on-S32G3/m-p/2366615#M16342</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-18T02:46:39Z</dc:date>
    </item>
  </channel>
</rss>