<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: s32g2 QNX PFE driver</title>
    <link>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345861#M16216</link>
    <description>Hi Joey,&lt;BR /&gt;I am using the customer board, and the CPU is S32G274A.&lt;BR /&gt;Yes, currently only core A is running. The QNX system is started via Uboot. If the above modifications are not added, the QNX system can start normally. However, after adding the modifications in PFE-DRV_S32G_QNX_1.8.0_IntegrationManual.pdf, the startup fails.&lt;BR /&gt;please help check.Thanks.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Miles</description>
    <pubDate>Tue, 07 Apr 2026 01:21:31 GMT</pubDate>
    <dc:creator>miles_yang</dc:creator>
    <dc:date>2026-04-07T01:21:31Z</dc:date>
    <item>
      <title>s32g2 QNX PFE driver</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345022#M16205</link>
      <description>&lt;P&gt;Hi Teams,&lt;/P&gt;&lt;P&gt;software information:&lt;BR /&gt;PFE QNX driver version: 1.8.0&lt;BR /&gt;PFE FW version: 1.11.0&lt;BR /&gt;QNX SDP version: 7.1.0&lt;BR /&gt;Uboot ATF BSP39.0&lt;BR /&gt;When I made these changes:&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;struct udevice *dev = NULL;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;const struct eth_ops* opsptr;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;char cmd[128];&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;/* Enable GMAC eqos eth */&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;ret = uclass_get_device_by_name(UCLASS_ETH, "ethernet@4033c000", &amp;amp;dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr = DM_DRIVER_GET(eth_eqos)-&amp;gt;ops;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;ret = opsptr-&amp;gt;start(dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;/* Enable PFE driver */&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;uclass_get_device_by_name(UCLASS_MISC, "pfeng-base", &amp;amp;dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;DM_DRIVER_GET(pfeng)-&amp;gt;probe(dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;uclass_get_device_by_name(UCLASS_ETH, "pfe2", &amp;amp;dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr = DM_DRIVER_GET(pfeng_netif)-&amp;gt;ops;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr-&amp;gt;start(dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;uclass_get_device_by_name(UCLASS_ETH,"pfe1",&amp;amp;dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr = DM_DRIVER_GET(pfeng_netif)-&amp;gt;ops;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr-&amp;gt;start(dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;uclass_get_device_by_name(UCLASS_ETH,"pfe0",&amp;amp;dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr = DM_DRIVER_GET(pfeng_netif)-&amp;gt;ops;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;opsptr-&amp;gt;start(dev);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;snprintf(cmd, sizeof(cmd), "scmi_clk gate protocol@14 pfe_ts 1");&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;run_command(cmd, 0);&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;snprintf(cmd, sizeof(cmd), "scmi_clk gate protocol@14 ftm 1");&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;run_command(cmd, 0);&lt;/FONT&gt;&lt;BR /&gt;And use these commands to start the QNX system&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g274a-rdb2.dtb; run atf_fdt_0to3; run&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;release_cpus; fatload mmc 0:1 0x80080000 ifs-s32g274a-rdb.ui; bootm 0x80080000 - 0x83E00000'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv atf_fdt_0to3 'fdt addr 0x83e00000; fdt resize; fdt set /cpus/cpu@1 cpu-release-addr &amp;lt;0x0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;0xa0000010&amp;gt;; fdt set /cpus/cpu@100 cpu-release-addr &amp;lt;0x0 0xa0000010&amp;gt;; fdt set /cpus/cpu@101&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;cpu-release-addr &amp;lt;0x0 0xa0000010&amp;gt;;'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv release_cpus 'run cpu_trap; mp 1 release 0xa0000000; mp 2 release 0xa0000000; mp 3 release&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;0xa0000000;'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv cpu_trap 'dcache off; mw.l 0xa0000000 0xd503205f; mw.l 0xa0000004 0x58000060; mw.l 0xa0000008&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;0xb4ffffc0; mw.l 0xa000000C 0xd61f0000; mw.q 0xa0000010 0x00000000; dcache on;'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv bootcmd 'run boot_qnx_atf'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv hwconfig "serdes0:mode=pcie,clock=ext;pcie0:mode=rc;serdes1:mode=xpcs0&amp;amp;xpcs1,&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;clock=ext,fmhz=125;xpcs1_0:speed=2G5;xpcs1_1:speed=1G"&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;setenv skip_scmi_reset_agent '1'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;saveenv&lt;/FONT&gt;&lt;BR /&gt;System will startup failed，&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;Starting kernel ...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;clk pfe1_tx_sgmii already disabled&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;clk pfe1_rx_sgmii already disabled&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;Found PFE version 0x50300 (S32G2)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;Found PFE version 0x50300 (S32G2)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;pfe2 Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;## Setting pfe_ts clock ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;## Setting ftm0_sys clock ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;## Setting ftm0_ext clock ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;## Setting ftm1_sys clock ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;## Setting ftm1_ext clock ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;Board: NXP S32G274A RDB2 Revision E&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#00CCFF"&gt;Error bringing up core 1 with error 0&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;The startup log has been uploaded to the attachment.&lt;/P&gt;&lt;P&gt;Best Regards&lt;BR /&gt;Miles&lt;/P&gt;</description>
      <pubDate>Fri, 03 Apr 2026 09:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345022#M16205</guid>
      <dc:creator>miles_yang</dc:creator>
      <dc:date>2026-04-03T09:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: s32g2 QNX PFE driver</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345054#M16208</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;miles_yang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Could you share more information with me?&lt;/P&gt;
&lt;P&gt;1.are you using the customer board or our development board RDB2/RDB3?&lt;/P&gt;
&lt;P&gt;2.Do you only use the PFE application on the A core?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Fri, 03 Apr 2026 10:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345054#M16208</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-04-03T10:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: s32g2 QNX PFE driver</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345861#M16216</link>
      <description>Hi Joey,&lt;BR /&gt;I am using the customer board, and the CPU is S32G274A.&lt;BR /&gt;Yes, currently only core A is running. The QNX system is started via Uboot. If the above modifications are not added, the QNX system can start normally. However, after adding the modifications in PFE-DRV_S32G_QNX_1.8.0_IntegrationManual.pdf, the startup fails.&lt;BR /&gt;please help check.Thanks.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Miles</description>
      <pubDate>Tue, 07 Apr 2026 01:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2345861#M16216</guid>
      <dc:creator>miles_yang</dc:creator>
      <dc:date>2026-04-07T01:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: s32g2 QNX PFE driver</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2347819#M16231</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;miles_yang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;Do you want to config the PFE in U-boat stage? About the more information, you can try to refer to the&amp;nbsp;7.3 Ethernet Software support on S32G2 of&amp;nbsp;S32G2_LinuxBSP_39.0_User_Manual.pdf.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Thu, 09 Apr 2026 02:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-QNX-PFE-driver/m-p/2347819#M16231</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-04-09T02:33:01Z</dc:date>
    </item>
  </channel>
</rss>