<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet on the S32G-VNP-RDB2 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339700#M16169</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260641"&gt;@MaximeGPwrx&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1. The PFE driver(&lt;SPAN&gt;Eth_43_PFE&lt;/SPAN&gt;) is released as a standalone package, and is not included in the standard RTD, you may need to integrate it with RTD to configure/build.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Unfortunately, the PFE driver configuration is not supported in S32DS and is only available in EB. so if you are willing to use this driver, I suggest using EB instead.&lt;/P&gt;
&lt;P&gt;3. If only testing with PFE_MAC2, then using BSP(A53 software packages) may be more easier, since no specific settings needed for enabling it on RDB2.&lt;/P&gt;
&lt;P&gt;Sorry for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Thu, 26 Mar 2026 02:43:33 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2026-03-26T02:43:33Z</dc:date>
    <item>
      <title>Ethernet on the S32G-VNP-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339097#M16164</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;What is the most easiest way to receive an ethernet france through the ethernet port PFE_MAC2 on the board&amp;nbsp;S32G-VNP-RDB2 ?&lt;BR /&gt;&lt;BR /&gt;Constraint : I don't want a complexe EBTresOS configuration.&lt;BR /&gt;&lt;BR /&gt;I want to stay in S32DS and at least just receive a frame on my rx buffer.&lt;BR /&gt;&lt;BR /&gt;All of the provided example are, for me, not enough straight forward and required an over complexification of the build process with EBTresOS.&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 09:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339097#M16164</guid>
      <dc:creator>MaximeGPwrx</dc:creator>
      <dc:date>2026-03-25T09:09:34Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet on the S32G-VNP-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339232#M16165</link>
      <description>&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. Sorry that currently the PFE examples included in the PFE MCAL packages are configured by the EB.&lt;/P&gt;
&lt;P&gt;2. There is a S32DS based demo, which could be downloaded from the following &lt;A href="https://www.nxp.com/webapp/Download?colCode=PFE-Ethernet-LWIP-FreeRTOS_S32G-demo" target="_self"&gt;link&lt;/A&gt;:&lt;/P&gt;
&lt;P&gt;But it is based on very early version code base and no formal updated version existed.&lt;/P&gt;
&lt;P&gt;3. If working with latest version BSP(A53 cores), then the default BSP images flashed to the SD card could boot the RDB2 correctly, and the PFE_MAC2 could receive frames with default settings.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 10:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339232#M16165</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-03-25T10:39:23Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet on the S32G-VNP-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339378#M16166</link>
      <description>&lt;P&gt;This example also use an EB TresOS configuration. This configuration has just been pre built by NXP.&lt;BR /&gt;&lt;BR /&gt;In order to use the PFE_MAC2 ethernet interface, what RTD driver I have to use ?&lt;BR /&gt;&lt;BR /&gt;For example, from the installation directory, Eth_TS and EthIf_TS is enough ?&lt;/P&gt;&lt;P&gt;Or I have to install something else ?&lt;/P&gt;&lt;P&gt;For example, in the example you shown, they use the driver Eth_43_PFE_TS&lt;BR /&gt;&lt;BR /&gt;What is the goal of this driver ?&lt;BR /&gt;&lt;BR /&gt;I just try to keep things simple. And for just an ethernet things, it looks like something really complex...&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Is it mandatory ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 13:27:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339378#M16166</guid>
      <dc:creator>MaximeGPwrx</dc:creator>
      <dc:date>2026-03-25T13:27:59Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet on the S32G-VNP-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339700#M16169</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260641"&gt;@MaximeGPwrx&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1. The PFE driver(&lt;SPAN&gt;Eth_43_PFE&lt;/SPAN&gt;) is released as a standalone package, and is not included in the standard RTD, you may need to integrate it with RTD to configure/build.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Unfortunately, the PFE driver configuration is not supported in S32DS and is only available in EB. so if you are willing to use this driver, I suggest using EB instead.&lt;/P&gt;
&lt;P&gt;3. If only testing with PFE_MAC2, then using BSP(A53 software packages) may be more easier, since no specific settings needed for enabling it on RDB2.&lt;/P&gt;
&lt;P&gt;Sorry for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 26 Mar 2026 02:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2339700#M16169</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-03-26T02:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet on the S32G-VNP-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2350853#M16260</link>
      <description>&lt;P&gt;This is very interesting.&lt;BR /&gt;&lt;BR /&gt;I have one another question :&lt;BR /&gt;&lt;BR /&gt;1/ What is the difference between the PFE Driver (the one that need EB) and the Eth_43_PFE that is standalone and don't require any configuration ?&lt;BR /&gt;&lt;BR /&gt;2/ Can we do the same things with them ?&lt;BR /&gt;&lt;BR /&gt;3/ If we only want to respond to some icmp request (ping) from PFE0, PFE1 and PFE2, what we have to do ? Like what peripheral we have to use in S32 Design Studio ? Please, without EB.&lt;BR /&gt;&lt;BR /&gt;4/ I'm curious. Why NXP choose to integrate EB in the dev workflow to configure the driver ?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Apr 2026 16:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Ethernet-on-the-S32G-VNP-RDB2/m-p/2350853#M16260</guid>
      <dc:creator>MaximeGPwrx</dc:creator>
      <dc:date>2026-04-14T16:42:45Z</dc:date>
    </item>
  </channel>
</rss>