<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G3 EthCtrlConfigShaper in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332199#M16113</link>
    <description>&lt;P&gt;Hi Joey,&lt;BR /&gt;&lt;BR /&gt;Thank you for the reply. Yes I did change the values in the config tool. The config tool only provides idleslopecredit, locredit and hicredit values to be modified. But these changes are not reflected when code is generated.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;</description>
    <pubDate>Fri, 13 Mar 2026 05:52:56 GMT</pubDate>
    <dc:creator>disrupt-user01</dc:creator>
    <dc:date>2026-03-13T05:52:56Z</dc:date>
    <item>
      <title>S32G3 EthCtrlConfigShaper</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2331243#M16107</link>
      <description>&lt;P&gt;I have s32g3 gold box, and I have this project&amp;nbsp;lwip_FreeRTOS_S32G399A_M7_rtd402. I am adding a&amp;nbsp;EthCtrlConfigShaper to Fifo_1, and setting max value to&amp;nbsp;EthCtrlConfigShaperIdleSlope which is&amp;nbsp;750000000. I don't see these values generated in Gmac_Ip_Sa_PBcfg.c&lt;BR /&gt;what I am getting is:&lt;/P&gt;&lt;P&gt;{&lt;BR /&gt;/*.weight = */0U,&lt;BR /&gt;/*.idleSlopeCredit = */0U,&lt;BR /&gt;/*.sendSlopeCredit = */0U,&lt;BR /&gt;/*.hiCredit = */0U,&lt;BR /&gt;/*.loCredit = */0,&lt;BR /&gt;/*.ringDesc = */GMAC_0_TxRing_1_DescBuffer,&lt;BR /&gt;/*.callback = */Eth_TxIrqCallback,&lt;BR /&gt;/*.buffer = */GMAC_0_TxRing_1_DataBuffer,&lt;BR /&gt;/*.interrupts = */(uint32)GMAC_CH_INTERRUPT_TI,&lt;BR /&gt;/*.bufferLen = */1536U,&lt;BR /&gt;/*.ringSize = */4U,&lt;BR /&gt;/*.priorityMask = */(uint8)GMAC_VLAN_PRIORITY_4 | (uint8)GMAC_VLAN_PRIORITY_5 | (uint8)GMAC_VLAN_PRIORITY_6 | (uint8)GMAC_VLAN_PRIORITY_7,&lt;BR /&gt;/*.dmaBurstLength = */64U,&lt;BR /&gt;/*.queueOpMode = */GMAC_OP_MODE_DCB_GEN&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;I would want the idlescopecredit, sendslopecredit and queueopmode be updated accordingly but its not happening.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 09:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2331243#M16107</guid>
      <dc:creator>disrupt-user01</dc:creator>
      <dc:date>2026-03-12T09:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 EthCtrlConfigShaper</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332100#M16111</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Do you have changed these values of (&lt;SPAN&gt;&amp;nbsp;idlescopecredit, sendslopecredit and queueopmode) in Config Tool? But do&amp;nbsp;you not find these values be modified in the code?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Joey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 02:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332100#M16111</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-03-13T02:25:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 EthCtrlConfigShaper</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332199#M16113</link>
      <description>&lt;P&gt;Hi Joey,&lt;BR /&gt;&lt;BR /&gt;Thank you for the reply. Yes I did change the values in the config tool. The config tool only provides idleslopecredit, locredit and hicredit values to be modified. But these changes are not reflected when code is generated.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 05:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332199#M16113</guid>
      <dc:creator>disrupt-user01</dc:creator>
      <dc:date>2026-03-13T05:52:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 EthCtrlConfigShaper</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332395#M16114</link>
      <description>&lt;P&gt;The problem is solved,&amp;nbsp;&lt;SPAN&gt;in the EthCtrlConfigSchedulerPredecessorRef destination we had to set the shaper instead of fifo.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 09:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-EthCtrlConfigShaper/m-p/2332395#M16114</guid>
      <dc:creator>disrupt-user01</dc:creator>
      <dc:date>2026-03-13T09:43:59Z</dc:date>
    </item>
  </channel>
</rss>