<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G LLCE  CAN TX in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1357734#M161</link>
    <description>&lt;P&gt;I use the demo "S32G_LLCE_1.0.2-&amp;gt;llce_sample_app_pfe" and Bridge Can0 and Can1 busses on S32GRV-PLATEVB. The project can be compiled normally.However, the code is always waiting for the transmission completion of llce can.&lt;/P&gt;&lt;P&gt;"while(txConfirmationCount &amp;lt; (4 * frame_ctr)) ; /* Wait for TX to avoid overloading the TX buffer */"&lt;/P&gt;</description>
    <pubDate>Tue, 19 Oct 2021 08:15:43 GMT</pubDate>
    <dc:creator>longfeiwang</dc:creator>
    <dc:date>2021-10-19T08:15:43Z</dc:date>
    <item>
      <title>S32G LLCE  CAN TX</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1357734#M161</link>
      <description>&lt;P&gt;I use the demo "S32G_LLCE_1.0.2-&amp;gt;llce_sample_app_pfe" and Bridge Can0 and Can1 busses on S32GRV-PLATEVB. The project can be compiled normally.However, the code is always waiting for the transmission completion of llce can.&lt;/P&gt;&lt;P&gt;"while(txConfirmationCount &amp;lt; (4 * frame_ctr)) ; /* Wait for TX to avoid overloading the TX buffer */"&lt;/P&gt;</description>
      <pubDate>Tue, 19 Oct 2021 08:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1357734#M161</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-10-19T08:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE  CAN TX</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1358621#M167</link>
      <description>&lt;P&gt;The Applications team have addressed this issue in the internal training Forum. Please avoid making duplicate posts.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 12:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1358621#M167</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-10-20T12:07:18Z</dc:date>
    </item>
    <item>
      <title>回复： S32G LLCE  CAN TX</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1602758#M2268</link>
      <description>How do you solve this problem?</description>
      <pubDate>Tue, 21 Feb 2023 09:33:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1602758#M2268</guid>
      <dc:creator>shanlan123</dc:creator>
      <dc:date>2023-02-21T09:33:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE  CAN TX</title>
      <link>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1602760#M2269</link>
      <description>Where can I see the solution? I still have this problem</description>
      <pubDate>Tue, 21 Feb 2023 09:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-LLCE-CAN-TX/m-p/1602760#M2269</guid>
      <dc:creator>shanlan123</dc:creator>
      <dc:date>2023-02-21T09:34:30Z</dc:date>
    </item>
  </channel>
</rss>