<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: s32_LLCE</title>
    <link>https://community.nxp.com/t5/S32G/s32-LLCE/m-p/2329686#M16099</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260398"&gt;@yuancz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;1. From S32G SOC perspective, LLCE is a IP block on the SOC,&amp;nbsp;&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;The LLCE offloads the Host CPU from all interface level tasks along with validating, authenticating of frames for security,&amp;nbsp;&lt;/SPAN&gt;it could be used for&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;Hardware acceleration for filtering and prioritization of messages&lt;/SPAN&gt;&amp;nbsp;, since the cores on S32 SOC would not need to run any code for processing such traffic, from this view, it is indeed hardware accelerated engine.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp; &lt;SPAN class="fontstyle0"&gt;LLCE is actually a combination of cores, memory, hardware acceleration IP blocks, and firmware developed by NXP.&lt;/SPAN&gt;&amp;nbsp;Looking into the IP block, the software(FW) is running on the M0+ cores, the cores and the other hardware involved all together to achieve the functions that required by the host via the FW APIs, from LLCE itself view, some of the operation is done via the code running on M0+ cores, which could be seen as software(FW) based operation.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 10 Mar 2026 10:27:21 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2026-03-10T10:27:21Z</dc:date>
    <item>
      <title>s32_LLCE</title>
      <link>https://community.nxp.com/t5/S32G/s32-LLCE/m-p/2329518#M16097</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Is it correct to understand that the acceleration method for the LLCE in the S32 series is primarily achieved through software-based routing and forwarding? In reality, the hardware only contains a lookup table, while the forwarding of destinations is entirely handled by software?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Mar 2026 08:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32-LLCE/m-p/2329518#M16097</guid>
      <dc:creator>yuancz</dc:creator>
      <dc:date>2026-03-10T08:49:04Z</dc:date>
    </item>
    <item>
      <title>Re: s32_LLCE</title>
      <link>https://community.nxp.com/t5/S32G/s32-LLCE/m-p/2329686#M16099</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260398"&gt;@yuancz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;1. From S32G SOC perspective, LLCE is a IP block on the SOC,&amp;nbsp;&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;The LLCE offloads the Host CPU from all interface level tasks along with validating, authenticating of frames for security,&amp;nbsp;&lt;/SPAN&gt;it could be used for&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;Hardware acceleration for filtering and prioritization of messages&lt;/SPAN&gt;&amp;nbsp;, since the cores on S32 SOC would not need to run any code for processing such traffic, from this view, it is indeed hardware accelerated engine.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp; &lt;SPAN class="fontstyle0"&gt;LLCE is actually a combination of cores, memory, hardware acceleration IP blocks, and firmware developed by NXP.&lt;/SPAN&gt;&amp;nbsp;Looking into the IP block, the software(FW) is running on the M0+ cores, the cores and the other hardware involved all together to achieve the functions that required by the host via the FW APIs, from LLCE itself view, some of the operation is done via the code running on M0+ cores, which could be seen as software(FW) based operation.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Mar 2026 10:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32-LLCE/m-p/2329686#M16099</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-03-10T10:27:21Z</dc:date>
    </item>
  </channel>
</rss>