<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: NXP-S32G399-RD3</title>
    <link>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325950#M16080</link>
    <description>First of all, thank you for your answer, but now I'm looking at the circuit diagram of s32g339-rd3 and now I'm connected from s32g339a to KSZ9031 RJ45 through GMAC0 and this is not connected to ETH_SWITCH SJA1110?</description>
    <pubDate>Wed, 04 Mar 2026 05:56:05 GMT</pubDate>
    <dc:creator>dongmin</dc:creator>
    <dc:date>2026-03-04T05:56:05Z</dc:date>
    <item>
      <title>NXP-S32G399-RD3</title>
      <link>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325841#M16076</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I'm a student studying tsn right now. The development board I'm using now is nxp-s32g399-rd3. I want to work on a project that implements Qbu functionality right now. First of all, it's not implemented on the GUI in SJA1110 in nxp-s32g399-rd3. So I'm not sure about the direction right now. I wonder if I should proceed with all of these registers as a register. And I'm also wondering what document these registers are organized in. And now I'm wondering if you're dealing with PFE, GMAC, and LLCE. Also, if I do Qbu, I usually go into eMAC and pMAC, but I'm wondering where layer I'll actually do this!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 01:38:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325841#M16076</guid>
      <dc:creator>dongmin</dc:creator>
      <dc:date>2026-03-04T01:38:16Z</dc:date>
    </item>
    <item>
      <title>Re: NXP-S32G399-RD3</title>
      <link>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325928#M16078</link>
      <description>&lt;P&gt;hi,&lt;SPAN&gt;dongmin&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;If you want to operate the SJA1110 register, you can refer to its User Manul and datasheet. All SJA1110 models are equipped with hardware-assisted information security and functional safety capabilities, multiple gigabit SGMII interfaces, and comply with the latest AVB and TSN standards.&lt;/P&gt;
&lt;P&gt;For gmac, it supports&amp;nbsp;Frame Preemption (IEEE 802.1Qbu) for time-sensitive networking. PFE supports 802.1AS-Rev and IEEE 1588 precision clock synchronization protocol. Provides QoS (Quality of Service). LLCE handles CAN/LIN/FlexRay acceleration and routing.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 04:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325928#M16078</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-03-04T04:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: NXP-S32G399-RD3</title>
      <link>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325950#M16080</link>
      <description>First of all, thank you for your answer, but now I'm looking at the circuit diagram of s32g339-rd3 and now I'm connected from s32g339a to KSZ9031 RJ45 through GMAC0 and this is not connected to ETH_SWITCH SJA1110?</description>
      <pubDate>Wed, 04 Mar 2026 05:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325950#M16080</guid>
      <dc:creator>dongmin</dc:creator>
      <dc:date>2026-03-04T05:56:05Z</dc:date>
    </item>
    <item>
      <title>Re: NXP-S32G399-RD3</title>
      <link>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325970#M16083</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;dongmin&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please refer to this link for the download of circuit&amp;nbsp;diagram.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/S32G-VNP-RDB3" target="_blank" rel="noopener"&gt;S32G3 Vehicle Networking Reference Design | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;I'm connected from s32g339a to KSZ9031 RJ45 through GMAC0 and this is not connected to SJA1110?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;Yes&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 06:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325970#M16083</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-03-04T06:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: NXP-S32G399-RD3</title>
      <link>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325971#M16084</link>
      <description>&lt;P&gt;So if I want to use the Frame Preemption feature now, I can't use SJA1110 and I can only use GMAC directly?&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 06:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/NXP-S32G399-RD3/m-p/2325971#M16084</guid>
      <dc:creator>dongmin</dc:creator>
      <dc:date>2026-03-04T06:42:04Z</dc:date>
    </item>
  </channel>
</rss>